Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Product List
NXP5P1000

The NX5P1000 is a member of the Advanced load switch family. This device was designed for single direction USB charging port protection but it can also be used for other applications requiring 5.5 V operation at up to 2 amps and overvoltage protection to 30 volts. The NX5P2090 device has similar operation but removes the onboard USB data ESD protection for a smaller package and increase current capacity of 2 amps.

PTM Published on: 2014-03-21