Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Product List
Solutions for Motion Control PowerSTEP01 Pt 1 of 2 Slide 34

Because of the SPI, the drivers can be put in daisy chain. This allows the user to decrease the number of required GPIOs for the microcontroller when several motors are used. It also allows the synchronization of the actions of several motors by releasing the chip select of the SPI bus at the same time for all the drivers. With the daisy chain the user can control an unlimited number of motors, requiring only four I/O pins.

PTM Published on: 2015-10-27