Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Product List
using a usbxpress
After the PC-side application is complete, it can be distributed or used on other machines. To use a USBXpress device with a deployed application, first make sure that the USBXpress driver is available on the system the application will be running on, and also make sure that the USBXpress device used contains the proper firmware with unique serial strings to communicate with the Windows application.
PTM Published on: 2011-12-09