Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Product List
interrupt trans
The interrupt transfer mode has a guaranteed latency, which makes it appropriate for applications such as keyboards and mice. This is important because the response time of these devices directly translates to the user experience. Interrupt transfer is also appropriate for these devices because they do not need a lot of bandwith.
PTM Published on: 2011-12-09