Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List
ISL8215M-Slide9

Few competitors have emerged in the 40V rated input voltage power module space. Differentiation in this space often resides in the packaging technology and, as previously illustrated, several trade-offs on feature set, package size, and output current need to be made. Intersil’s unique full copper lead frame technology guarantees close to full output current capability across the full temperature range, while their controller technology offers one of the better feature sets in the industry. The ISL8215M is the highest current capable device in its category, provides a superior performance, and is a cost effective solution.

PTM Published on: 2017-12-01