Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
Clock Basics Slide 7

A Multiplier/Divider clocking circuit uses multipliers and dividers on the input signal to generate an output with a higher or lower frequency than the source. These devices are most commonly used for distribution as well, having multiple outputs at the new frequency. PLL based clocks are required for multiplying to a higher frequency, but for simple integer division to lower the frequency, a counter can be used instead of a PLL.

PTM Published on: 2011-11-08