Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
Wireless Communication with IrDA Standard Protocol Slide 4
IrDA enhances mobility since cables are no longer required. Since it is a Universal standard, it ensures interoperability with many existing devices. Some other wireless technologies (such as RF) radiate noise, they can cause interaction and interference. Since IR uses light, which is directional, these issues don’t occur. This lack of interference means that IR is safe to use in any environment such as planes and hospitals . This also eases regulatory approval. Lastly, the cost of a wireless solution can be implemented near the same cost as a wired solution.
PTM Published on: 2011-10-28