Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
Slide17
The addition of the Model TCS-DL004-250-WH reduces the current seen by the PHY by approximately 90%. The voltage isolation provided by the TCS™ device reduces the voltage level seen by the PHY by over 50%. Combining these two effects, users see a reduction in the energy the PHY must absorb of over 90%.
PTM Published on: 2012-11-27