Maker.io main logo

How To Use SMART Monitoring in Linux NAS Drives

79

2026-02-23 | By Maker.io Staff

Network-Attached Storage (NAS) devices combine multiple HDDs and SSDs and make them accessible over a network, making them ideal for backups and long-term storage for large files. But like any hardware, drives can fail as they age, and catching problems early is crucial to preventing data corruption and loss. Read on to learn how to use automated SMART monitoring to detect potential drive problems before they result in a failure.

Image of How To Use SMART Monitoring in Linux NAS Drives

What is SMART?

Self-Monitoring, Analysis, and Reporting Technology (SMART) is an industry standard supported by virtually all consumer-level HDDs, SSDs, and some flash storage media. Its purpose is to help detect and predict potential drive failures before they happen by observing values reported by various sensors built into the drive.

Hardware failures generally fall into two categories: unpredictable and predictable. Unpredictable failures happen spontaneously, such as when a device is physically damaged by a drop or a component suddenly fails. The only reliable precaution is maintaining regular backups. Predictable failures, on the other hand, typically occur as a device wears out due to use. They usually announce themselves through measurable changes in operating parameters, like increased vibration, temperature, or error rates.

SMART is designed to detect these predictable failures. It defines a set of attributes, such as temperature, reallocated sectors, read/write error rates, spin-up time, and power-on hours, along with threshold values for each. Monitoring software can read these attributes and issue warnings if any values exceed their thresholds. A system, whether a computer or a NAS, can then react automatically or alert an administrator, who can take action such as creating backups or replacing the affected drive.

Why SMART Monitoring is Vital in a NAS

Network-Attached Storage (NAS) can be especially vulnerable to hardware failures, since the drives often run continuously, particularly in 24/7 setups. Additionally, NAS devices are often used to back up important files, and data corruption can be costly. Automated warnings that predict potential drive failures before they occur can help protect your data and prevent loss.

Installing a Linux SMART Monitor

Getting started with SMART monitoring on Linux only requires the installation of a single package:

Copy Code
sudo apt update 
sudo apt install smartmontools

Once installed, the following command lists the system’s block devices, and it helps identify the drive names of the devices to monitor:

Copy Code
lsblk

Image of How To Use SMART Monitoring in Linux NAS Drives This screenshot demonstrates the output of the lsblk command.

Next, check whether SMART is enabled on the devices you want to monitor. Use the following command to determine the SMART status, but make sure to replace drive_identifier with the actual device name, for example, sda1:

Copy Code
sudo smartctl -i /dev/drive_identifier

Virtually all recent HDDs and SSDs support SMART. However, the check can still reveal that the feature is turned off, in which case you can enable SMART on a drive by typing:

Copy Code
sudo smartctl -s on /dev/drive_identifier

Finally, verify that the smart monitor works as expected by printing a health report of all relevant devices with the following command:

Copy Code
sudo smartctl -H /dev/drive_identifier

Image of How To Use SMART Monitoring in Linux NAS Drives The screenshot shows the result of the SMART info output and the self-test result.

Using the -A flag with a drive lists all available attributes and their current values, and the -t flag starts a short/long self-test, depending on the parameter value:

Copy Code
sudo smartctl -A /dev/drive_identifier # Show attributes
sudo smartctl -t short /dev/drive_identifier # Quick self-test 
sudo smartctl -t long /dev/drive_identifier # Full self-test

Image of How To Use SMART Monitoring in Linux NAS Drives Use the -A flag to show the available SMART attributes and their values.

Configuring Automated SMART Warnings

Manually running health checks can give a snapshot of a drive’s current condition. However, devices typically fail silently at the worst possible time, and manual checks might miss emerging problems. Most SMART monitors can be configured to continuously keep an eye on drives and send an email alert to an administrator should they detect an issue.

Users only have to adjust a single configuration file to activate this feature:

Copy Code
sudo nano /etc/smartd.conf

By default, the file contains numerous comments, and it should have a single line starting with the DEVICESCAN keyword. Make sure to comment out the line by adding a pound symbol (#) at the start:

Copy Code
#DEVICESCAN -d removable -n standby -m root -M exec
/usr/share/smartmontools/smartd-runner

Then, add an entry for each drive you want the tool to monitor:

Copy Code
/dev/drive_identifier -a -o on -S on -s 
(S/../.././02|L/../../6/03) -m you@example.com

Each line starts with the device identifier. It’s then followed by the -a flag, which tells smartd to monitor all available SMART attributes. The -o and -S flags turn on offline data collection and threshold persistence, respectively. The values in the parentheses instruct smartd to conduct a short (S) test each day at two in the morning, and a long (L) test on each Sunday at three in the morning. Lastly, the -m flag and its parameter specify who will be contacted in case of a problem.

Once configured, start and activate the background service by typing:

Copy Code
sudo systemctl enable smartmontools 
sudo systemctl start smartmontools

Installing a Mail Transfer Agent (MTA)

The SMART monitor alone cannot send emails; instead, it relies on a mail transfer agent (MTA). You can install an MTA and the accompanying packages for smartd by typing:

Copy Code
sudo apt install msmtp msmtp-mta bsd-mailx

Once installed, edit or create a global configuration file:

Copy Code
sudo nano /etc/msmtprc

Add your email provider’s configuration details to this file. In this example, I’ll configure a Google Mail account for sending out warning emails:

Copy Code
# Default account
defaults
auth        on 
tls         on
tls_trust_file /etc/ssl/certs/ca-certificates.crt
logfile /var/log/msmtp.log
# Gmail account
account     gmail
host        smtp.gmail.com
port        587
from        your_gmail_address@gmail.com
user        your_gmail_address@gmail.com
password    your_app_password
# Set default account
account default  :  gmail

When using Gmail, the client expects an app password, which is different from the Google account password. It must be created by navigating to the Google account settings and then selecting app passwords from the search bar on the security settings page:

Image of How To Use SMART Monitoring in Linux NAS Drives  Follow the highlighted steps to navigate to the app password settings in your Google account settings.

Next, enter a name that describes what the password will be used for:

Image of How To Use SMART Monitoring in Linux NAS Drives Click the highlighted button to create a GMail app password.

Google creates a unique passphrase that's only displayed once. Copy the passcode and paste it into the MTA configuration file. Note that Google shows the 16-character code with spaces separating the individual four-character groups. You must remove these whitespace characters from the code in the configuration file:

Image of How To Use SMART Monitoring in Linux NAS Drives Your MTA configuration file should look similar to the one shown in this screenshot.

Finally, adjust some system permissions so that the root user can access the newly created MTA configuration file. This step is necessary because the SMART monitor runs as a root process, and it sends emails using the root account:

Copy Code
sudo chmod 600 /etc/msmtprc
sudo chown root:root /etc/msmtprc

You can test your MTA setup and configuration using the following command:

Copy Code
echo "Test email from msmtp" | sudo msmtp
your_gmail_address@gmail.com

If configured correctly, the MTA sends an email to the specified email address using the Google Mail account you set up earlier.

Lastly, restart the SMART monitor background service so that it picks up the changed configuration files and MTA settings:

Copy Code
sudo systemctl restart smartmontools

The SMART monitor includes a test mode that lets you verify that the whole setup works as expected. To do so, open up the configuration file from before:

Copy Code
sudo nano /etc/smartd.conf

Then, find the lines you added before, and append -M test to each entry. For example:

Copy Code
/dev/drive_identifier -a -o on -S on -s 
(S/../.././02|L/../../6/03) -m you@example.com -M test

Finally, restart the smartmontools service. It should start up as expected, and you should see a message similar to the following one in your email inbox:

Image of How To Use SMART Monitoring in Linux NAS Drives If everything is configured correctly, the service should immediately send a test mail after restarting it.

Do not forget to remove the -M option from the configuration file and restart the service one last time once you have verified that it works as expected:

Image of How To Use SMART Monitoring in Linux NAS Drives The final configuration entries should not include the -M test mode option.

Limitations of SMART

SMART is a valuable tool for maintaining the reliability of NAS and long-term backup drives. It cannot guarantee that all failures are detected in advance. For example, an older Google study found that roughly a third of drives fail without any prior SMART warnings. Still, in about two-thirds of cases, SMART was able to flag issues before they resulted in data loss. For these reasons, it’s essential to combine SMART monitoring with RAID redundancy and regular backups to keep important files safe.

Summary

SMART is an essential tool for maintaining the health and reliability of NAS drives. By tracking critical device attributes such as temperature, reallocated sectors, read/write error rates, spin-up time, and power-on hours, SMART can provide early warnings of predictable hardware failures. On Linux systems, this monitoring can be automated, enabling administrators to schedule regular self-tests, track all available SMART attributes, and receive alerts via email when issues arise.

To enable email notifications, a Mail Transfer Agent (MTA) must be configured so that the SMART monitor can dispatch alerts. This ensures that potential problems are flagged before they occur, allowing you to create backups or replace drives.

SMART cannot catch every failure, but it effectively identifies most predictable problems, making it a vital complement to RAID setups and routine backups. By combining automated monitoring, scheduled self-tests, and proactive alerting, users can reduce the risk of unexpected drive failures and protect valuable data in long-term storage environments.

Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.