Maker.io main logo

What Are Servos - A Brief Guide

69

2023-07-27 | By Kitronik Maker

License: See Original Project

Courtesy of Kitronik

Guide by Kitronik Maker

Radio Control (RC) Servos are a simple way to provide electronically controlled ‎movement for many projects. Figure 1, for instance, shows a small RC servo-‎controlled robot arm. In this document, the word ‘servo’ refers to a servo designed ‎to be used with a radio control system, typically terminated in a 3-pin plug (figure ‎‎2). It does not refer to the more general, wide-ranging, description of a servo motor ‎‎– that is a motor which has feedback control.‎

servos_1

I am not aware of any actual 'standard' in the ISO (International Standards ‎Organisation) sense that governs radio control servos. That said the many ‎different manufacturers have mostly converged, such that most general-purpose ‎servos will perform as expected with most controllers.‎

Download this guide as a PDF

Servos – A Brief Guide:‎

This document does not consider the advanced features that latest range of 'digital' ‎servos may have (such as faster frame rates, programmable end stops etc.). It ‎treats things such as brushless motors, 7.4V LiPo compatibility and similar as not ‎important to the fundamental understanding it hopes to convey. ‎‎

A Little History:‎

Radio Control for hobby use has been around for a long time. Figure 3 shows a ‎club meeting of The Johnson Space Center Radio Control Club around 1967, ‎showing some very old RC equipment.‎

club_2

‎Figure 3 The Johnson Space Center RC club

‎Multi-channel Radio Control systems existed in the 1960s and were relatively ‎common in the early 1980s (when I started modelling as a hobby). This document ‎is not especially concerned with the mechanics of how the control signal gets from ‎the radio transmitters 'stick' to the radio receiver that would typically be controlling ‎the servos – the radio part of RC. It is only concerned with how the receiver ‎controls the servos, and how that can also be used in programmable systems. ‎‎ ‎

Today’s Servos:‎

The servos we buy today are based on a system that was devised by Doug Spreng ‎and Don Mathes in the 1960s. They developed a servo mechanism that would ‎respond to a changing pulse width. That pulse was 1-2mS in width and repeated ‎over a 'frame rate' of 50Hz. To allow multiple channels control the system simply ‎sends each servo in turn, followed by a 'sync' period of no pulses of at least 2 ‎channels (4mS). This allows the receiver to 'know' when the first servo is, and ‎hence to control the correct channels. Figure 4 illustrates 3 different pulse trains, ‎with 4 servos in each at 1, 1.5 and 2mS pulse widths.‎

trains_3 ‎ ‎

Figure 4 Servo Pulse Trains‎

‎The Servo itself also generates a set of pulses and uses the width of the received ‎pulse as a reference to adjust its internal timer. It does this by using the error ‎‎(defined as the difference between the 2 pulses) to drive a motor, which then turns ‎a set of gears. As it does so a potentiometer is also moved by the gear train, ‎altering the internal timer. When the pulse trains match (within a deadband) the ‎servo stops moving. The Servo output horn is fixed to the end of this gear train. An ‎update rate of 50Hz is fast enough for most purposes, but if driving servos from a ‎microcontroller they are usually quite forgiving of faster (and slower update rates.) ‎If you do not send any control pulses then the servo will hold its last position or ‎give up holding position altogether. This is another none specified feature that ‎varies from manufacturer to manufacturer.‎‎ ‎

Servo Ranges:‎

Typically, the 1-2mS pulse used with a servo will create a movement range of ‎between 60 and 90 degrees of the output shaft. +- 45 degrees is plenty for the ‎control of a model aeroplane surface, the original design intention. (Figure 5).‎

horn_4

Figure 5 Servo Horn (Red) at +- 45 degrees‎‎

‎A lot of servos are available, especially for robotics advertising different movement ‎ranges: 90 degrees, 180 degree and continuous rotation being typical examples. ‎Whilst it is possible to provide 180 degrees of rotation from the normal 1-2mS ‎pulse this requires changing the gearing of the servo. A lot of the cheaper servos ‎advertised as 180 degrees actually require a longer pulse to provide full travel. ‎Remember that 90 degrees is typically a variation of 1mS, so for a generic 180-‎degree servo, the pulse must vary by 2mS. Often this requires sending a pulse of ‎‎0.5 to 2.5mS. Figure 6 shows how pulse width and servo horn movement match.‎

pulse_5

Figure 6 Servo position related to pulse-width

‎‎This can be an issue for use with radio control systems, where there may not be a ‎travel adjust option to stretch the pulses. More advanced radio systems are able to ‎generate longer / shorter pulses to deal with this. If the servo is being used in a ‎programmable system, for instance with an Arduino or micro:bit controlling it, then ‎this is less of an issue. The software in these systems will allow control over both ‎the pulse range and repetition frequency. Both of these systems (and many other ‎hobbyist microcontrollers) can generate longer pulses. The Arduino's popular servo ‎library, for instance, uses 0.544mS to 2.4mS as it limits, and the BBC micro:bit ‎generates pulses from 0.5 to 2.5mS.‎ ‎‎

360 or Continuous Rotation Servos:‎

servowheel_6

Figure 7 A Continuous rotation servo and wheel‎ ‎

Whilst continuous rotation servos look like and are controlled like servos, (figure 7) ‎they are actually not a servo system at all. The general description of a servo ‎motor is a system with a motor and some positional feedback on the output of that ‎motor. In a 360 degree servo, the feedback potentiometer is replaced with either a ‎small trimmer potentiometer, which is not connected to the output shaft or a fixed ‎potential divider, made from fixed value resistors. In a servo, the speed with which ‎the output shaft moves to the commanded position is proportional to the error in ‎position. With a 360 servo, the feedback is fixed at the neutral (~1.5mS pulse width) ‎position. This then allows the command of a position to be effectively translated to ‎a command of speed. Because the feedback is mechanically disconnected the ‎error does not change, and the motor continues to turn. If the error is small (such ‎as a commanded position of 100 degrees ~ 1.6mS) then the motor turns relatively ‎slowly. If it is large, such as a commanded position of 180 degrees (2.5mS) then ‎the motor turns fast. (Figure 8)‎

movement_7 ‎ ‎

Figure 8 Commanded position vs speed of movement‎

‎Error and Speed of Movement:

Without getting into detail about control and system bandwidths it is simplest to ‎say that the speed a servo moves is proportional to the error between the ‎commanded position and the measure position. This is true for servos up to an ‎error of about 20% of the travel. After that point, the servo is already moving as ‎fast as it can and increasing the error won't generally give any faster response. ‎Going back to the origin of the system a 20% error in where a model aeroplane ‎control surface is supposed to be is already very large. For servos, there are not ‎normally any noticeable effects of this limitation. For 360-degree servos however it ‎can mean that precise speed control is difficult – the speed range is compressed ‎into a commanded position of around +-36 degrees. Add to this that cheaper servos ‎exhibit ‘stiction’ where they don’t start smoothly, slight variations in the neutral ‎position due to voltage fluctuations, and the effect is that to go at a precise speed ‎needs very careful control of the timing of the pulse - a variation of around 400 ‎microseconds (0.0004 seconds) is the full range of the speed control. If smooth, ‎precise speed control of motors is required, but using a servo interface, then an ‎RC motor speed controller is probably a better solution.‎‎

‎Power and Signal Limits:‎

The IC that was the de facto standard for servo controls was the Signetics NE554. ‎This chip has a supply voltage of 3.2 - 6V, handily covered by 4x batteries - ‎‎(around 4.8 to 6V). What many people don’t realise is that the input for the control ‎signal is independent of the supply voltage, and it has a much lower threshold (of ‎typically 1.5V). In radio control, the servos are usually operated at the same ‎voltage as the receiver, and that is typically around 5V. When interfacing servos to ‎modern microcontrollers the servo performance may be limited by the supply ‎voltage required to run the controller – which can be around 3V. Fortunately, you ‎can supply the servo with 5V (via its +V and GND pins) and it will still respond to ‎control signals from a 3V microcontroller. Servos often specify a speed of ‎response – typically so many seconds to move 60 degrees (see figure 9 for an ‎extract of a typical spec sheet). 360-degree servos rarely specify a speed.‎

sheet_8

Figure 9 Extract from typical Futaba servo spec sheet‎

‎The speed of response is mostly a factor of the gearing, which is fixed by the ‎manufacturer, and the voltage. Often the ratings are given at 6V and 4.8V. Running ‎servos on a lower voltage will slow them down. This doesn’t usually matter for ‎most robotics projects but can be important for applications such as radio control ‎helicopters.‎

Conclusions:‎

RC servos are a simple way to add movement to many projects, and most of the ‎detail in this document is not required to use them. It is hoped the background ‎provided, however, may in future, make a difficult application simpler. ‎

By:

David Sanderson, MEng (hons) DIS, CEng MIMarEST Technical Director at ‎Kitronik‎ ‎

Download this guide as a PDF‎

Images used in this document sourced from:‎

Figure 1: a MeArm, photograph by Kitronik. Figure 2: Servo, photograph by Kitronik. ‎Figure 3: The Johnson Space Center Radio Control Club, photograph, viewed 28th ‎Feb 2019, http://www.jscrcc.com/images/history/picture_2.jpg Figure 4: Servo ‎pulse trains, diagram by Kitronik. Figure 5: Servo horn positions, diagram by ‎Kitronik. Figure 6: Servo positions related to pulse widths, diagram by Kitronik, ‎Figure 7: A 360-degree servo and wheel, photograph by Kitronik. Figure 8: ‎Commanded position vs speed of movement, diagram by Kitronik Figure 9: Extract ‎from typical Futaba servo spec sheet, screenshot of webpage, viewed 27th Feb ‎‎2019, https://www.futabarc.com/servos/analog.html

‎©Kitronik Ltd – You may print this page & link to it but must not copy the page or part thereof ‎without Kitronik's prior written consent.‎

Mfr Part # 2589
SERVOMOTOR RC 130 RPM 4.8-6V
Kitronik Ltd.
Mfr Part # SER0006
SERVOMOTOR RC 4.8V
DFRobot
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.