Maker.io main logo

SparkFun Indoor Air Quality Sensor - ENS160 (Qwiic) Hookup Guide

103

2023-03-14 | By SparkFun Electronics

License: See Original Project

Courtesy of SparkFun

Guide by ELL C

Introduction

The SparkFun Indoor Air Quality Sensor - ENS160 (Qwiic) makes use of the ENS160 from ‎ScioSense - a digital multi-gas sensor solution with four sensor elements that can be used in a wide ‎range of applications including building automation, smart home, and HVAC. The independent ‎hotplate control allows the detection of volatile organic compounds (VOCs) including ethanol, ‎toluene, hydrogen, and oxidizing gases with superior sensitivity. The ENS160 supports intelligent ‎algorithms to process raw sensor measurements on-chip. These algorithms calculate CO2-‎equivalents, TVOC, air quality indices (AQIs) and perform humidity and temperature compensation, ‎as well as baseline management, all on chip. Raw sensor measurements can be read for further ‎customization. Let's dig in!‎

SparkFun Indoor Air Quality Sensor - ENS160 (Qwiic)

 

Required Materials

To follow along with this tutorial, you will need the following materials. You may not need everything ‎though depending on what you have. Add it to your cart, read through the guide, and adjust the cart ‎as necessary.‎

SparkFun Indoor Air Quality Sensor - ENS160 (Qwiic) Hookup Guide Wish ‎List SparkFun Wish List

‎VIEW SPARKFUN INDOOR AIR QUALITY SENSOR - ENS160 (QWIIC) HOOKUP GUIDE ‎WISH LIST ON SPARKFUN.COM

Suggested Reading

If you aren't familiar with the Qwiic system, we recommend reading here for an overview.‎

qwiic_1

Qwiic Connect System

We would also recommend taking a look at the following tutorials if you aren't familiar with them.‎

  • Serial Terminal Basics: This tutorial will show you how to communicate with your serial devices ‎using a variety of terminal emulator applications.‎

  • How to Work with Jumper Pads and PCB Traces: Handling PCB jumper pads and ‎traces is an essential skill. Learn how to cut a PCB trace, add a solder jumper between pads to ‎reroute connections, and repair a trace with the green wire method if a trace is damaged.‎

  • RedBoard Qwiic Hookup Guide: This tutorial covers the basic functionality of the RedBoard ‎Qwiic. This tutorial also covers how to get started blinking an LED and using the Qwiic system.‎

Hardware Overview

ENS160 Digital Metal-Oxide Multi-Gas Sensor

The ENS160 from ScioSense is a digital multi-gas sensor consisting of four independent heaters ‎and gas sensor elements based on metal oxide (MOX) technology, and a controller. TrueVOC® air ‎quality detection provides outputs such as eCO2, TVOC, and AQI in compliance with worldwide IAQ ‎standards.‎

The ENS160 includes a standard 2-wire digital I2C interface (SCL, SDA) or 4-wire digital SPI ‎interface (SCLK, MOSI, MISO, CSn) for communication to the main host processor. For more ‎information, refer to the datasheet.‎

gas_2

Qwiic Connectors

Our Qwiic Ecosystem makes sensors pretty much plug and play. There are two Qwiic connectors ‎on either side of the Indoor Air Quality Sensor - ENS160 Sensor board to provide power and I2C ‎connectivity simultaneously.‎

connectors_3

Power

Ideally, power will be supplied via the Qwiic connectors on either side of the board. Alternatively, ‎power can be supplied through the header along the bottom side of the board labeled 3V3 and GND. ‎The ENS160 functions at 1.8V so an on-board regulator

VDD input range is 1.71-1.98V, VDDIO input range is 1.71-3.6V.‎

power_4

I2C Pins

The I2C pins break out the functionality of the Qwiic connectors. Depending on your application, ‎you can connect to these pins via the plated through holes for SDA and SCL.‎

pins_5

ADDR/POCI, Chip Select, and Interrupt Pins

The ADDR/POCI and Chip Select Pins are for use with SPI functionality. The interrupt pin is broken ‎out to use for triggered events.‎

addr_6

Power LED

When power is supplied to the board, this LED will light up.‎

led_7

Jumpers

I2C Jumper

Like our other Qwiic boards, the Indoor Air Quality Sensor comes equipped with pull-up resistors ‎on the clock and data pins. If you are daisy chaining multiple Qwiic devices, you will want to cut this ‎jumper; if multiple sensors are connected to the bus with the pull-up resistors enabled, the parallel ‎equivalent resistance will create too strong of a pull-up for the bus to operate correctly. As a ‎general rule of thumb, disable all but one pair of pull-up resistors if multiple devices are connected ‎to the bus. To disable the pull up resistors, use an X-acto knife to cut the joint between the two ‎jumper pads highlighted below.‎

jumper_8

Address Jumper

By default, the 7-bit un-shifted I2C address of the board is 0x53. However, by manipulating the ‎jumper on the back of the board, this address can be changed:‎

table_9

addrjumper_10

LED Jumper

If power consumption is an issue, cutting this jumper will disable the Power LED on the front of the ‎board.‎

ledjumper_11

Board Outline

Like most of our standard Qwiic boards, the SparkFun Indoor Air Quality Sensor - ENS160 ‎measures 1 inch by 1 inch.‎

Hardware Hookup

The delightful thing about our Qwiic System is that it makes hooking up your project as easy as plug ‎and play. Pop one end of your Qwiic connector into the controlling board and plug the other end of ‎your Qwiic connector into your Air Quality Sensor board! Voila!‎

hookup_12

Software

Note: Make sure you are using the latest stable version of the Arduino IDE on your desktop. If this ‎is your first time using Arduino, please review our tutorial on installing the Arduino IDE. If you have ‎not previously installed an Arduino library, please check out our installation guide.‎

SparkFun has written a library to work with the SparkFun Indoor Air Quality Sensor - ENS160 ‎‎(Qwiic). You can obtain this library through the Arduino Library Manager by searching for "ENS160". ‎Find the one written by SparkFun Electronics and install the latest version. If you prefer ‎downloading libraries manually, you can grab them from the GitHub Repository.‎

SPARKFUN INDOOR AIR QUALITY SENSOR-ENS160 ARDUINO LIBRARY GITHUB

Example 1: Basic Readings

Once the library is installed, go ahead, and open up File->Examples->SparkFun Indoor Air ‎Quality Sensor - ENS160->example1_basic. Make sure to select your board (SparkFun ‎RedBoard) and COM port before hitting upload to begin experimenting with the air quality sensor.‎

reading_13

Alternatively, you can copy and paste the code below to a shiny new Arduino file:‎

Copy Code
/* example1_basic.ino

 This example shows basic data retrieval from the SparkFun Indoor Air Quality Sensor - ENS160.

 Written by: 
    Elias Santistevan @ SparkFun Electronics October, 2022

 Product: 
  https://www.sparkfun.com/products/20844

 Repository:
    https://github.com/sparkfun/SparkFun_Indoor_Air_Quality_Sensor-ENS160_Arduino_Library

 SparkFun code, firmware, and software is released under the MIT
 License(http://opensource.org/licenses/MIT).

*/
#include <Wire.h>
#include "SparkFun_ENS160.h"

SparkFun_ENS160 myENS; 


void setup()
{
    Wire.begin();

    Serial.begin(115200);

    if( !myENS.begin() )
    {
        Serial.println("Did not begin.");
        while(1);
    }

    if( myENS.setOperatingMode(0xF0) )
        Serial.println("Ready.");

    delay(100);

    myENS.setOperatingMode(0x02);

    if( myENS.checkOperationMode() )
        Serial.println("Running.");

}

void loop()
{
    if( myENS.checkDataStatus() )
    {
        Serial.print("Air Quality Index (1-5) : ");
        Serial.println(myENS.getAQI());

        Serial.print("Total Volatile Organic Compounds: ");
        Serial.print(myENS.getTVOC());
        Serial.println("ppb");

        Serial.print("CO2 concentration: ");
        Serial.print(myENS.getECO2());
        Serial.println("ppm");
    }

    delay(200);
}

Once you've got your code uploaded, open up a Serial Monitor and check out your output. In the ‎example below, you can see where the board gave me baselines, then readings from my breath. ‎Maybe I should've held off on that peanut butter toast...‎

com_14

Example 2: Interrupts

Once the library is installed, go ahead, and open up File->Examples->SparkFun Indoor Air ‎Quality Sensor - ENS160->example2_interrupts. Make sure to select your board (SparkFun ‎RedBoard) and COM port before hitting upload to begin experimenting with the air quality sensor.‎

interrupts_15

Alternatively, you can copy and paste the code below into a nice new Arduino sketch:‎

Copy Code
/* example2_interrupts.ino

 This example shows how to configure interrupts for the SparkFun 
 Indoor Air Quality Sensor - ENS160.

 Written by: 
    Elias Santistevan @ SparkFun Electronics October, 2022

 Product: 
  https://www.sparkfun.com/products/20844

 Repository:
    https://github.com/sparkfun/SparkFun_Indoor_Air_Quality_Sensor-ENS160_Arduino_Library

 SparkFun code, firmware, and software is released under the MIT
 License(http://opensource.org/licenses/MIT).

*/
#include <Wire.h>
#include "SparkFun_ENS160.h"

SparkFun_ENS160 myENS; 

int ensInt = 2; 
int ensStatus; 

void setup()
{
    pinMode(ensInt, INPUT_PULLUP);

    Wire.begin();

    Serial.begin(115200);

    if( !myENS.begin() )
    {
        Serial.println("Did not begin.");
        while(1);
    }

    // Reset the indoor air quality sensor's settings.
    if( myENS.setOperatingMode(SFE_ENS160_RESET) )
        Serial.println("Ready.");

    delay(100);

    // Device needs to be set to idle to apply the following settings.
    myENS.setOperatingMode(SFE_ENS160_IDLE);

    //myENS.configureInterrupt(0x61); //If you want to do the following stuff but all at once.

    myENS.enableInterrupt();            // Enable physical interrupt.
    myENS.setDataInterrupt();           // Enable the data ready bit on the physical interrupt pin.
    //myENS.setInterruptPolarity(); // Changes interrupt from active low to active high.
    //myENS.setInterruptDrive();    //Changes interrupt from active low to push-pull.

    // Set to standard operation
    // Others args include SFE_ENS160_DEEP_SLEEP and SFE_ENS160_IDLE
    myENS.setOperatingMode(SFE_ENS160_STANDARD);

    delay(100);


    // There are four values here: 
    // 0 - Operating ok: Standard Opepration
    // 1 - Warm-up: occurs for 3 minutes after power-on.
    // 2 - Initial Start-up: Occurs for the first hour of operation.
  //                                                and only once in sensor's lifetime.
    // 3 - No Valid Output
    ensStatus = myENS.getFlags();
    Serial.print("Gas Sensor Status Flag: ");
    Serial.println(ensStatus);
}

void loop()
{
    if( digitalRead(ensInt) == LOW )
    {
        Serial.print("Air Quality Index (1-5): ");
        Serial.println(myENS.getAQI());

        Serial.print("Total Volatile Organic Compounds: ");
        Serial.print(myENS.getTVOC());
        Serial.println("ppb");

        Serial.print("CO2 concentration: ");
        Serial.print(myENS.getECO2());
        Serial.println("ppm");
    }

    delay(200);
}

Note that depending on which processor board you are using, you may need to alter the Interrupt ‎Pin. Since we're using a RedBoard here, our Interrupt Pin is 2 (ensInt = 2). Also, in this example, ‎we've soldered headers to our Air Quality Sensor so that we can use the interrupt pin. Your ‎hardware hookup should look something like the following:‎

board_16

Once you've got your code uploaded, open up a Serial Monitor and check out your output. You ‎should see something like the following:‎

serial_17

Example 3: Temp RH Compensation

This example shows how to give the ENS160 Temperature and Relative Humidity Data for ‎compensation. Note that the values that are given for compensation are not populated in their ‎registers until the Air Quality Sensor is set to "Standard" operation and when data is ready i.e., the ‎data ready bit is set. Also note that there will be some rounding of the temperature and relative ‎humidity values when they're given to the sensor and again when they're read back.‎

Go ahead and open up File->Examples->SparkFun Indoor Air Quality Sensor - ENS160-‎‎>example3_temp_rh_compensation. Make sure to select your board (SparkFun RedBoard) and ‎COM port before hitting upload to begin experimenting with the air quality sensor.‎

example3_18

Alternatively, you can copy and paste the code below into a nice new Arduino sketch:‎

Copy Code
/* example3_temp_rh_compensation.ino

 This example shows how to give the ENS160 Temperature and Relative Humidity
 Data for compensation. Note that the values that are given for compensation are not
 populated in their registers until the Air Quality Sensor is set to "Standard" operation
 and when data is ready i.e. the data ready bit is set. Also note that there will be some 
 rounding of the temperature and relative humidity values when they're given to the sensor
 and again when they're read back. 

 Written by: 
    Elias Santistevan @ SparkFun Electronics October, 2022

 Products: 
  Air Quality Sensor              -  https://www.sparkfun.com/products/20844
  Humidity and Temperature Sensor -  https://www.sparkfun.com/products/16467

 Repository:
    https://github.com/sparkfun/SparkFun_Indoor_Air_Quality_Sensor-ENS160_Arduino_Library

 SparkFun code, firmware, and software is released under the MIT
 License(http://opensource.org/licenses/MIT).

*/
#include <Wire.h>
#include "SparkFun_ENS160.h"
#include "SparkFun_SHTC3.h" // Click here to get the library: http://librarymanager/All#SparkFun_SHTC3

SHTC3 mySHTC3;              // Humidity and Temp Sensor.

SparkFun_ENS160 myENS; 

bool printedCompensation = false; 
int ensStatus; 

float rh;
float tempC; 
SHTC3_Status_TypeDef result; 


void setup()
{
    Wire.begin();

    Serial.begin(115200);

    if( !myENS.begin() )
    {
        Serial.println("Air Quality Sensor did not begin.");
        while(1);
    }

    if( mySHTC3.begin() != SHTC3_Status_Nominal )
    {
        Serial.println("Humidity and Temperature Sensor did not begin.");
        while(1);
    }

    // Reset the indoor air quality sensor's settings.
    if( myENS.setOperatingMode(SFE_ENS160_RESET) )
        Serial.println("Ready.");

    delay(100);

    // Device needs to be set to idle to apply any settings.
    myENS.setOperatingMode(SFE_ENS160_IDLE);

    mySHTC3.update(); // Send command to take a measurement
    if( mySHTC3.lastStatus != SHTC3_Status_Nominal )
    {
        Serial.println("Humidity and Temperature Sensor is not ready.");
        while(1);
    }

    rh = mySHTC3.toPercent();
    tempC = mySHTC3.toDegC();
    Serial.print("Relative Humidity: ");
    Serial.println(rh);
    Serial.print("Temperature(Celsius): ");
    Serial.println(tempC);

    // Give values to Air Quality Sensor. 
    myENS.setTempCompensationCelsius(tempC); 
    myENS.setRHCompensationFloat(rh); 

    delay(500);

    // Set to standard operation
    // Others include SFE_ENS160_DEEP_SLEEP and SFE_ENS160_IDLE
    myENS.setOperatingMode(SFE_ENS160_STANDARD);

    // There are four values here: 
    // 0 - Operating ok: Standard Opepration
    // 1 - Warm-up: occurs for 3 minutes after power-on.
    // 2 - Initial Start-up: Occurs for the first hour of operation.
  //                                                and only once in sensor's lifetime.
    // 3 - No Valid Output
    ensStatus = myENS.getFlags();
    Serial.print("Gas Sensor Status Flag: ");
    Serial.println(ensStatus);

}

void loop()
{
    if( myENS.checkDataStatus() )
    {

        if( printedCompensation == false)
        {
            Serial.println("---------------------------");
            Serial.print("Compensation Temperature: ");
            Serial.println(myENS.getTempCelsius());
            Serial.println("---------------------------");
            Serial.print("Compensation Relative Humidity: ");
            Serial.println(myENS.getRH());
            Serial.println("---------------------------");
            printedCompensation = true;
            delay(500);
        }

        Serial.print("Air Quality Index (1-5) : ");
        Serial.println(myENS.getAQI());

        Serial.print("Total Volatile Organic Compounds: ");
        Serial.print(myENS.getTVOC());
        Serial.println("ppb");

        Serial.print("CO2 concentration: ");
        Serial.print(myENS.getECO2());
        Serial.println("ppm");

    }

    delay(200);
}

Your hardware hookup should look something like the following:‎

hardware_19

Once you've got your code uploaded, open up a Serial Monitor and check out your output. You ‎should see something like the following:‎

output_20

Example 4: Basic SPI

This example shows basic data retrieval from the SparkFun Indoor Air Quality Sensor - ENS160 ‎using SPI.‎

Go ahead and open up File->Examples->SparkFun Indoor Air Quality Sensor – ENS160-‎‎>example4_basic_spi. Make sure to select your board (SparkFun RedBoard) and COM port ‎before hitting upload to begin experimenting with the air quality sensor.‎

file_21

Alternatively, you can copy and paste the code below into a nice new Arduino sketch:‎

Copy Code
/* example4_basic_example_spi.ino

 This example shows basic data retrieval from the SparkFun Indoor Air Quality Sensor - ENS160 using SPI.

 Written by: 
    Elias Santistevan @ SparkFun Electronics October, 2022

 Product: 
  https://www.sparkfun.com/products/20844

 Repository:
    https://github.com/sparkfun/SparkFun_Indoor_Air_Quality_Sensor-ENS160_Arduino_Library

 SparkFun code, firmware, and software is released under the MIT
 License(http://opensource.org/licenses/MIT).

*/
#include <SPI.h>
#include "SparkFun_ENS160.h"

SparkFun_ENS160_SPI myENS; 

// Adjust pin select to suit your project's needs.
int chipSelect = 1; 
int ensStatus = 0; 

void setup()
{

    pinMode(chipSelect, OUTPUT);
    digitalWrite(chipSelect, HIGH);

    SPI.begin();

    Serial.begin(115200);

    if( !myENS.begin(chipSelect) )
    {
        Serial.println("Did not begin.");
        while(1);
    }

    // Reset the indoor air quality sensor's settings.
    if( myENS.setOperatingMode(SFE_ENS160_RESET) )
        Serial.println("Ready.");

    delay(100);

    // Device needs to be set to idle to apply any settings.
  //    myENS.setOperatingMode(SFE_ENS160_IDLE);


    // Set to standard operation
    // Others include SFE_ENS160_DEEP_SLEEP and SFE_ENS160_IDLE
    myENS.setOperatingMode(SFE_ENS160_STANDARD);
    Serial.print("Operating Mode: ");
    Serial.println(myENS.getOperatingMode());

    // There are four values here: 
    // 0 - Operating ok: Standard Opepration
    // 1 - Warm-up: occurs for 3 minutes after power-on.
    // 2 - Initial Start-up: Occurs for the first hour of operation.
  //                                                and only once in sensor's lifetime.
    // 3 - No Valid Output
    ensStatus = myENS.getFlags();
    Serial.print("Gas Sensor Status Flag: ");
    Serial.println(ensStatus);
}

void loop()
{
    if( myENS.checkDataStatus() )
    {
        Serial.print("Air Quality Index (1-5) : ");
        Serial.println(myENS.getAQI());

        Serial.print("Total Volatile Organic Compounds: ");
        Serial.print(myENS.getTVOC());
        Serial.println("ppb");

        Serial.print("CO2 concentration: ");
        Serial.print(myENS.getECO2());
        Serial.println("ppm");
    }

    delay(200);
}

Hookup for this example is a bit more complicated.‎

complicted_22

Let's sort through all those wires:‎

table_23

So! Everything is hooked up and you've got your code uploaded - now you can open up a Serial ‎Monitor and check out your output. You should see something like the following:‎

see_24

Troubleshooting

Need help? ‎

If your product is not working as you expected or you need technical assistance or information, ‎head on over to the SparkFun Technical Assistance page for some initial troubleshooting. ‎

If you don't find what you need there, the SparkFun Forums are a great place to find and ask for ‎help. If this is your first visit, you'll need to create a Forum Account to search product forums and ‎post questions.

Resources and Going Further

Now that you've successfully got your SparkFun Indoor Air Quality Sensor - ENS160 (Qwiic) up and ‎running, it's time to incorporate it into your own project!‎

For more information, check out the resources below:

Mfr Part # 20844
SPARKFUN INDOOR AIR QUALITY SENS
SparkFun Electronics
£21.16
View More Details
Mfr Part # 16467
HUMIDITY SENSOR BREAKOUT - SHTC3
SparkFun Electronics
Mfr Part # 15123
REDBOARD QWIIC ATMEGA328 EVAL BD
SparkFun Electronics
£16.26
View More Details
Mfr Part # 10215
USB MICRO-B CABLE - 6 FOOT
SparkFun Electronics
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.