Maker.io main logo

Roller Mill Remote Scale Display

11

2021-07-10 | By M5Stack

License: General Public License Arduino

* Thanks for the source code and project information provided by @Eathan Rethmeier

 

Story
 

 

 
 
 
 
 
 
Code
 
Copy Code
//5_14_2021
//Smart Scale

//todo list
#include <Adafruit_GFX.h>
#include <Adafruit_NeoMatrix.h>
#include <Adafruit_NeoPixel.h>
#include "M5Atom.h"

// Fields
uint8_t res;
//const char* ssid = "";
//const char* password = "";
//const char* hostname = "";
//const byte DNS_PORT = 53;
//IPAddress apIP( 192, 168, 4, 1 );
//DNSServer dnsServer;

//User defined stored data
int Scale_Type = 1;
int Scale_Color = 0;
String ch = "";

//neopixel pin designation
#define PIN 26

// MATRIX DECLARATION:
// Parameter 1 = width of NeoPixel matrix
// Parameter 2 = height of matrix
// Parameter 3 = pin number (most are valid)
// Parameter 4 = matrix layout flags, add together as needed:
// NEO_MATRIX_TOP, NEO_MATRIX_BOTTOM, NEO_MATRIX_LEFT, NEO_MATRIX_RIGHT:
// Position of the FIRST LED in the matrix; pick two, e.g.
// NEO_MATRIX_TOP + NEO_MATRIX_LEFT for the top-left corner.
// NEO_MATRIX_ROWS, NEO_MATRIX_COLUMNS: LEDs are arranged in horizontal
// rows or in vertical columns, respectively; pick one or the other.
// NEO_MATRIX_PROGRESSIVE, NEO_MATRIX_ZIGZAG: all rows/columns proceed
// in the same order, or alternate lines reverse direction; pick one.
// See example below for these values in action.
// Parameter 5 = pixel type flags, add together as needed:
// NEO_KHZ800 800 KHz bitstream (most NeoPixel products w/WS2812 LEDs)
// NEO_KHZ400 400 KHz (classic 'v1' (not v2) FLORA pixels, WS2811 drivers)
// NEO_GRB Pixels are wired for GRB bitstream (most NeoPixel products)
// NEO_GRBW Pixels are wired for GRBW bitstream (RGB+W NeoPixel products)
// NEO_RGB Pixels are wired for RGB bitstream (v1 FLORA pixels, not v2)


// Example for NeoPixel Shield. In this application we'd like to use it
// as a 5x8 tall matrix, with the USB port positioned at the top of the
// Arduino. When held that way, the first pixel is at the top right, and
// lines are arranged in columns, progressive order. The shield uses
// 800 KHz (v2) pixels that expect GRB color data.
Adafruit_NeoMatrix matrix = Adafruit_NeoMatrix(29, 8, PIN,
NEO_MATRIX_TOP + NEO_MATRIX_LEFT +
NEO_MATRIX_ROWS + NEO_MATRIX_ZIGZAG,
NEO_RGB + NEO_KHZ800);

const uint16_t colors[] = {
matrix.Color(255, 0, 0), matrix.Color(0, 255, 0), matrix.Color(0, 255, 0) };

//uint16_t Serial_Output;

void setup() {

M5.begin();
// Serial2.begin(unsigned long baud, uint32_t config, int8_t rxPin, int8_t txPin, bool invert)
Serial2.begin(9600, SERIAL_8N1, 22, 19);
//Serial2.begin(9600, 22, 19);
//
// #if defined(ESP32)
// WiFi.setHostname( hostname );
//#else
// WiFi.hostname( hostname );
//#endif
//
// // try to connect to existing network
// WiFi.begin( ssid, password );
// Serial.print(F( "\n\nTry to connect to existing network") );
//
// {
// uint8_t timeout = 20;
//
// // Wait for connection, 5s timeout
// do {
// delay( 500 );
// Serial.print( "." );
// timeout--;
// } while ( timeout && WiFi.status() != WL_CONNECTED );
//
// // not connected -> create hotspot
// if ( WiFi.status() != WL_CONNECTED ) {
// Serial.print( F("\n\nCreating hotspot") );
//
// WiFi.mode( WIFI_AP );
// WiFi.softAPConfig( apIP, apIP, IPAddress( 255, 255, 255, 0 ) );
// WiFi.softAP( "ScaleDisplay");
//
// timeout = 5;
//
// do {
// delay( 500 );
// Serial.print( "." );
// timeout--;
// } while ( timeout );
// }
// }
//
// dnsServer.start( DNS_PORT, "*", apIP );
//
// /////
// Serial.println( "\n\nWiFi parameters:" );
// Serial.print( "Mode: " );
// Serial.println( WiFi.getMode() == WIFI_AP ? "Station" : "Client" );
// Serial.print( "IP address: " );
// Serial.println( WiFi.getMode() == WIFI_AP ? WiFi.softAPIP() : WiFi.localIP() );
//
//
// uint16_t tab1 = ESPUI.addControl( ControlType::Tab, "Settings 1", "Scale" );
// uint16_t tab2 = ESPUI.addControl( ControlType::Tab, "Settings 2", "Settings" );
//
//Serial_Output =ESPUI.addControl( ControlType::Label, "Scale", "", ControlColor::Turquoise, tab1 );
//
//
//
// ESPUI.begin("Scale");
// // put your setup code here, to run once:
//matrix.setTextColor(matrix.Color(7,0,0));
matrix.setBrightness(64);
}

//
int x= matrix.width();
int pass = 0;

//

void loop() {
// put your main code here, to run repeatedly:
//dnsServer.processNextRequest();
if(Serial2.available()) {
{
//ch = Serial2.readStringUntil((''));
ch = Serial2.parseInt();
//ch.trim();
// Serial.print(ch);
// Serial.flush();
// ESPUI.updateControlValue(Serial_Output, ch);
//M5.dis.drawpix(0, 0x00ffff);
M5.update();
delay(50);
//LED Matrix update
matrix.fillScreen(0);
matrix.setCursor(0, 0);
matrix.setTextColor(colors[pass]);
matrix.print(ch);
matrix.show();

delay(100);
}
}
}
Mfr Part # A093
DIGITAL RGB LED WEATHERPROOF STR
M5Stack Technology Co., Ltd.
Mfr Part # A093-B
DIGITAL RGB LED WEATHERPROOF STR
M5Stack Technology Co., Ltd.
Mfr Part # A093-C
DIGITAL RGB LED WEATHERPROOF STR
M5Stack Technology Co., Ltd.
£10.74
View More Details
Mfr Part # A093-D
DIGITAL RGB LED WEATHERPROOF STR
M5Stack Technology Co., Ltd.
£22.60
View More Details
Mfr Part # K046
ATOM RS232 KIT
M5Stack Technology Co., Ltd.
£12.56
View More Details
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.