Maker.io main logo

Pico Drawing Robot Arm Code Explanation

86

2023-11-30 | By Kitronik Maker

License: See Original Project

Courtesy of Kitronik

Guide by Kitronik Maker

drawing_1

Overview

The biggest challenge behind making the Cardboard and Advanced drawing robot ‎arms was figuring out how to move the arm to a specific position. This is needed ‎so that we can use the line coordinates from our vectorised images to move the ‎robot arm and draw the image. We need some way of converting the x, y ‎coordinates into angles that we can use to set the shoulder servo and elbow servo.‎

The DrawingRobot library can be found on our GitHub repo.‎

The blogs in this series are:‎

  1. Making a Cardboard Pico Drawing Robot Arm
  2. Making an Advanced Pico Drawing Robot Arm
  3. Pico Drawing Robot Arm Code Explanation

Pico Drawing Robot Arm Theory

Below is a diagram that shows the idea behind the drawing robot arm. We'll use the ‎shoulder and elbow arm lengths from the CAD based drawing robot making them ‎both 160 millimeters. We can imagine the shoulder servo is at point 0, 0 and we ‎want our pen to be at 160, 80. The coordinates, like the arm lengths, are going to ‎be in millimeters. To put the pen at 160, 80 the elbow servo will have to be at some ‎x coordinate near the middle of the shoulder, but we don't actually need to know the ‎exact coordinates of the elbow. We can't just tell the servos to move to these ‎coordinates as they have no meaning to our servos. Instead, we must calculate ‎what angles the shoulder and elbow servos need to be at to position the pen at ‎point 160, 80.‎

calculate_2

We are going to be calculating the angles for our servos in radians before ‎converting them to degrees. We will use radians for the calculations as the Python ‎Math module returns values in radians for the angle related functions we are going ‎to use. We then need to convert these angles from radians to degrees as our servo ‎code sets the positions of the servos using angles in degrees.‎‎ ‎

Radians are a measurement of angles inside of a circle based on the radius of the ‎circle. The measurement of the angle around half of a circle, or 180 degrees, in ‎radians is PI. This is what allows us to calculate the circumference of a circle ‎using the diameter times PI, as the diameter of a circle is 2 times its radius. To ‎convert an angle from radians to degrees we multiply the angle by 180 and divide ‎by PI.‎‎

‎To calculate our angles, we need to start by imagining an invisible side between ‎the pen and shoulder servo to create a triangle between our two servos and the pen. ‎Then we need to calculate the length of the invisible side using Pythagoras ‎Theorem with the x, y coordinates. For our example of moving the pen to 160, 80 ‎this will give the invisible side a length of 178.8854. This is done by square rooting ‎the sum of 1602 and 802:‎

‎√ x2 + y2‎

length_3

Now that we have a triangle where we know the length of all three sides, we can ‎use the law of cosines to calculate our inner and outer angles which will be used ‎when setting the shoulder and elbow servos.‎‎ ‎

For the inner angle we know that the cosine of the inner angle is equal to:‎

‎(shoulderLength2 + invisibleLength2 - elbowLength2) / (2 * ‎shoulderLength + inisibleLength)‎

This gives us 0.559017. When we then rearrange the formula to find the inner ‎angle, we find that the arc cosine of 0.559017 is equal to the inner angle in radians ‎which is 0.9775965.‎‎ ‎

For the outer angle we perform the same set of calculations with different values. ‎Instead, we know the cosine of the outer angle is equal to:‎

‎(elbowLength2 + shoulderLength2 - invisibleLength2) / (2 * elbowLength + ‎shoulderLength)‎

This gives us 0.375. When we then rearrange the formula to find the outer angle, ‎we find that the arc cosine of 0.375 is equal to the outer angle in radians which is ‎‎1.1864.‎

angle_4

To set the shoulder servo to the correct angle we also need to calculate the gap ‎angle between the invisible side and our base. We can then add this gap angle to ‎our inner angle to get full angle between the shoulder arm and base. To find the ‎gap angle we convert the rectangular coordinates into polar coordinates using the ‎inverse tangent function.‎‎ ‎

Polar coordinates are used to represent a coordinate using an angle from the base ‎along with the distance between the base point and the coordinate. We can use ‎polar coordinates to determine the angle between the invisible side and our base. ‎We have already calculated the distance between our shoulder servo and the point ‎we're moving our pen to using Pythagoras Theorem. Now we can find our gap ‎angle which is equal to the arc tangent of 80 / 160 giving us an angle of 0.4636476 ‎in radians.‎

atan(y / x)

collected_5

We have now collected all the information we need to calculate the angles our ‎shoulder and elbow servos need to be positioned at to move the pen to 160, 80. For ‎our shoulder servo we can find the angle it needs to be at by adding the inner angle ‎to the gap angle giving us 1.4412441 in radians. Then we can convert this to ‎degrees which gives us a shoulder servo angle of 82.5772. For our elbow servo we ‎can find the angle it needs to be at by minusing the outer angle from PI giving us ‎‎1.9551 in radians. We use PI here to calculate our angle backwards from 180 ‎degrees. Setting our elbow servo to 180 degrees positions it to face back at the ‎shoulder servo and the calculation we did for our outer angle is from the shoulder ‎to the pen. We can again convert our angle to degrees which gives us an elbow ‎servo angle of 112.0243.‎

convert_6

Pico Drawing Robot Arm Code

Now let's see how we can use this idea to convert an x, y coordinate to the angles ‎for our servos. We define a function called plot that takes the two x, y coordinate ‎values as its inputs. We then offset these x and y values using variables we setup ‎earlier in our DrawingRobot library. These offsets stop the robot arm from drawing ‎too close to the base of the arm. Then using the x and y values we apply ‎Pythagoras Theorem to calculate the length of our invisible side and store it in ‎the lenHypot variable. Next, we want to check if the length of the invisible side is ‎longer than the length of our two arms, as this would be out of reach of our robot.‎

Copy Code
def plot(self, x, y):
x += self.xOffset
y += self.yOffset
lenHypot = sqrt(x ** 2 + y ** 2)

if lenHypot > self.shoulderLength + self.elbowLength:
return 0, 0

Our next step is to use the law of cosines to calculate our inner and outer angles ‎using the three side lengths of our triangle. This uses the math ‎module's acos function which is used to find the arc cosine of a number.‎

Copy Code
angleInner = acos((self.shoulderLength ** 2 + lenHypot ** 2 - self.elbowLength ** 2)
/ (2 * self.shoulderLength * lenHypot))
angleOuter = acos((self.elbowLength ** 2 + self.shoulderLength ** 2 - lenHypot ** 2)
/ (2 * self.elbowLength * self.shoulderLength))

With the two angles inside of our triangle calculated, we need to find the gap angle ‎using polar coordinates. This is done using the math module's arc tangent of y ‎over x, returning the angle in radians.‎

Copy Code
angleGap = atan2(y, x)

Finally, we convert our angles into degrees for both the shoulder angle and elbow ‎angle before returning these angles. We can then use the returned angles to ‎gradually move the shoulder and elbow servos into these positions. When they ‎reach these positions, the pen will be at the coordinates x and y.‎

Copy Code
shoulderAngle = degrees(angleInner + angleGap)
elbowAngle = degrees(pi - angleOuter)

return shoulderAngle, elbowAngle

Below is the full code snippet for converting the x, y coordinates to the angles used ‎by the shoulder and elbow servos.‎

Copy Code
# Convert an x, y coordinate into shoulder and elbow servo angles
def plot(self, x, y):
# Offset the x and y coordinates
x += self.xOffset
y += self.yOffset
# Calculate the length of the invisible side
lenHypot = sqrt(x ** 2 + y ** 2)

# Stop if the coordinate is too far to reach
if lenHypot > self.shoulderLength + self.elbowLength:
return 0, 0

# Calculate the angles inside the triangle for the shoulder and elbow
angleInner = acos((self.shoulderLength ** 2 + lenHypot ** 2 - self.elbowLength ** 2)
/ (2 * self.shoulderLength * lenHypot))
angleOuter = acos((self.elbowLength ** 2 + self.shoulderLength ** 2 - lenHypot ** 2)
/ (2 * self.elbowLength * self.shoulderLength))
# Calculate the angle of the gap between the base and start of the triangle
angleGap = atan2(y, x)

# Convert the angles from radians to degrees
shoulderAngle = degrees(angleInner + angleGap)
elbowAngle = degrees(pi - angleOuter)

return shoulderAngle, elbowAngle

‎‎With the plot function complete we can then use it to move our pen to an x, y ‎coordinate. We could just tell our servos to move the angles returned by plot, but ‎this would cause our robot arm to jolt into position and wouldn't create a very ‎precise line. Instead we use the moveTo function, full code on our GitHub, to ‎gradually move the servos to the positions we need in small steps.‎‎ ‎

We do this by calculating the difference between the current servo angles and the ‎desired servo angles. Using this, we then divide the angle differences by the ‎maximum difference times 4 to create the steps we'll use to move the servos. This ‎makes sure both servos make little adjustments to their angles over time to move ‎to their new positions. With our steps defined, the moveTo function then ‎continuously moves the servos by our steps until the servos are less than one step ‎away from their desired position. At this point, the difference between the angles is ‎so small that we just set the servo angles to the new position, completing the move ‎of the pen to the x, y coordinate.‎‎ ‎

With our moveTo function also complete, the rest of our DrawingRobot functions ‎now make use of moveTo to move the robot arm and draw on our paper. ‎The moveTo function is used in conjunction with the penUp and penDown functions ‎to lift the pen up from the paper which stops it from drawing and push the pen down ‎on to the paper which allows it to draw. The drawImage function simply retrieves ‎the line coordinates from the text file and moves the pen to each of the coordinates ‎on the line. It then makes use of the penUp and penDown functions to lift the pen ‎up between drawing lines and push the pen down when drawing a line.‎

‎©Kitronik Ltd – You may print this page & link to it but must not copy the page or part thereof ‎without Kitronik's prior written consent.‎

Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.