Maker.io main logo

I Invented Chow Check to Help My Friend

2024-03-08 | By Zach Hipps

License: See Original Project 3D Printing Wifi ESP32

Recently, my friend got a new dog, and he's been having a hard time remembering whether or ‎not he feeds the dog throughout the day. Because he's a maker, he wanted to design and build a ‎device that would help remind him whether or not he feeds his dog.

dog_1

The thing I like about this project is that it doesn't have to be specific to feeding your dog. This ‎little device could help you remember to do anything three times a day. Whether that's watering ‎your plants, getting up to stretch, taking a walk, or maybe taking medication. This could be ‎customized to fit any need.‎

 

case_2

He got started on this project and has a really solid foundation, but he asked for my help, so I ‎stepped in to help him build this project.‎

design_3

These are his design requirements:

  • Push buttons that have an RGB-illuminated LED
  • One button for breakfast, one button for lunch, and one button for dinner
  • The three buttons will remind him to feed his dog three times during the day, 7 ‎a.m., 1 p.m., and 6 p.m.
  • At the set times to feed his dog, the appropriate light turns blue. If he hasn't fed ‎the dog yet and it's been more than 15 minutes after the set times, the light turns ‎red. As soon as he feeds the dog, he can push the button and it turns green, and ‎that tells him and his whole family that the dog has been fed. The same scenario ‎happens at 1 p.m. and 6 p.m.
  • Wife approval - so I can't have this thing strung out on a breadboard
  • Must be internet-connected

buttons_4

light_5

I'll use a Wi-Fi-enabled microcontroller and connect it to the Telegram messaging app. Any time ‎the light turns red, meaning that it's been too long, and the dog has not been fed, it will send him ‎a Telegram message. I need to design a minimal and nice-looking case for this that everything ‎will fit into, and it will sit on their kitchen counter and not look too distracting. As I'm thinking about ‎this design off the top of my head, I'm kind of worried about how much wiring there's going to be. ‎I think I'll design a circuit board that everything will connect to, and it will take care of the rat's ‎nest of wires that I want to avoid. I'll start by drawing this circuit on a computer and designing the ‎PCB. The first thing I need to do is add the microcontroller. I will use the ESP32 feather board ‎from Adafruit. I find the symbol for that and add it to the schematic. ‎

schematic_6

Next, I need to create a symbol for that LED push button. It doesn’t exist in the library, so I'll have ‎to make it from scratch. I'll take an existing push button that has an LED in it and just modify that ‎symbol to have a red, green, and blue LED. These RGB LEDs are common cathode. I can tie ‎each LED cathode to ground and the anode to one of the pins on the push button. I add a ‎current-limiting resistor to each of the LEDs and then I give them a net name that I can tie to the ‎microcontroller.‎

symbol_7

On the microcontroller side, I just need to assign each of these net names open so that I can ‎control them individually. Finally, I asked my friend if he wanted this to make any sounds. He ‎said, “Absolutely not!” (He doesn't want it to be annoying, but I think I'm going to sneak a little ‎buzzer in here just in case at some point, he decides he wants to add a little bit of sound to this ‎project.) One of the nice things about designing a PCB is that it doesn't cost extra to add ‎footprints. When I go to build this board, I don't have to place that buzzer component on there. I ‎can just leave the footprint blank. That's pretty much it for the schematic. I can assign footprints ‎to all of these symbols and then design the board layout.‎

I lay all three buttons in a horizontal configuration, and I quickly decided that I didn't like that ‎design and that a vertical orientation would look a lot better. So instead, I'll place the footprints for ‎my buttons in a vertical layout, and then I add the current limiting resistors to each of those LEDs, ‎and then finally I connect the microcontroller pins to their proper inputs and outputs.‎

configure_8

Before I can design the board outline, I need to know what my mechanical enclosure is going to ‎look like. I open up Fusion 360 and start modeling the enclosure with a simple box. Next, I use ‎the fillet tool to give it some rounded edges. I know that we want the enclosure to sit at an angle, ‎so I use the chamfer tool to create a 45-degree angle on the bottom. Once I have those features, ‎I use the shell tool to hollow out the box so that I can fit all the stuff inside of it.‎

enclose_9

The enclosure with all of the electronics will be 3D printed while the base plate and the faceplate ‎will be cut out of metal. My friend and I discussed different ways to make sure this little device ‎doesn't slide around. We came up with the idea of just using a heavy metal plate as the base. I ‎ordered them from an online service, and hopefully, the weight of the plate will be enough to ‎keep this thing from sliding around on the counter. I add some holes into the design so that I can ‎screw these pieces together.‎

Next comes the faceplate. I use the same spacing that I used on the circuit board design to ‎create three holes for the faceplate, and that's where the buttons will be inserted. I fiddled with ‎this for a couple of hours, adding some minor details here and there and adjusting a few things, ‎and I'm pretty happy with how it looks.‎

face_10

At this point, I'm ready to order my PCB, the laser-cut parts, and electronic components and ‎print the 3D-printed parts here in my workshop.‎

I used a carbon fiber filament, and this thing turned out perfect. Look how flawless that looks! ‎While I wait for the circuit board and the laser cut parts to arrive, I 3D print some mock-up pieces ‎out of plastic, and I’ll use those to assemble this and do a dry run.‎

filament_11

There’s a big downside to this design; these buttons have to be soldered to a PCB, but before I ‎can do that, they have to slide through the faceplate. Once I slide these buttons through the ‎faceplate and solder them onto the PCB, this becomes a permanent subassembly. There's no ‎way to remove them from the faceplate without desoldering them from the PCB. I knew that ‎going into it, but that's a tradeoff that I'm willing to make.‎

downside_12

All the parts that I ordered arrived, and I'm excited to start assembling this. I’m also excited to try ‎something new for the front face panel. I ordered some aluminum composite material; as the ‎name suggests, it's a composite material. The center of it is a high-density plastic, and the outer ‎two skins are made from a thin sheet of aluminum. The reason I chose black aluminum ‎composite material is because I want to laser engrave a logo as well, as some labels on this face ‎plate.‎

panel_13

To engrave this faceplate, I use a CO2 laser cutter. This laser cutter has a built-in camera to help ‎align things, but if I want to get the text to align perfectly with these holes, I'm going to have to ‎use a little bit of a trick. The first thing I do is put a piece of cardboard into the laser cutter. Then, I ‎open up my design in the laser software and I make sure I add an outline just a little bit bigger ‎than the outline of the faceplate. I’ll put that outline on a separate layer and cut it out of the ‎cardboard just on its own. Now, I can place the faceplate inside that cutout, and all of the other ‎engraving that takes place on the other layers will line up perfectly.‎

engrave_14

engrave_15

My friend with the dog came up with the name “Chow Check” for this product, and he even ‎designed a little logo that I'm laser engraving on the faceplate. This engraving is way better than I ‎expected so I will definitely use this process in the future.‎

logo_16

As I said earlier, I have to install the buttons through the faceplate and then solder them to the ‎PCB, and this becomes a permanent subassembly. I have to do this step now before it is too late. ‎If I assemble everything first and then try to engrave it, it won't work. This is one of those things ‎that I'm spending a little extra time on to make sure I get correct because if I do this wrong, this ‎part is basically scrapped, and I have to start over again.‎

solder_17

solder_18

Do you remember earlier when I talked about one of the requirements being that this thing ‎doesn't slide around too much? My solution to that was to build a really heavy baseplate. I chose ‎a quarter-inch steel plate as the material, but I wonder how much more the baseplate weighs ‎than the enclosure and the electronics. I put the enclosure and the electronics on a scale, and it ‎looks like they weigh about 86 grams (3 oz.). If I put the baseplate on there, I see that it weighs ‎‎164 grams (5.8 oz). That's roughly twice as much! When I attach the baseplate to the bottom of ‎the enclosure, that weight should be more than enough to keep it from sliding around too much.‎

baseplate_19

baseplate_20

baseplate_21

With all of these components under the board, I'm ready to program this project. I have the ‎Arduino IDE open, and I start by defining which GPIO pins I need. Each button has a switch as ‎well as a red, green, and blue LED pin. I can always refer back to the schematic to remember ‎which pins I assigned to each. Next, I use the pinMode() function to set the switches as inputs ‎and the LED pins as outputs. In the main loop, I pretty much have two tasks… 1) I want to ‎structure this in a way where I assign the colors to each of the buttons, and 2) I use a custom ‎function to actually set the colors on the buttons. I make sure not to use any delays in the main ‎function because I want to continuously assign and set these LEDs. I need to write some ‎conditions to set the color either to red or to blue, so I write an “if statement” and check to see if ‎the current time is greater than the task time plus my 15-minute grace period. If that condition is ‎met, then I assign the color red. Otherwise, the code checks to see if the current time is later ‎than the task time, and if so, I'll set the color as blue. It's always good to have a default condition. ‎If no other conditions are met, I'll assign the color black, which just means that the LEDs will be ‎turned off. Of course, I'll do this for all three buttons.‎

program_22

program_23 ‎ ‎

When the current time reaches midnight, I want everything to reset and turn the LEDs off. To ‎read the button presses, I use an interrupt service routine, as I do with all electromechanical ‎switches. I take care of bouncing within that interrupt service routine by checking to see if it's ‎been long enough for the bouncing to have stopped. If so, I set the color to green.‎

One nice thing about using a Wi-Fi microcontroller is that I can get the current time using an NTP ‎‎(Network Time Protocol) server, and I want to make sure that I'm updating that as often as I can ‎in the main loop.‎

A lot of this is pseudocode, and it's not fully fleshed out, but this is the general idea of how this ‎code works. To begin, all three buttons are turned off. After a few moments, the light will turn ‎blue because it will be time to feed Luna breakfast. Now, if my friend Jonathan is passing by and ‎he happens to see that the light has turned blue, he can go feed the dog and push the button, and ‎the button will turn green, indicating that the dog has been fed. Let's say one of his kids comes ‎by and pushes the button without actually feeding the dog; each button can be reset to their ‎previous state by holding it down for 3 seconds. But what happens if Jonathan doesn't walk past ‎and see that it's time to feed the dog? After 15 minutes, the light will turn red, and Jonathan will ‎get a telegram message sent to him, reminding him to feed Luna lunch. Then, if he feeds the dog, ‎he presses the button, and it still turns green.‎

green_23

green_24

push_30

red_25

red_26

However, the telegram interface doesn't stop there. If I want to change any of the settings for the ‎buttons, all I do is type in /settings, and a little menu pops up. I can choose which of the three ‎tasks I want to edit. For example, let's say I want to edit the lunchtime. Instead of feeding Luna at ‎‎1:00 p.m., let's say I want to feed her at 1:30 p.m. All I have to do is reply to the message and ‎type in “13:30” (24-hour time), and it replies, letting me know that the time has been changed. ‎Remember earlier how I held down the button to reset it back to its previous state? I can do the ‎same things right here in the app. I can choose “reset feed Luna lunch” and the LED will change ‎from green back to its previous state.‎

settings_26

settings_27

What I like about this project is that it doesn't have to be used to remind you to feed a dog. It can ‎be used to remind you to do other tasks. I'm still working on the code, but the next feature I want ‎to add is being able to edit the task label, so instead of saying “Feed Luna,” it can say, “Go ‎outside and take a walk.”‎‎

If you're interested in building a task reminder like this, all of the source files will be available on ‎my GitHub.

Mfr Part # 5345
ESP32-S2 REVERSE TFT FEATHER
Adafruit Industries LLC
£18.55
View More Details
Mfr Part # BH16NBBBRGB
SWITCH PB SPST 1A 125VAC
CIT Relay and Switch
£14.92
View More Details
Mfr Part # PKMCS0909E4000-R1
BUZZER PIEZO 9X9MM SMD
Murata Electronics
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.