Maker.io main logo

How to Make Simplest Possible Autorange Capacitance Meter

233

2024-05-24 | By Mirko Pavleski

License: General Public License Capacitors Arduino

The capacity measurement option is usually only available in more expensive multimeters, so it is desirable to make such an instrument ourselves, especially if it is very simple to make and inexpensive.

 

Exactly these conditions are fulfilled in the instrument described below. The measured value is displayed on a large readable display, and its measuring range is from 1 pF to 99 µF which are actually the most frequently used values. The fact that only two components are needed to make this capacitance meter is almost unbelievable, namely an microcontroller board and an LCD.

wqerw4

I specifically in this case use an Arduino Nano microcontroller board, and LCD 128x64 dots with an ST7565 driver chip.

ewfre

The measurement is performed in such a way that the measured capacitor is charged with current from the PULLUP resistor from the microprocessor input, and the required charging time is measured. The capacitor whose value we need to measure is connected to one analog and one digital pin of the microcontroller, and if it is a polarized capacitor, the positive pole is connected to the first defined pin in the code. The simplicity of this device is due to the excellent "capacitor" Arduino library that is made specifically, for this purpose and you can download it directly from the author's  GitHub page.

erwgte

Now let's see how this useful instrument works in real conditions. For this purpose, I will use capacitors of different types and with different values. At first, the display shows a capacitance of about 1 pF which is actually the capacitance between the wires and the connectors, which is minimal and does not affect measurements.

QAS

As you can see from the presentation, the accuracy and speed of measurement are satisfactory. And finally, a short conclusion. This is the simplest possible stand-alone capacitance meter that you can make using only two electronic components. Even simpler, if you use the device on your desktop, you only need the microcontroller, and you can read the results on the serial monitor from the Arduino IDE application on the PC. Of course, it is advisable to embed the device in a suitable box with plugins, so that you can make measurements more easily.

fgnh

Copy Code
#include <U8g2lib.h>
#include <Capacitor.h>

U8G2_ST7565_ERC12864_1_4W_SW_SPI u8g2 ( U8G2_R0, /* scl=*/ 13 , /* si=*/ 11 , /* cs=*/ 10 , /* rs=*/ 9 , /* rse=*/ 8 ) ;

Capacitor cap1(7,A2);

int X1,C; //resistance value
byte f_ic, xp;
char R1_str[3];
char R_str[4];
float tau1;
unsigned long T1, T2, tau;

void setup() {
Serial.begin(9600);
u8g2.begin();
u8g2.setContrast(35);
}


void loop() {
// Serial.println(cap1.Measure()); // Measure the capacitance (in pF), print to Serial Monitor
// delay(1000); // Wait for 1 second, then repeat
Pomiar_C();
}


void Pomiar_C(){
Cyfry();
char C_str[4];
sprintf(C_str,"%d", X1);
u8g2.firstPage();
do {

u8g2.drawFrame(0,0,128,64);
u8g2.drawRFrame(2,2,124,60,3);

u8g2.setFont(u8g2_font_10x20_tr);
u8g2.drawStr(20, 18, "Capacity:");
if (f_ic > 6) {
u8g2.setFont(u8g2_font_fub25_t_symbol);
u8g2.drawGlyph(80,52,956); //symbol u
}
u8g2.setFont(u8g2_font_fub25_tr);
u8g2.drawStr(xp, 52, C_str);
if (f_ic < 7) {u8g2.drawStr(76, 52, "n");}
if (f_ic < 4) {u8g2.drawStr(76, 52, "p");}
u8g2.drawStr(100, 52, "F");
if (f_ic == 1 or f_ic == 4 or f_ic == 7) {
u8g2.drawStr(28, 52, ".");
u8g2.drawStr(40, 52, R1_str);
}
} while ( u8g2.nextPage() );
delay(500);
}

void Cyfry(){
// if (P1 == LOW) {tau1 = tau/2.329;}
// if (P2 == LOW) {tau1 = tau/350;}
// if (P3 == LOW) {tau1 = cap1.Measure();}

tau1 = cap1.Measure();
//obliczenie ilości cyfr wartości
if (tau1 >= 1 && tau1 <10) {
X1 = tau1;
int X2 = 10 * (tau1 - X1);
sprintf(R1_str,"%d", X2);
f_ic = 1;
xp = 10;
}
if (tau1 >= 10 && tau1 <100) {
X1 = tau1;
f_ic = 2;
xp = 32;
}
if (tau1 >= 100 && tau1 <1000) {
X1 = tau1;
f_ic = 3;
xp = 10;
}
if (tau1/1000 >= 1 && tau1/1000 <10) {
X1 = int(tau1/1000);
f_ic = 4;
xp = 10;
int X2 = 10 * (tau1/1000 - X1);
sprintf(R1_str,"%d", X2);
}
if (tau1/10000 >= 1 && tau1/10000 <10) {
X1 = int(tau1/1000);
f_ic = 5;
xp = 32;
}
if (tau1/100000 >= 1 && tau1/100000 <10) {
X1 = int(tau1/1000);
f_ic = 6;
xp = 10;
}
if (tau1/1000000 >= 1 && tau1/1000000 <10) {
X1 = int(tau1/1000000);
f_ic = 7;
xp = 10;

int X2 = 10 * (tau1/1000000 - X1);
sprintf(R1_str,"%d", X2);
}
if (tau1/10000000 >= 1 && tau1/10000000 <10) {
X1 = int(tau1/1000000);
f_ic = 8;
xp = 30;
}
}

 

Mfr Part # A000005
ARDUINO NANO ATMEGA328 EVAL BRD
Arduino
£19.04
View More Details
Mfr Part # NHD-C12864A1Z-FSB-FBW-HTT
GRAPHIC DISPLAY FSTN BLACK (BLUE
Newhaven Display Intl
£18.14
View More Details
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.