Maker.io main logo

CircuitPython Hardware LED Backpacks and FeatherWings

34

2018-05-04 | By Adafruit Industries

License: See Original Project Solder Adafruit Feather

Courtesy of Adafruit

Guide by Tony DiCola

 

! Note the video above was made showing the MicroPython version of this library. Follow the guide to see both CircuitPython and MicroPython versions of the LED backpack library.

LED backpacks are bright and beautiful LED displays with a built-in controller chip that makes them super easy to use.  These displays come in all sorts of varieties, like matrices that are a grid of LED pixels or segment displays that can show numbers and characters.  Because these displays use LEDs they're bright and easy to read--perfect for showing simple measurements, time, basic graphics, and more.

And now you can use LED backpack displays with Python. This guide explores how to use LED matrix, 7-segment, and 14-segment quad alphanumeric displays with CircuitPython and MicroPython!

Be sure to check out the Adafruit LED Backpack guide for details on all of the LED backpack modules.

Hardware

Parts

You'll need the following parts to follow this guide:

Image 2

CircuitPython board. This guide focuses on the ESP8266 and Feather M0/SAMD21-based boards, but any CircuitPython board that supports I2C should work.

If your board doesn't come with CircuitPython running on it already then check out your board's guide for how to load CircuitPython firmware. For example the Feather M0 express guide is a good reference.

If you're using a Feather board and FeatherWing you probably want a Feather female header set or Feather stacking female header set.

Image 3a

LED Matrix, 7-segment, or 14-segment FeatherWing or Backpack Display. If you're using a Feather the 8x16 Matrix FeatherWing, 14-segment Quad Alphanumeric FeatherWing, or 7-segment FeatherWing are perfect options that easily connect to the Feather board. For other boards check out the large assortment of LED backpacks--the matrix (both single and bi-color), 14-segment quad alphanumeric, and 7-segment numeric backpacks can be used with the CircuitPython library.

Make sure to check if your backpack requires 5V or 3.3V of power. Larger displays like the 1.2" 7-segment display need 5V of power, but boards like Feathers only provide 5V power when plugged in to USB ports. Read the LED backpack guide for details on the power needed for each type of backpack!

Image 4

Breadboard and jumper wires. If you aren't using a Feather and FeatherWing you'll need a breadboard and jumper wires to connect the components.

Soldering tools. You'll need to solder headers to the boards Check out the guide to excellent soldering if you're new to soldering.

Make sure to follow the board and LED FeatherWing or backpack product guides to assemble and verify they work before continuing.

Wiring

If you're using a FeatherWing and Feather just slide the wing onto the Feather board and you're all set! The FeatherWing will automatically be connected to the board using its I2C connection. Skip to the next page to learn about the software to control the display.

If you're using a LED backpack breakout you'll need to connect its power, ground, and I2C connections to the board. For example the wiring for a LED matrix to Feather HUZZAH ESP8266, and 14-segment display to Feather M0 might look like:

Image 5

Fritzing Source

  • Board SCL / I2C clock to LED Backpack SCL / C
  • Board SDA / I2C data to LED Backpack SDA / D
  • Board 3.3V power to LED Backpack VCC / + (note some larger backpacks prefer 5V power but might still at 3.3V with less light output, check your product's guide for details)
  • Board 3.3V power to LED Backpack VI2C / logic level voltage (not all backpacks have a VI2C or logic level pin, check your product's guide for details)
  • Board GND / ground to LED Backpack GND / -

Remember to read about your backpack's power requirements in the LED backpack guide. Some of the large backpack displays (like the 1.2" 7-segment display) need 5V of power to run, and others require an explicit VI2C or logic level voltage input.

CircuitPython

Adafruit CircuitPython Module Install

To use the LED backpack with your Adafruit CircuitPython board you'll need to install the Adafruit_CircuitPython_HT16K33 module on your board. Remember this module is for Adafruit CircuitPython firmware and not MicroPython.org firmware!

First make sure you are running the latest version of Adafruit CircuitPython for your board. Next you'll need to install the necessary libraries to use the hardware--read below and carefully follow the referenced steps to find and install these libraries from Adafruit's CircuitPython library bundle.

Bundle Install

For express boards that have extra flash storage, like the Feather/Metro M0 express and Circuit Playground express, you can easily install the necessary libraries with Adafruit's CircuitPython bundle. This is an all-in-one package that includes the necessary libraries to use the LED backpack display with CircuitPython. To install the bundle follow the steps in your board's guide, like these steps for the Feather M0 express board.

Remember for non-express boards like the Trinket M0, Gemma M0, and Feather/Metro M0 basic you'll need to manually install the necessary libraries from the bundle:

  • adafruit_ht16k33
  • adafruit_bus_device
  • adafruit_register

If your board supports USB mass storage, like the M0-based boards, then simply drag the files to the board's file system. Note on boards without external SPI flash, like a Feather M0 or Trinket/Gemma M0, you might run into issues on Mac OSX with hidden files taking up too much space when drag and drop copying, see this page for a workaround.

If your board doesn't support USB mass storage, like the ESP8266, then use a tool like ampy to copy the file to the board. You can use the latest version of ampy and its new directory copy command to easily move module directories to the board.

Before continuing make sure your board's lib folder or root filesystem has at least the adafruit_ht16k33, adafruit_bus_device, and adafruit_register folders/modules copied over.

Image 6

Usage

The following section will show how to control the LED backpack from the board's Python prompt / REPL. You'll walk through how to control the LED display and learn how to use the CircuitPython module built for the display. As a reference be sure to see the Adafruit HT16K33 module documentation too.

First connect to the board's serial REPL so you are at the CircuitPython >>> prompt.

I2C Initialization

First you'll need to initialize the I2C bus for your board. First import the necessary modules:

Copy Code
import board
import busio as io

 

Note if you're using the ESP8266 or other boards which do not support hardware I2C you need to import from the bitbangio module instead of busio:

import boardimport bitbangio as io

Copy Code
import board
import bitbangio as io

Now for either board run this command to create the I2C instance using the default SCL and SDA pins (which will be marked on the boards pins if using a Feather or similar Adafruit board):

Copy Code
i2c = io.I2C(board.SCL, board.SDA)

LED Matrix

To use a LED matrix you'll first need to import the adafruit_ht16k33.matrix module and create an instance of the appropriate Matrix class. There are three classes currently available to use:

  • Matrix8x8 - This is for a simple 8x8 matrix (square or round pixels, they're both the same driver and code)
  • Matrix16x8 - This is for a 16x8 matrix (i.e. double the width of the 8x8 matrices). For the LED Matrix FeatherWing you want to use this Matrix16x8 class
  • Matrix8x8x2 - This is for a 8x8 bi-color matrix

For example to use the Matrix16x8 class import the module and create an instance with:

Copy Code
import adafruit_ht16k33.matrix 
matrix = adafruit_ht16k33.matrix.Matrix16x8(i2c)

 

Image 7

The above command will create the matrix class using the default I2C address of the display (0x70). If you've changed the I2C address (like when using multiple backpacks or displays) you can override it in the initializer using an optional address keyword argument.

For example to create an instance of the Matrix8x8 class on address 0x74:

Copy Code
matrix2 = adafruit_ht16k33.matrix.Matrix8x8(i2c, address=0x74)

 

You might notice the matrix turns on to a 'jumbled' collection of random LEDs. Don't worry! The display isn't broken, right now the module that controls it doesn't clear the display state on startup so you might see noise from random memory values.

To clear the display and turn all the pixels off you can use the fill command with a color of 0 (off):

Copy Code
matrix.fill(0)
matrix.show()

 

Image 8

Notice you must call the show function after calling fill to make the changes visible. All of the LED backpack library operations operate on a buffer in memory and must be pushed to the display by calling show. Don't forget any time you want an update to be visible on the display call show!

To turn all the pixels on you can use fill with a color of 1 (on):

Copy Code
matrix.fill(1)
matrix.show()

 

Image 9

If you're using the bi-color matrix you can even use a fill color of 2 or 3 to change to different colors of red, green, and yellow (red + green).

Next you can set pixels on the display using the pixel function. This function takes the following parameters:

  • X position - X position of the pixel on the matrix
  • Y position - Y position of the pixel on the matrix
  • Color - 0 for off, 1 for on (or one of the LEDs for bi-color display), 2 or 3 for other bi-color display colors

For example to set the first pixel at position 0, 0 to on:

Copy Code
matrix.pixel(0, 0, 1)
matrix.show()

 

Image 10

Don't forget to call show to make the pixel visible!

Or to set the opposite corner pixel at position 7, 7 to on: 

Copy Code
matrix.pixel(7, 7, 1)
matrix.show()

 

Image 11

That's all there is to controlling the pixels on a LED matrix! Right now the matrix library is simple and only exposes basic pixel control. In the future more advanced drawing commands might be avaialable.

Brightness and Blinking

You can change the brightness of the entire display with the brightness function. This function takes a value from 0 to 15 where 0 is the lowest brightness and 15 is the highest brightness. Note that you don't need to call show after calling brightness, the change is instant.

For example to set the brightness to the minimum:

Copy Code
matrix.brightness(0)

 

Image 12

Or to set it back to maximum:

Copy Code
matrix.brightness(15)

 

Image 13

You can also make the entire display blink at 3 different rates using the blink_rate function. Pass in a value 0 to 3:

  • 0 = no blinking
  • 1 = fast blinking (~once a 1/2 second)
  • 2 = moderate blinking (~once a second)
  • 3 = slow blinking (~once every 2 seconds)

Again you don't need to call show after setting the blink rate, the change will immediately take effect.

For example to blink quickly:

Copy Code
matrix.blink_rate(1)

 

And to stop blinking:

Copy Code
matrix.blink_rate(0)

 

LED 7-segment Display

To use a 7-segment display you'll first need to import the adafruit_ht16k33.segments module and create an instance of the Seg7x4 class. 

Copy Code
import adafruit_ht16k33.segments
display = adafruit_ht16k33.segments.Seg7x4(i2c)

 

Image 14

The above command will create the 7-segment class using the default I2C address of the display (0x70). If you've changed the I2C address (like when using multiple backpacks or displays) you can override it in the initializer using an optional address keyword argument.

For example to create an instance of the Seg7x4 class on address 0 x 74:

Copy Code
display = adafruit_ht16k33.Seg7x4(i2c, address=0x74)

 

You might notice the display turns on to a 'jumbled' collection of random LEDs. Don't worry! The display isn't broken, right now the module that controls it doesn't clear the display state on startup so you might see noise from random memory values.

To clear the display and turn all the LEDs off you can use the fill command with a color of 0 (off):

Copy Code
display.fill(0)
display.show()

 

Image 15

Put Characters

You can put a numeric value in any of the display's 4 positions with the put function. For example to set position 0 to the number 1 and position 1 to the number 2 call:

Copy Code
display.put('1', 0)
display.put('2', 1)
display.show()

 

Image 16

The put function takes these parameters:

  • The character to display - This needs to be a string and not an integer or number
  • The position to place the character - This can be a value of 0, 1, 2, or 3

Remember to call show to make the change visible!

You can also pass some special characters to display to the put function:

  • Colon - Use ':' to turn the colon on, you don't need to specify the position parameter. To turn the colon off you must currently clear the entire display with fill as shown above
  • Period / decimal point - Use '.' to turn a decimal point on at the specified position. To turn the decimal point off set the character at the same position again (the decimal point will not be preserved)
  • Hex character - Use a character 'a' through 'f' to display a high hex character value at a specified position

Display Numbers and Hex Values

There are also functions to display a number or hex value for convenience. Remember the display only has 4 digits so a best effort will be made to display the number--you might need to round the number or adjust it to fit!

To display a number call the number function with an integer or floating point value:

Copy Code
display.number(1234)
display.show()
display.number(3.141)
display.show()

 

Image 17

Or to display a hex value call the hex function with the value (remember only 4 digits are available so values from 0x0000 to 0xFFFF):

Copy Code
display.hex(0xFEED)
display.show()

 

Image 18

You can also adjust the brightness and blinking of the 7-segment display just like with the matrix display above. See the matrix brightness and blinking section for details on the functions to call.

LED 14-segment Quad Alphanumeric Display

To use a 14-segment quad alphanumeric display it's almost exactly the same as the 7-segment display, but with a slightly different class name. Import the adafruit_ht16k33.segments module again but this time create an instance of the Seg14x4 class.

Copy Code
import adafruit_ht16k33.segments
display = adafruit_ht16k33.segments.Seg14x4(i2c)

 

The above command will create the 14-segment class using the default I2C address of the display (0x70). If you've changed the I2C address (like when using multiple backpacks or displays) you can override it in the initializer using an optional address keyword argument.

For example to create an instance of the Seg14x4 class on address 0 x 74:

Copy Code
display = adafruit_ht16k33.segments.Seg14x4(i2c, address=0x74)

 

Image 19

You might notice the display turns on to a 'jumbled' collection of random LEDs. Don't worry! The display isn't broken, right now the module that controls it doesn't clear the display state on startup so you might see noise from random memory values.

To clear the display and turn all the LEDs off you can use the fill command with a color of 0 (off):

Copy Code
display.fill(0)
display.show()

 

Image 20

To use the display you can use the put function just like with the 7-segment display. However the put function for the 14-segment display can take any alphanumeric character. For example to write 'hi' to the display:

Copy Code
display.put('C', 0)
display.put('I', 1)
display.put('P', 2)
display.put('Y', 3)
display.show()

 

Image 21

You can also display numbers and hex values just like with the 7-segment display using the number and hex function.

However you can also display a text string with the text function. Remember there are only 4 characters available so keep the message short! For example to write 'mpy!':

Copy Code
display.text('CPY!')
display.show()

 

Image 22

And just like with the 7-segment display you can use the brightness and blink functions just like with the matrices to control those attributes of the display!

MicroPython

! Note this page describes how to use a MicroPython.org version of this library with MicroPython boards. Skip back to the previous page if you're using a CircuitPython board like the Feather M0 express!

In addition to CircuitPython there's an older MicroPython version of the HT16K33 library that you can use with some MicroPython boards. Before you get started it will help to be familiar with these guides for working with MicroPython:

See all the MicroPython guides in the learning system for more information.

MicroPython Module Install

To use the LED backpack with your MicroPython board you'll need to install the micropython-adafruit-ht16k33 MicroPython module on your board. Remember this module is for MicroPython.org firmware and not Adafruit CircuitPython!

First make sure you are running the latest version of MicroPython for your board. If you're using the ESP8266 MicroPython port you must be running version 1.8.5 or higher as earlier versions do not support using .mpy modules as shown in this guide.

Next download the latest ht16k33_matrix.mpy and ht16k33_seg.mpy files from the releases page of the micropython-adafruit-ht16k33 GitHub repository. You'll need to copy all of the files to your MicroPython board's file system using a tool like ampy to copy the files to the board.

Usage

The following section will show how to control the LED backpack from the board's Python prompt / REPL. You'll walk through how to control the LED display and learn how to use the MicroPython module built for the display. As a reference be sure to see the micropython-adafruit-ht16k33 module documentation too.

First connect to the board's serial REPL so you are at the MicroPython >>> prompt.

MicroPython I2C Initialization

On MicroPython.org firmware which uses the machine API you can initialize I2C like the MicroPython I2C guide mentions. For example on a board like the ESP8266 you can run (assuming you're using the default SDA gpio #4 and SCL gpio #5 pins like on a Feather & LED backpack FeatherWing):

Copy Code
import machine
i2c = machine.I2C(scl=machine.Pin(5), sda=machine.Pin(4))

 

Matrix & Segment Display Usage

Once you've initialized the I2C bus you're ready to create instances of the matrix and display classes. These classes are exactly the same as the CircuitPython version of the library, but instead live in the ht16k33_matrix module. For example to create a 8x8 matrix you could run:

Copy Code
import ht16k33_matrix
matrix = ht16k33_matrix.Matrix16x8(i2c)

 

See the CircuitPython library usage for information on the functions you can call to control the matrix and segment displays. Once you've created the display class like above its usage is the same as with CircuitPython!

Mfr Part # 3090
0.8" 8X16 LED MATRIX WITHOUT LED
Adafruit Industries LLC
Mfr Part # 3149
0.8" 8X16 LED MATRIX WHITE
Adafruit Industries LLC
£14.78
View More Details
Mfr Part # 2945
NEOPIXEL FEATHERWING
Adafruit Industries LLC
£11.08
View More Details
Mfr Part # 3134
15X7 CHARLIEPLEX LED RED
Adafruit Industries LLC
Mfr Part # 3137
15X7 CHARLIEPLEX LED BLUE
Adafruit Industries LLC
Mfr Part # 3152
0.8" 8X16 LED MATRIX RED
Adafruit Industries LLC
Mfr Part # 3138
15X7 CHARLIEPLEX LED COOL WHITE
Adafruit Industries LLC
Mfr Part # 3150
0.8" 8X16 LED MATRIX BLUE
Adafruit Industries LLC
£11.08
View More Details
Mfr Part # 2900
FEATHERWING OLED - 128X32 OLED A
Adafruit Industries LLC
£11.08
View More Details
Mfr Part # 3108
0.56" 4-DIGIT 7-SEGMENT RED
Adafruit Industries LLC
Mfr Part # 3315
FEATHERWING 2.4" 320X240 TFT LCD
Adafruit Industries LLC
£25.90
View More Details
Mfr Part # 3088
0.56" 4-DIGIT 7-SEGMENT W/O LED
Adafruit Industries LLC
50-PIN 0.5MM PITCH FPC FLEX CABL
Mfr Part # 1682
50-PIN 0.5MM PITCH FPC FLEX CABL
Adafruit Industries LLC
Mfr Part # 3107
0.56" 4-DIGIT 7-SEGMENT GREEN
Adafruit Industries LLC
More Info
View More Details
Mfr Part # 3110
0.56" 4-DIGIT 7-SEGMENT YELLOW
Adafruit Industries LLC
Mfr Part # 3089
0.54" 4-DIGIT 14-SEGMENT W/O LED
Adafruit Industries LLC
Mfr Part # 3109
0.56" 4-DIGIT 7-SEGMENT WHITE
Adafruit Industries LLC
Mfr Part # 3106
0.56" 4-DIGIT 7-SEGMENT BLUE
Adafruit Industries LLC
Mfr Part # 1676
TOUCH SCREEN RESISTIVE 7.0"
Adafruit Industries LLC
£11.08
View More Details
Mfr Part # 3128
0.54" 4-DIGIT 14-SEGMENT BLUE
Adafruit Industries LLC
£10.34
View More Details
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.