Maker.io main logo

Arduino Nano ESP32 How to Blink an LED Using Visuino Visual Programming

355

2025-07-17 | By Ron Cutts

License: General Public License LED / Display Drivers LED Matrix LED Strips Signal Generator Arduino

Learn how to program an Arduino Nano ESP32 board to blink the built-in LED using Visuino.

Watch the Video!

Step 1: What You Will Need

What You Will Need

What You Will Need

Step 2: Start Visuino, and Select the Arduino Nano ESP32 Board Type

Start Visuino, and Select the Arduino Nano ESP32 Board Type

Start Visuino, and Select the Arduino Nano ESP32 Board Type

Start Visuino as shown in the first picture. Click on the "Tools" button on the Arduino component (Picture 1) in Visuino. When the dialog appears, select "Arduino Nano ESP32" as shown in Picture 2

Step 3: In Visuino, Add & Connect Components

imageimage

  • Add "Pulse Generator" component

  • Connect "PulseGenerator1" pin [Out] to Arduino Nano ESP32 > Digital pin [13]

  • If you want to increase the speed of the blinking, select "PulseGenerator1" and in the properties window, change the "Frequency" value

Step 4: Generate, Compile, and Upload the Project

Generate, Compile, and Upload the Project

  • In Visuino, at the bottom, click on the "Build" Tab, make sure the correct port is selected, then click on the "Compile/Build and Upload" button.

Step 5: Play

After uploading the project to the Arduino Nano ESP32 board, the internal LED will blink.

Congratulations! You have completed your LED project with Visuino. Also attached is the Visuino project that I created for this Tutorial. You can download and open it in Visuino: https://www.visuino.com

Download Visuino file: Arduino Nano ESP32-LED-blink.visuino

Mfr Part # ABX00083
ARDUINO NANO ESP32 WITH HEADERS
Arduino
£14.30
View More Details
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.