DS593 (v1.5) June 23, 2015
www.xilinx.com
PN 0011051 04
1
© Copyright 2008–2015 Xilinx, Inc. Xilinx, the Xilinx logo, Artix, ISE, Kintex, Spartan, Virtex, Vivado, Zynq, and other designated brands included herein are trademarks of Xilinx
in the United States and other countries. All other trademarks are the property of their respective owners.
Features
High-performance FPGA and PROM programming and
configuration
Includes innovative FPGA-based acceleration
firmware encapsulated in a small form factor pod
attached to the cable
Leverages high-speed slave-serial mode
programming interface
Note:
Slave-serial mode is supported in Xilinx®
iMPACT software v10.1.
Recommended for prototyping use only
Easy to use
Fully integrated and optimized for use with Xilinx
iMPACT software
Intuitive multiple cable management from a single
application
Supported on the following operating systems:
Note:
See the Xilinx design tool release notes for
supported operating systems.
-
Microsoft Windows XP Professional
-
Microsoft Windows Vista
-
Red Hat Enterprise Linux
-
SUSE Linux Enterprise
Automatically senses and adapts to target I/O
voltage
Interfaces to devices operating at 5V (TTL), 3.3V
(LVCMOS), 2.5V, 1.8V and 1.5V
Intuitive flyleads-to-cable interface labeling
Reliable
Backwards compatibility with Platform Cable USB,
including Pb-Free (RoHS-compliant)
USB Integrators Forum (USB-IF) certified
CE and FCC compliant
Leverages industry standards, including JTAG
boundary-scan IEEE 1149.1, SPI and USB 2.0
Programs and configures all Xilinx devices
XC18V00 ISP PROMs
Platform Flash XCF00S/XCF00P/XL PROMs
All UltraScale™, 7 series, Virtex®, and Spartan®
FPGA families, and Zynq-7000 AP SoCs
XC9500XL and CoolRunner™ XPLA3 /
CoolRunner-II CPLDs
Note:
Xilinx iMPACT software or Vivado design tools
are required for programming and configuration. See the
design tool release notes for supported devices.
Third-party PROM device programming support
Directly programs selected Serial Peripheral
Interface (SPI) flash memory devices
Note:
Direct SPI flash memory programming supported
in Xilinx iMPACT software v10.1.
Indirectly programs selected SPI or parallel flash
memory devices via FPGA JTAG port
Highly optimized for use with Xilinx design tools
Vivado® design tools or ISE® design tools
Embedded Development Kit
ChipScope™ Pro Analyzer
System Generator for DSP
Platform Cable USB II Description
Much more than just a simple USB cable, Platform Cable
USB II (
Figure 1
) provides integrated firmware (hardware
and software) to deliver high-performance, reliable and
easy-to-perform configuration of Xilinx devices.
Platform Cable USB II attaches to user hardware for the
purpose of configuring Xilinx FPGAs, programming Xilinx
PROMs and CPLDs, and directly programming third-party
SPI flash devices. In addition, the cable provides a means of
indirectly programming Platform Flash XL, third-party SPI
flash memory devices, and third-party parallel NOR flash
memory devices via the FPGA JTAG port. Furthermore,
Platform Cable USB II is a cost effective tool for debugging
36
Platform Cable USB II
DS593 (v1.5) June 23, 2015
Platform Cable USB II
DS593 (v1.5) June 23, 2015
www.xilinx.com
2
embedded software and firmware when used with applications such as Xilinx's Embedded Development Kit and ChipScope
Pro Analyzer.
Platform Cable USB II is an upgrade to and replaces Platform Cable USB. Similar to its popular predecessor, Platform Cable
USB II is intended for prototyping environments only. Platform Cable USB II is backwards Compatible with Platform Cable
USB and is supported by all Xilinx design tools that support Platform Cable USB.
Platform Cable USB II attaches to the USB port on a desktop or laptop PC using an off-the-shelf Hi-Speed USB A–B cable.
The cable derives all operating power from the hub port controller — no external power supply is required.
Note:
Sustained data transfer rates in a Hi-Speed USB environment vary according to the number of USB devices sharing the hub
bandwidth. Native signaling rate (480 MHz) is not directly correlated to application throughput.
Device configuration and programming operations using Platform Cable USB II are supported by Xilinx iMPACT download
software using boundary-scan (IEEE 1149.1/IEEE 1532), slave-serial mode, or serial peripheral interface (SPI). The Vivado
design tools support device configuration with the Platform Cable USB II using boundary-scan (IEEE 1149.1).
Note:
iMPACT software is bundled with the ISE design tools and WebPACK™ ISE software. The slave-serial mode and direct SPI are
only supported in limited versions of the ISE iMPACT tool.
In addition, Platform Cable USB II is optimized for use with the Xilinx Embedded Development Kit, ChipScope Pro Analyzer,
and System Generator for DSP. When used with these software tools, the cable provides a connection to embedded target
systems for hardware configuration, software download, and real-time debug and verification. Target clock speeds are
selectable from 750 kHz to 24 MHz.
Platform Cable USB II attaches to target systems using a 14-conductor ribbon cable designed for high-bandwidth data
transfers. An optional adapter for attaching a flying lead set is included for backward compatibility with target systems not
using a ribbon cable connector.
X-Ref Target - Figure 1
Figure 1:
Xilinx Platform Cable USB II
D
S
59
3
_01_02140
8
Platform Cable USB II
DS593 (v1.5) June 23, 2015
www.xilinx.com
3
Physical Description
The Platform Cable USB II electronics are housed in a recyclable, fire-retardant plastic case (
Figure 2
). An internal EMI
shield attenuates internally generated emissions and protects against susceptibility to radiated emissions.
Operation
This section describes how to connect and use Platform Cable USB II.
Minimum Host System Requirements
The host computer must contain a USB Host Controller with one or more USB ports. The controller can reside on the PC
motherboard, or can be added using an expansion or PCMCIA card.
Platform Cable USB II is designed to take full advantage of the bandwidth of USB 2.0 ports, but it is also backward-
compatible with USB 1.1 ports. Refer to
USB Hub Types and Cable Performance, page 29
for additional information on
connection environments and bandwidth.
For Platform Cable USB II compatibility with Vivado design tools, see the
Vivado design tools release notes
. The
Architecture Support and Requirements
chapter in the release notes lists the supported operating systems and cable
installation requirements.
X-Ref Target - Figure 2
Figure 2:
Plastic Case Physical Description
Top View
S
ide View
STATUS
25.4 mm
16.5 mm
115.6 mm
5
3
.
3
mm
Made in U.S.A.
Serial
XU - 12345
Model
DLC10
Platform Cable USB II
Power
5V
0.15A
2mm
CONNECTOR
SIGNALS
RoHS
Compliant
VREF
PROG
CCLK
DONE
DIN
INIT
----
or
orSerial
1.5 < VREF < 5.0 VDC
VREF
VREF
SS
TMS
SCK
TCK
MISO
TDO
MOSI
TDI
----
----
SPI
JTAG
WP
HALT
Gnd
Gnd
Gnd
Gnd
Gnd
----
PGND
D
S
59
3
_02_02190
8
HI-SPEED
CERTIFIED
USB
®
Platform Cable USB II
DS593 (v1.5) June 23, 2015
www.xilinx.com
4
For Platform Cable USB II compatibility with ISE design tools, see the
ISE design tools release notes
. The
Architecture
Support and Requirements
chapter in the release notes lists supported operating systems and cable installation
requirements.
Table 1
lists Platform Cable USB II compatibility with the Xilinx design tools.
The minimum system requirements for Vivado design tools are outlined in the
Vivado design tools release notes
. The
Architecture Support and Requirements
chapter in the release notes lists supported operating systems and cable
installation requirements.
The minimum system requirements for ISE design tools are outlined in the
ISE design tools release notes
. The
Architecture
Support and Requirements
chapter in the release notes lists supported operating systems and cable installation
requirements.
Note:
To receive the current enhancements and bug fixes, Xilinx recommends using the newest version of a tool and applying the latest
service pack.
Operating Power
Platform Cable USB II is a bus-powered device (drawing less than 150 mA from the host USB port under all operating
conditions), automatically adapting to the capabilities of the host USB port to achieve the highest possible performance.
Platform Cable USB II enumerates on any USB port type: USB ports on root hubs, external bus-powered hubs, external self-
powered hubs and legacy USB 1.1 hubs (see
USB Hub Types and Cable Performance, page 29
). However, performance is
not optimal when attached to USB 1.1 hubs (refer to
Hot Plug and Play, page 5
for an explanation of USB enumeration).
Device Driver Installation
For a complete guide to installation of the Platform Cable USB II refer to the
USB Cable Installation Guide
(
UG344
).
A proprietary device driver is required to use Platform Cable USB II. This driver is automatically installed when a supported
Xilinx design tool is installed.
Note:
Automatic driver installation is available beginning with version 10.1 of Xilinx design tools. For earlier versions, a driver installer
must be run prior to using the cable. Refer to the
USB Cable Installation Guide
for instructions on downloading and running the installer.
Firmware Updates
The Platform Cable USB II firmware resides in an USB microcontroller and a FPGA/PROM. The microcontroller is RAM-
based and firmware is downloaded each time the cable is connected and detected by the host operating system. Additional
firmware can also be downloaded to the microcontroller once a design tool establishes a connection with the cable. The USB
protocol guarantees that the firmware is successfully downloaded.
Upgraded firmware for the USB microcontroller is periodically distributed in Xilinx design tool releases or, on rare occasions,
in a
Xilinx Answer Record
. In most cases, an upgrade requires replacing one or more of the design tool's application files and
depending on operating system, one or more cable driver files.
Platform Cable USB II contains a Xilinx Spartan-3A FPGA with an in-system programmable Xilinx XCF02S PROM. Each
time a design tool establishes a connection with the cable, the firmware version stored in the PROM is examined. The PROM
Table
1:
Platform Cable USB II Software Compatibility
Software
Version
Vivado Design Tools
2013.1 and later
ISE Foundation/ISE WebPACK
6.3i SP3 and later
ChipScope Pro Analyzer
6.3i SP3 and later
Embedded Development Kit
7.1i and later
System Generator for DSP
8.1i and later
Notes:
1.
An installer must be run to enable Platform Cable USB II for use with Xilinx design tools
prior to 10.1. Refer to
Device Driver Installation, page 4
for additional details.
Platform Cable USB II
DS593 (v1.5) June 23, 2015
www.xilinx.com
5
is automatically reprogrammed over the cable if the firmware version is out of date. If an update is required, the design tool
displays the following warning message:
Warning: USB Cable firmware must be updated. This operation may take up to 40 seconds. Do not stop
the process or disconnect the cable prior to completion. The cable STATUS LED will be RED for the
duration of the update process.
Similarly, upgraded firmware for the FPGA/PROM is periodically distributed in Xilinx design tool releases or, on rare
occasions, in a
Xilinx Answer Record
. In most cases, an upgrade requires replacing a single design tool application file. The
PROM is reprogrammed with the new firmware the next time the tool connects to the cable. PROM reprogramming takes
approximately 40 seconds over a USB 2.0 port and 60 seconds over a USB 1.1 port. Reprogramming times vary depending
on the Xilinx design tool version, the type of USB port and the performance of the host system.
During a PROM update, the cable's status LED illuminates red (
Figure 8, page 11
), and a progress bar indicates
communication activity. PROM updates should never be interrupted. When an update is complete, the status LED returns to
either amber or green, and the cable is ready for normal operation.
Hot Plug and Play
Platform Cable USB II can be attached and removed from the host computer without the need to power-down or reboot.
There is a momentary delay after connecting the cable to an available port before the status LED illuminates — this process
is called enumeration.
Connecting to the Cable in the Vivado Design Tools
For instructions on connecting the cable in the Vivado design tools, see the
Setting Up
section in the
Vivado Design Suite
Tutorial: Programming and Debugging
.
Connecting to the Cable in iMPACT Software
This section describes some of the ways to connect to Platform Cable USB II using the Xilinx iMPACT graphical user
interface (GUI). For cable communication using other Xilinx design tools or methods, please refer to the appropriate software
user guide.
Select a Flow
From the iMPACT GUI, select a flow on the
Modes
tab (
Figure 3
). Double-click on the desired flow.
X-Ref Target - Figure 3
Figure 3:
iMPACT (9.2i) Modes Tab
D
S
59
3
_0
3
_02140
8
Platform Cable USB II
DS593 (v1.5) June 23, 2015
www.xilinx.com
6
Note:
For a description of the different flows, please refer to
iMPACT
Help
.
Establishing a Connection
Once a flow is selected, there are a number of ways to establish a connection with the cable. Two common options are
described here:
Option 1: Cable Auto Connect
To auto connect the cable, select
Output
Cable Auto Connect
(
Figure 4
).
Note:
During the auto-connect sequence, the iMPACT tool selects Parallel Cable IV (PC4) as the active cable if both PC4 and Platform
Cable USB II are connected to the same host system. If two or more USB cables are connected to the same host, the active cable is the
first USB cable physically connected to the host system. See
Multiple USB Cable Management, page 7
, for information on controlling
more than one USB cable from a single application.
Option 2: Manual Cable Connect
To manually connect the cable, select
Output
Cable Setup
. Select the
Xilinx USB Cable
radio button in the Cable
Communication Setup dialog box (
Figure 5
).
X-Ref Target - Figure 4
Figure 4:
iMPACT Software (9.2i) Output Pull-Down Menu
D
S
59
3
_04_02140
8
Platform Cable USB II
DS593 (v1.5) June 23, 2015
www.xilinx.com
7
It is necessary to perform a cable disconnect when switching from boundary-scan or Direct SPI Configuration mode to slave-
serial mode, or vice versa. iMPACT software can be disconnected from the cable using
Output
Cable Disconnect
(
Figure 4, page 6
). After the mode switch is complete, reestablish the cable connection using the
Output
Cable Setup
dialog. It is not necessary, however, to perform a cable disconnect when switching between boundary-scan and Direct SPI
Configuration modes.
If an iMPACT session is active when an
Output
Cable Disconnect
or
Output
Disconnect All Cables
operation is
performed, or if the cable is physically disconnected from the host system, the Cable Status Bar (
Figure 7, page 10
) at the
bottom, right-hand edge of the GUI immediately indicates a
No Cable Connection
.
Xilinx design tools employ system semaphores to manage access to Xilinx cables, allowing multiple applications to
simultaneously access (connect to) a single cable (but only one application can perform cable operations at a given time).
For example, assume two instances of iMPACT (instance A and instance B) are connected to a single cable. If A begins a
programming operation, and B then attempts a programming operation, B is temporarily blocked from accessing the cable.
B receives a message indicating that the cable is
locked,
and the operation must be attempted again later.
Multiple USB Cable Management
Platform Cable USB II contains a 64-bit electronic serial number used by applications to uniquely identify and access a
specific USB cable when multiple USB cables (up to 127) are connected to the same host. iMPACT software provides a
dialog box (
Figure 6, page 8
) allowing users to select a specific cable from a list of attached cables. When one of the cables
in the list is highlighted, the status LED on the appropriate cable blinks, allowing users to make a logical-to-physical
association. When the desired cable is
connected
and the dialog box closed, the status LED no longer blinks.
The Cable Setup Information dialog box (
Figure 6
) appears when the
Advanced USB Cable Setup
button is pressed in the
Cable Communication Setup dialog box (
Figure 5
).
Note:
The multiple USB cable management feature is only available in iMPACT software version 10.1 and later. Refer to the iMPACT
section of Xilinx
ISE software manuals
for additional details on this feature.
X-Ref Target - Figure 5
Figure 5:
iMPACT Software (10.1) Cable Communication Setup
D
S
59
3
_05_02140
8
Platform Cable USB II
DS593 (v1.5) June 23, 2015
www.xilinx.com
8
Configuration Clock Speed
The Platform Cable USB II configuration clock (TCK_CCLK_SCK) frequency is selectable.
Table 2
shows the complete set
of available TCK_CCLK_SCK speed selections.
iMPACT 7.1i (and later) provides a feature wherein the BSDL file of each device in a target JTAG chain is scanned to
determine the maximum boundary-scan clock (JTAG TCK) frequency. iMPACT 7.1i (and later) automatically restricts the
available TCK_CCLK_SCK selections to frequencies less than or equal to the slowest device in the chain. By default,
iMPACT 7.1i (or later) selects either 6 MHz or the highest common frequency when any device in the JTAG chain is not
capable of 6 MHz operation.
Table 3
shows the maximum supported JTAG TCK frequency for a variety of Xilinx devices. See
the device data sheet or BSDL file for maximum JTAG TCK specifications.
Note:
Certain Xilinx design tools and iMPACT versions earlier than 7.1i do not restrict the TCK_CCLK_SCK selections in JTAG mode.
Accordingly, users should take care to select a TCK_CCLK_SCK frequency matching the JTAG TCK specifications for the slowest device
in the target chain.
In slave-serial or direct SPI configuration mode, the TCK_CCLK_SCK speed can be set to any one of the available
selections. By default, the TCK_CCLK_SCK speed is set to 6 MHz. Users should take care to select a TCK_CCLK_SCK
frequency matching the slave-serial clock (CCLK or SPI clock) specification of the target device.
X-Ref Target - Figure 6
Figure 6:
iMPACT (10.1) Cable Setup Information
Table
2:
Configuration Speed Selections
TCK_CCLK_SCK Frequency
Notes
24 MHz
24 MHz is supported in limited versions of the ISE iMPACT tool up to version 11.5.
12 MHz
6 MHz (Default)
3MHz
1.5 MHz
750 kHz
Table
3:
Maximum JTAG Clock Frequencies
Device Family
Maximum JTAG Clock Frequency (MHz)
Zynq-7000
66 MHz
Virtex-7
15–66 MHz
Kintex-7
15–66 MHz
Artix-7
15–66 MHz
D
S
59
3
_06_02140
8
Platform Cable USB II
DS593 (v1.5) June 23, 2015
www.xilinx.com
9
Virtex-6
33–66 MHz
Spartan-6
18–33 MHz
XC9500XL
10
XPLA3
10
CoolRunner-II
33
XC18V00
10
XCF00S/XCF00P
15
Virtex
33
Virtex-II
33
Virtex-II Pro
33
Virtex-4
33
Virtex-5
33
Spartan-II
33
Spartan-3
33
Spartan-3A
33
Spartan-3AN
(50, 200 and 400 densities)
33
Spartan-3AN
(700 and 1400 densities)
20
Spartan-3E
30
Notes:
1.
See the individual device data sheet for the maximum JTAG TCK clock frequency.
Table
3:
Maximum JTAG Clock Frequencies
(Cont 'd)
Device Family
Maximum JTAG Clock Frequency (MHz)
Platform Cable USB II
DS593 (v1.5) June 23, 2015
www.xilinx.com
10
iMPACT Cable Status Bar
A status bar on the bottom edge of the iMPACT GUI (
Figure 7
) provides information about cable operating conditions. For
example, if the host port is USB 2.0, Platform Cable USB II connects at Hi-Speed and the status bar shows usb-hs. If the
host port is USB 1.1, Platform Cable USB II connects at full-speed, and the status bar shows usb-fs. Finally, the status bar
displays the active cable and TCK_CCLK_SCK frequency.
Status Indicator
Platform Cable USB II uses a tri-color status LED to indicate the presence of target voltage and to indicate that a cable
firmware update is in progress (
Figure 8
).
When the cable is connected (using a ribbon cable, or flying leads) to a mating connector on the target system, the status
LED is illuminated as a function of the voltage present on pin 2 (V
REF
). Users must design their system hardware with pin 2
attached to a voltage plane suppling the JTAG, SPI, or slave-serial pins on the target device(s). Some devices have separate
power pins for this purpose (V
AUX
), while others have a common supply for both V
CCIO
and the JTAG pins (TCK, TMS, TDI,
and TDO). Refer to the target device data sheet for details on JTAG, slave serial, or SPI pins.
The status LED is amber when any one or more of the following conditions exist:
The cable is not connected to a target system
The target system is not powered
The voltage on the V
REF
pin is
+1.3V.
The status LED is green when all of the following conditions exist:
The cable is connected to a target system
The target system is powered
The voltage on the V
REF
pin is
+1.5V.
Note:
There is 200 mV of hysteresis in the V
REF
detection circuit. If V
REF
drops below 1.3V, the status LED turns amber and does not
turn green until V
REF
is raised above 1.5V.
The status LED is red whenever a cable firmware update is in progress.
X-Ref Target - Figure 7
Figure 7:
iMPACT (10.1) Cable Status Bar
D
S
59
3
_07_02190
8
Platform Cable USB II
DS593 (v1.5) June 23, 2015
www.xilinx.com
11
The status LED is off whenever Platform Cable USB II enters a suspend state (see
System Suspend, page 12
), is
disconnected from a USB port, or is connected to an un-powered USB port.
Table 4
summarizes the various status LED states.
Table
4:
Interpreting the Status LED
LED Color
LED State
Condition
OFF
Continuous
Host power OFF
AMBER
Continuous
Target V
REF
1.3V
AMBER
Blinking
Target V
REF
1.3V AND multiple cable identification active
GREEN
Continuous
Target V
REF
1.5V
GREEN
Blinking
Target V
REF
1.5V AND multiple cable identification active
RED
Continuous
FPGA firmware update in progress
X-Ref Target - Figure 8
Figure 8:
Cable Status LED
Am
b
er indic
a
te
s
no t
a
rget volt
a
ge (V
REF
)
Green indic
a
te
s
t
a
rget volt
a
ge (V
REF
) pre
s
ent
Red indic
a
te
s
c
ab
le firmw
a
re
u
pd
a
te
D
S
59
3
_0
8
_120
3
07
Platform Cable USB II
DS593 (v1.5) June 23, 2015
www.xilinx.com
12
System Suspend
The cable's status LED is extinguished when the host system enters a suspend (power-saving) state. A system can suspend
for a number of reasons. For example:
The user puts the host system into standby or hibernate.
The suspend function key on a laptop computer is pressed.
The display panel of a laptop is closed.
The host system is configured to suspend (standby or hibernate) after a specified amount of inactivity.
The current drawn by the cable while suspended depends on the type of suspend state: standby or hibernate. While the host
system is in standby, the cable draws approximately 350 μA from the USB port. When the host is hibernating, all power is
removed from the USB ports so the cable draws no current while in this state.
The target interface output drivers are not powered while the host is suspended. These signals float to any DC bias level
provided by the target hardware during suspend.
If an iMPACT (10.1 or later) operation is in progress when suspend is attempted, iMPACT displays a message (
Figure 9
)
indicating that suspend is blocked until the operation is complete or manually aborted.
Note:
This feature is not supported in earlier versions of iMPACT, while iMPACT is operating in batch mode, or by other Xilinx design
tools. In these cases, it is recommended that suspend be disabled in the host system when performing long, continuous operations.
The cable is automatically disconnected when the host system is suspended. A reconnect is necessary when the host re-
awakens from the suspend state (see
Connecting to the Cable in iMPACT Software, page 5
).
Platform Cable USB II Connections
This section discusses physical connections from Platform Cable USB II to the host PC and the target system.
High Performance Ribbon Cable
A 6-inch ribbon cable is supplied and recommended for connection to target systems (
Figure 10
). The cable incorporates
multiple signal-ground pairs and facilitates error-free connections. The Xilinx product number for the 6-inch ribbon cable is
HW-RIBBON14.
To take advantage of the ribbon cable, a mating connector must be incorporated into the target system. This connector is
normally installed only during prototype checkout. When the production hardware is functional and the ISP devices can be
configured from alternate sources, the connector can be eliminated to reduce cost. Maintaining the footprint for this
connector is recommended if space permits.
X-Ref Target - Figure 9
Figure 9:
Suspend Warning When iMPACT (10.1 or later) is Busy
D
S
59
3
_09_02140
8
Platform Cable USB II
DS593 (v1.5) June 23, 2015
www.xilinx.com
13
The connector is a 2 mm shrouded keyed header. See
Table 5, page 15
for vendor part numbers and pin assignments.
Flying Wire Adapter
An adapter with wires (
Figure 11
) is provided for attachment to legacy target systems that do not incorporate a shrouded
2 mm connector. The adapter makes it possible to use flying wires for connections to distributed terminals on a target
system.
The adapter is a small circuit board with two connectors (
Figure 12
). The connector on the bottom side of the adapter mates
with the 14-pin Platform Cable USB II male 2 mm connector. A 7-pin right-angle header on the top side of the adapter mates
with the standard Xilinx flying wire set.
Note:
This method of connection is not recommended because it can result in poor signal integrity. Additionally, damage can result if the
leads are unintentionally connected to high voltages.
The Xilinx product number for the flying wire set is HW-USB-FLYLEADS-G.
X-Ref Target - Figure 10
Notes:
1.
Ribbon Cable: 14-pin conductor, 1.0 mm center, round-conductor flat cable, 28 AWG (7 x 36) stranded conductors, gray PVC with pin 1 edge
marked.
2.
2 mm ribbon female polarized connector, IDC connection to ribbon. Contacts are beryllium copper plated 30 micro-inches gold plating over
50-micro-inches nickel. The connectors mate to 0.5 mm square posts on 2 mm centers.
Figure 10:
High Performance Ribbon Cable
X-Ref Target - Figure 11
Figure 11:
Flying Wire Adaptor (Top) with Wires
D
S
59
3
_10_112607
STATUS
Made in U.S.A.
Serial
XU - 12345
Model
DLC10
Platform Cable USB II
Power
5V
0.15A
2mm
CONNECTOR
SIGNALS
RoHS
Compliant
VREF
PROG
CCLK
DONE
DIN
INIT
- -
or
orSerial
1.5 < VREF < 5.0 VDC
VREF
VREF
SS
TMS
SCK
TCK
MISO
TDO
MOSI
TDI
- -
- -
SPI
JTAG
WP
HALT
Gnd
Gnd
Gnd
Gnd
Gnd
- -
PGND
HI-SPEED
CERTIFIED
USB
®
JTAG
/
SERIAL
/
SPI
VREF
/
VREF
/
VREF
GND
/
GND
/
GND
TCK
/
CCLK
/
SCK
TDO
/
DONE
/
MISO
TDI
/
DIN
/
MOSI
TMS
/
PROG
/
SS
HALT
/
INIT
/
WP
ADAPTER
D
S
59
3
_11_02190
8
Platform Cable USB II
DS593 (v1.5) June 23, 2015
www.xilinx.com
14
Physical Connection to the Host
Each Platform Cable USB II includes a detachable, Hi-Speed-USB-certified, 1.8-meter A–B cable (
Figure 13
). Under no
circumstances should user-supplied cables exceed 5 meters. Sub-channel cables (intended for low-speed 1.5 Mb/s
signaling) should not be used with Platform Cable USB II.
A standard series B receptacle (
Figure 13
) is incorporated into the case for mating with the detachable Hi-Speed A–B cable.
A separate chassis ground is attached to the A–B cable drain wire and returns ESD current to the host system ground.
X-Ref Target - Figure 12
Figure 12:
Flying Wire Adapter (Side) without Wires
X-Ref Target - Figure 13
Figure 13:
Standard A-B Host Interface Cable and Series B Receptacle
D
S
59
3
_12_01250
8
Ad
a
pter Circ
u
it Bo
a
rd
D
S
59
3
_1
3
_112607
Platform Cable USB II
DS593 (v1.5) June 23, 2015
www.xilinx.com
15
Target Interface Connectors
Mating connectors for attachment of the high-performance ribbon cable to a target system are available in both through-hole
and surface mount configurations (
Figure 14
). Shrouded and keyed versions should always be used to guarantee proper
orientation when inserting the cable. The connector requires only 105 mm
2
of board space.
The target system voltage applied to pin 2 of this connector is used as a power source for the output buffers that drive the
output pins (see
Target Interface Reference Voltage and Signals, page 20
).
Table 5, page 15
provides some third-party sources for mating connectors that are compatible with the Platform Cable
USB II ribbon cable.
X-Ref Target - Figure 14
Figure 14:
Target Interface Connector Dimensions and Signal Assignments
Table
5:
Mating Connectors for 2 mm pitch, 14-Conductor Ribbon Cable
Manufacturer
(1)
SMT,
Vertical
Through-Hole,
Vertical
Through-Hole,
Right Angle
Web Site
Molex
87832-1420
87831-1420
87833-1420
www.molex.com
FCI
98424-G52-14
98414-G06-14
98464-G61-14
www.fciconnect.com
Comm Con Connectors
2475-14G2
2422-14G2
2401R-G2-14
www.commcon.com
Notes:
1.
Some manufacturer pin assignments do not conform to Xilinx pin assignments. Please refer to the manufacturer's data sheet for more
information.
2.
Additional ribbon cables can be purchased separately from the
Xilinx Online Store
.
PGND
GND
GND
GND
GND
GND
NC
TDI
TDO
TCK
TM
S
Vref
HALT
7.59 mm
6.
3
0 mm
12.00 mm
2.00 mm
1
3
11
9
7
5
3
1
12
10
8
6
4
2
14
NC
NC
MO
S
I
DIN
MI
S
O
DONE
S
CK
CCLK
SS
PROG
Vref
Vref
WP
INIT
JTAG
S
PI
S
l
a
ve
S
eri
a
l
TYP.
16.66 mm
2.00 mm
0.50 mm
D
S
59
3
_14_01250
8
Platform Cable USB II
DS593 (v1.5) June 23, 2015
www.xilinx.com
16
Target System Connections
This section provides examples of the various configuration topologies supported by Platform Cable USB II. Each example
incorporates the 2 mm connector (see
Target Interface Connectors, page 15
) as the cable interface. Diagrams in this section
provide a functional relationship between the cable interface and the target devices.
Note:
Signal integrity is not considered in these examples. Refer to
Signal Integrity, page 28
for details on buffering and termination.
JTAG and Slave Serial
Multiple devices can be cascaded when using either a JTAG or slave-serial topology in target systems.
Figure 15
and
Figure 17, page 18
show typical routing for JTAG and slave-serial topologies, respectively.
Note:
The cable supports the slave-serial topology with iMPACT v10.1 only. The Vivado Design Tools do not support slave-serial with the
cable.
Platform Cable USB II provides a multi-use signal on its target interface connector called pseudo ground (PGND). The
PGND pin is connected to an open-drain driver (see
Pseudo Ground Signal in iMPACT, page 23
); hence, it is either Low or
high-Z. The behavior of PGND is determined by the host application connected to the cable. In iMPACT, PGND is active-Low
during JTAG, slave-serial and SPI operations (for example, programming, configuration, read back, etc.) and high-Z when
the cable is idle.
Figure 16, page 17
shows a typical use of PGND as a control signal to manage a target system's JTAG chain. PGND drives
the select (S) term on a set of multiplexers that switch between the primary configuration source and the cable. When PGND
is active-Low, the cable drives the JTAG chain. When PGND is high-Z, the primary configuration source drives the JTAG
chain. This capability allows Platform Cable USB II to remain attached to the target system while remaining isolated from the
primary configuration source. A similar scheme can be used with slave-serial topologies.
Note:
PGND is supported in Vivado Hardware Manager and Xilinx SDK tools. These tools drive PGND Low while the application is
connected to the cable. PGND is high-Z when all applications are disconnected from the cable.
Note:
PGND is supported in iMPACT versions 10.1 and later. PGND remains high-Z in earlier versions of iMPACT and in Xilinx design
tools that do not support PGND.
The DONE pin on FPGAs can be programmed to be an open-drain or active driver. For cascaded slave-serial topologies, an
external pull-up resistor should be used, and all devices should be programmed for open-drain operation.
X-Ref Target - Figure 15
Notes:
1.
Example implies that V
CCO
, V
CCJ
, and V
CCAUX
for various devices are set to the same voltage. Refer to the device data sheet for the
appropriate JTAG voltage-supply levels.
2.
Attach the following 2 mm connector pins to digital ground: 3, 5, 7, 9, and 11.
Figure 15:
Example of JTAG Chain Topology
I
S
P
PROM
TDO
TDI
TCK
TM
S
FPGA
D
S
59
3
_15_01150
8
TDI
TCK
TM
S
CPLD
TDO
TDI
TCK
TM
S
TM
S
TCK
TDI
TDO
GND
(2)
V
REF
2
*
8
10
4
6
2-mm Connector
TDO
V
CCAUX
(1)
Platform Cable USB II
DS593 (v1.5) June 23, 2015
www.xilinx.com
17
X-Ref Target - Figure 16
Notes:
1.
Example implies that V
CCO
, V
CCJ
, and/or V
CCAUX
for various devices in the JTAG chain are set to the same voltage.
2.
Attach the following 2 mm connector pins to digital ground: 3, 5, 7, 9, and 11.
3.
The cable uses an open-drain driver to control the pseudo ground (PGND) signal — an external pull-up resistor is required.
4.
Assumes that the multiplexor supply voltages pins are connected to V
CCAUX
.
5.
Pin 13 is grounded on legacy Xilinx USB cables (models DLC9, DLC9G and DLC9LP), and Parallel Cable IV (model DLC7). These cables
need to be manually detached from the 2 mm connector to allow the primary configuration source to have access to the JTAG chain.
Figure 16:
Example Using PGND in a JTAG Chain with the ISE iMPACT Tool
8
2
10
4
6
1
3
*
V
REF
TDO
TDI
TM
S
TCK
PGND
(5)
GND
(2)
JTAG CHAIN
TDI
TDO
TM
S
TCK
TM
S
TDI
TDO
TCK
A
B
S
Y
MUX Tr
u
th T
ab
le
S
O
u
tp
u
t
HY
=
A
LY
=
B
A
B
S
Y
A
B
Y
S
Config
u
r
a
tion
S
o
u
rce
(Prim
a
ry)
2-mm
Connector
Pl
a
tform C
ab
le U
S
B II
(
S
econd
a
ry)
V
CCAUX
(1)
1 K
Ω
Re
qu
ired
P
u
ll-Up
(
3
)
D
S
59
3
_16_02140
8
(4)
(4)
(4)
10 K
Ω
V
CCAUX
10 K
Ω
10 K
Ω
V
CCAUX
Platform Cable USB II
DS593 (v1.5) June 23, 2015
www.xilinx.com
18
Direct SPI
Platform Cable USB II can connect directly to a single SPI flash device.
Figure 18, page 19
shows an example SPI flash
connection. The application note
Configuring Xilinx FPGAs with SPI Serial Flash
(
XAPP951
) provides additional details of
the cable connections necessary to program a FPGA bitstream into a SPI flash device.
Note:
See
Configuring Xilinx FPGAs with SPI Serial Flash
for a list of supported SPI devices. Direct SPI is supported with iMPACT v10.1
only. The Vivado Design Tools do not support direct SPI with the cable.
By connecting PGND to PROG_B of the FPGA (
Figure 17
), the FPGA can be commanded to set its SPI signals to high-Z
while the cable programs a SPI flash device. PGND is pulled Low when the cable is driving its SPI signals in SPI mode and
set to high-Z when the cable is not driving its SPI signals. PGND eliminates the need for a hardware jumper to ground on the
PROG_B signal and the need for additional control logic. PGND is controlled by an open-drain driver.
Note:
PGND control for SPI programming is available in iMPACT versions 9.2i and later.
X-Ref Target - Figure 17
Notes:
1.
Set mode pins (M2-M0) on each FPGA to slave-serial mode when using the USB cable, so the CCLK is treated as an input.
2.
Example uses generalized nomenclature for the voltages-supply levels. Refer to the device data sheet for the appropriate serial configuration
voltage-supply levels.
3.
Attach the following 2 mm connector pins to digital ground: 3, 5, 7, 9, and 11.
4.
A pull-up is required when two or more devices are cascaded and programmed for open-drain operation.
5.
This diagram is not applicable to the Vivado Design Tools. The Vivado Design Tools do not support the slave-serial topology.
Figure 17:
Example of Cascaded Slave-Serial Topology with the iMPACT Software
FPGA
1
FPGA
2
FPGA
n
DOUT
DIN
CCLK
(1)
DONE
INIT
DOUT
DIN
CCLK
(1)
DONE
INIT
DOUT
DIN
CCLK
(1)
DONE
INIT
INIT
CCLK
DIN
DONE
PROG
PROG
PROG
PROG
V
CCAUX
(2)
V
CCAUX
(2)
V
CCO
(2)
GND
(
3
)
V
REF
2
6
4
10
14
8
*
2-mm Connector
D
S
59
3
_17_02140
8
470
Ω
(4
)
Platform Cable USB II
DS593 (v1.5) June 23, 2015
www.xilinx.com
19
Indirect SPI
When used with Xilinx design tools, Platform Cable USB II can be used to indirectly program some third-party SPI serial
flash PROMs via the target FPGA's JTAG port. For a complete description on using Platform Cable USB II for indirect
programming of third-party SPI serial flash PROMs and for a complete list of supported SPI serial flash memories, refer to
the application note
Indirect Programming of SPI Serial Flash PROMs with Spartan-3A FPGAs
(
XAPP974
).
X-Ref Target - Figure 18
Notes:
1.
The pin names for a ST Microsystems M25Pxx serial flash device are shown in this example. SPI flash devices from other vendors can have
different pin names and requirements. Refer to the SPI flash data sheet for the equivalent pins and device requirements.
2.
The example shows the interconnect and device requirements for a Xilinx Spartan-3E FPGA. Other SPI-capable FPGAs can have different
pin names and requirements. Please refer to the FPGA data sheet for equivalent pins and device requirements.
3.
The cable uses an open-drain driver to control the pseudo ground (PGND) signal — an external pull-up resistor is required.
4.
Attach the following 2 mm connector pins to digital ground: 3, 5, 7, 9 and 11.
5.
Typically, an FPGA and other slave SPI devices (not shown) are connected to the SPI bus. The other devices on the SPI bus must be disabled
when the cable is connected to the 2 mm connector to avoid signal contention. When a Xilinx FPGA is connected to the SPI bus, the cable
holds the FPGA PROG_B pin Low to insure the FPGA SPI pins are 3-stated.
6.
This diagram is not applicable to the Vivado Design Tools. The Vivado Design Tools do not support the direct SPI topology.
Figure 18:
Example of Direct SPI Topology with the iMPACT Software
MO
S
I
PROG_B
GND
S
p
a
rt
a
n-
3
E
(2)
FPGA
VCCINT
VCCO_0
VCCO_2
VCCAUX
VCC
W
HOLD
D
DIN
Q
C
S
O_B
S
CCLK
C
GND
S
T Micro
M25Pxx
(1)
S
PI Fl
as
h
2
8
10
4
6
1
3
*
V
REF
MI
S
O
MO
S
I
SS
S
CK
PGND
GND
(4)
2 mm
Connector
+
3
.
3
V
S
PI B
us
(5)
+2.5V
+
3
.
3
V
+1.2V
+
3
.
3
V
4.7 k
Ω
(
3
)
+ 2.5V
‘1
‘1
D
S
59
3
_1
8
_02150
8
Platform Cable USB II
DS593 (v1.5) June 23, 2015
www.xilinx.com
20
Indirect BPI
When used with the ISE design tools, Platform Cable USB II can be used to indirectly program Platform Flash XL, or some
third-party NOR flash memories (BPI PROMs) via the target FPGA's JTAG port. For a description of the indirect Platform
Flash programming solution, see the
Platform Flash XL User Guide
(
UG438
).
For a complete description on using Platform Cable USB II for indirect programming of third-BPI PROMs and for a complete
list of supported BPI PROMs, refer to the
iMPACT Flash device support table
.
Target Interface Reference Voltage and Signals
Target Reference Voltage Sensing (V
REF
)
Platform Cable USB II incorporates an over-voltage clamp on the V
REF
pin of the 2 mm ribbon cable connector. The clamped
voltage (V
REF_CLAMP
) supplies high-slew-rate buffers that drive each of the output signals (see
Output Driver Structure
).
V
REF
must be a regulated voltage.
Note:
Do not insert a current-limiting resistor in the target system between the V
REF
supply and pin 2 on the 2 mm connector.
When Platform Cable USB II is idle, a nominal amount of current is drawn from the target system V
REF
.
Figure 19
shows the
V
REF
current as a function of V
REF
voltage.
No damage to Platform Cable USB II occurs if the A–B cable is unplugged from the host while the ribbon cable or flying leads
are attached to a powered target system. Similarly, no damage to target systems occurs if Platform Cable USB II is powered
and attached to the target system while the target system power is off.
Bidirectional Signal Pins
Platform Cable USB II provides five bidirectional signal pins: TDI_DIN_MOSI, TDO_DONE_MISO, TCK_CCLK_SCK,
TMS_PROG_SS and HALT_INT_WP. Each pin incorporates the same I/O structure. The state of each pin (reading or
writing) is determined by the current mode of the cable (JTAG, SPI, or slave-serial).
Output Driver Structure
Each output signal is routed through a NC7SZ126 ultra high-speed CMOS buffer (
Figure 20, page 21
). Series-damping
resistors (30.1
Ω
) reduce reflections. Weak pull-up resistors (20 k
Ω
) terminating at V
REF_CLAMP
maintain a defined logic level
when the buffers are set to high-Z. Schottky diodes provide the output buffers with undershoot protection.
The FPGA sets the output buffers to high-Z when V
REF
drops below 1.30 V. In addition, an over-voltage Zener on V
REF
clamps V
REF_CLAMP
to approximately 3.9V.
Figure 21, page 22
shows the relationship between the output drive voltage and V
REF
.
Note:
The output drivers are enabled only during cable operations; otherwise, they are set to high-Z between operations.
Xilinx design tools actively drive the outputs to logic 1 before setting the respective buffer to high-Z, avoiding the possibility
of a slow rise-time transition caused by a charge path through the pull-up resistor into parasitic capacitance on the target
system.
Platform Cable USB II
DS593 (v1.5) June 23, 2015
www.xilinx.com
21
X-Ref Target - Figure 19
Figure 19:
V
REF
Current vs. V
REF
Voltage
X-Ref Target - Figure 20
Figure 20:
Target Interface Driver Topology
D
S
59
3
_19_02140
8
FPGA
NC7
S
Z126
O
u
tp
u
t
High-Z Control
I/O Pin
2-mm Connector
BAT54
V
REF_CLAMP
V
REF_CLAMP
3
0.1
Ω
20 k
Ω
To inp
u
t
bu
ffer
D
S
59
3
_20_02140
8
Platform Cable USB II
DS593 (v1.5) June 23, 2015
www.xilinx.com
22
Input Receive Structure
Figure 22
shows the input receive structure. Each input signal is routed through a NC7WZ07 ultra high-speed CMOS, open-
drain receive buffer. Series-termination resistors (499
Ω
) provide current limit protection for positive and negative excursions.
Schottky diodes provide the input buffers with undershoot protection. The receive buffers are biased by an internal 1.8V
power supply. See
Table 9, page 33
for V
IL
and V
IH
specifications. The receive buffers can tolerate voltages higher than the
bias voltage without damage, compensating for target system drivers in multi-device chains where the last device in the
chain might be referenced to a voltage other than V
REF
(for example, the TDO output at the end of a JTAG chain).
X-Ref Target - Figure 21
Figure 21:
Output Drive Voltage vs. V
REF
X-Ref Target - Figure 22
Figure 22:
Target Interface Receiver Topology
O
u
tp
u
t Drive Volt
a
ge (V)
V
REF
Volt
a
ge (VDC)
D
S
59
3
_21_02140
8
FPGA
NC7WZ07
Inp
u
t
I/O Pin
2 mm Connector
BAT54
499
Ω
To o
u
tp
u
t
bu
ffer
D
S
59
3
_22_02140
8
Platform Cable USB II
DS593 (v1.5) June 23, 2015
www.xilinx.com
23
Pseudo Ground Signal in iMPACT
The pseudo ground (PGND) pin on target interface connector is routed to a ultra-high-speed buffer with an open-drain output
(
Figure 23
). A pull-up resistor is required on target systems that utilize this signal. The buffer can tolerate a pull-up voltage
as high as 6.0V.
HALT_INIT_WP Signal in iMPACT
Platform Cable USB II provides a second multi-use signal on its target interface connector called HALT_INIT_WP (this signal
is referred to as HALT when the cable is in JTAG mode). The HALT_INIT_WP pin is connected to a three-state CMOS driver
(see
Bidirectional Signal Pins, page 20
).
The behavior of HALT_INIT_WP is determined by the host application connected to the cable. iMPACT provides the option
of enabling the HALT pin during JTAG operations (
Figure 24
). This option is accessed by clicking on the Xilinx FPGA in the
iMPACT GUI and selecting
Edit
Set Programming Properties...
to open the Device Programming Properties dialog
box. Check “Assert Cable INIT during programming” to enable the HALT signal.
When enabled in iMPACT, HALT is active-Low while the cable is performing JTAG operations on any Xilinx FPGA and high-
Z when the cable is idle. HALT is active-High while JTAG operations are being performed on other devices. The HALT signal
remains high-Z when not enabled (iMPACT default) or when the cable is in slave-serial or SPI modes.
Note:
HALT signal control is available in iMPACT 9.2i and later. The Vivado Design Tools do not support the HALT function. HALT
remains high-Z in earlier versions of iMPACT and in Xilinx design tools where the HALT signal is not supported.
X-Ref Target - Figure 23
Figure 23:
PGND Signal
FPGA
NC7WZ07
PGND_CNTL
PGND
2-mm Connector
D
S
59
3
_2
3
_02150
8
Y
A
Inp
u
t
A
O
u
tp
u
t
Y
H
LL
Z
Platform Cable USB II
DS593 (v1.5) June 23, 2015
www.xilinx.com
24
Timing Specifications
For JTAG, SPI, and slave-serial configuration modes, the TDI_DIN_MOSI and TMS_PROG_SS outputs change on falling
edges of TCK_CCLK_SCK (
Figure 25
). Target devices sample TDI_DIN_MOSI and TMS_PROG_SS on rising edges of
TCK_CCLK_SCK. The minimum setup time T
TSU(MIN)
for target device sampling of TDI_DIN_MOSI or TMS_PROG_SS is:
T
TSU(MIN)
= T
CLK/2
– T
CPD(MAX)
= 20.8 ns – 16.0 ns
= 4.8 ns
where:
T
CLK/2
= TCK_CCLK_SCK low time at 24 MHz,
T
CPD(MAX)
= Maximum TDI_DIN_MOSI or TMS_PROG_SS propagation delay relative to
TCK_CCLK_SCK
inherent in
the output stage of the cable.
Reducing the TCK_CCLK_SCK frequency increases the data setup time at the target.
Note:
Timing specifications apply when V
REF
= 3.3V. Operations at 24 MHz might not be possible when using a V
REF
below 3.3V due to
the increased propagation delay through the output buffer stage of the cable.
TDO/MISO Timing Considerations
Designers of target systems must take care to observe specific timing requirements for TDO (JTAG chains) or MISO
(dedicated SPI in-system programming) when incorporating the 2 mm IDC connector. In particular, if an open-drain or open-
collector buffer is inserted between TDO (MISO) and the cable, the value of the pull-up resistor at the output of such buffers
must be relatively small (for example, less than 330
Ω
) to avoid delays associated with parasitic capacitance.
Figure 26, page 26
and
Figure 27, page 27
show the timing relationship between TCK and TDO. The signal TDO_SMPL is
an internal logic signal not available at the target interface, but is shown to highlight the location of the TDO sampling point.
In
Figure 26
, the negative TCK transition at G1 causes the last device in the target system JTAG chain to drive TDO, which
propagates to the cable at G2. The time from G1 to G2 is the sum of the propagation delays in the driver stage of the target
device and the receiver stage of the cable (37 ns in this example).
In
Figure 27
, the cursors show the total setup time (42 ns) before TDO is sampled by the cable.
Figure 28, page 28
is an
analog representation of the logical condition shown in
Figure 26
and
Figure 27
captured at the target system.
X-Ref Target - Figure 24
Figure 24:
Enabling the HALT Signal in iMPACT (9.2i)
D
S
59
3
_24_02140
8
Platform Cable USB II
DS593 (v1.5) June 23, 2015
www.xilinx.com
25
Note:
The propagation delay from TCK to TDO is 26 ns. Because
Figure 26
shows a propagation delay of 37 ns, the difference of 11 ns
is attributable exclusively to input delays in the cable. At 12 MHz, there is still sufficient setup time before the cable samples prior to the
next negative TCK transition.
X-Ref Target - Figure 25
Figure 25:
TDI_DIN_MOSI and TMS_PROG_SS Timing with Respect to TCK_CCLK_SCK
TM
S
_PROG ch
a
nge
s
on Neg
a
tive
Edge of TCK_CCLK (G1)
TDI_DIN
Ch
a
nge
s
on Neg
a
tive Edge
of TCK_CCLK (G2)
D
S
59
3
_25_02140
8
Platform Cable USB II
DS593 (v1.5) June 23, 2015
www.xilinx.com
26
X-Ref Target - Figure 26
Figure 26:
TDO Sampling Example at 12 MHz (TDO Propagation Delay)
D
S
59
3
_26_02140
8
Neg
a
tive TCK tr
a
n
s
ition
a
t G1 c
aus
e
s
t
a
rget device to
ch
a
nge TDO
s
t
a
te, which prop
a
g
a
te
s
to the c
ab
le
a
t G2 in
le
ss
th
a
n ½ clock cycle in thi
s
12-MHz ex
a
mple.
Platform Cable USB II
DS593 (v1.5) June 23, 2015
www.xilinx.com
27
X-Ref Target - Figure 27
Figure 27:
TDO Sampling Example at 12 MHz (TDO Setup Time Relative to Sampling Point)
D
S
59
3
_27_01150
8
TDO
s
et
u
p time prior to intern
a
l
sa
mpling clock (G2 – G1)
i
s
42n
s
in thi
s
12-MHz ex
a
mple.
Platform Cable USB II
DS593 (v1.5) June 23, 2015
www.xilinx.com
28
Signal Integrity
Platform Cable USB II uses high-slew-rate buffers to drive its output pins. Each buffer has a 30.1
Ω
series termination
resistor. Users should pay close attention to PCB layout to avoid transmission line effects. Visit the
Xilinx Signal Integrity
Central
website for detailed signal integrity assistance.
If the target system has only one programmable device, the 2 mm connector should be located as close as possible to the
target device. If there are multiple devices in a JTAG or slave-serial single chain on the target system, users should consider
buffering TCK_CCLK_SCK. Differential driver/receiver pairs provide excellent signal quality when the rules identified in
Figure 29
are followed. Buffering is essential if target devices are distributed over a large PCB area.
Each differential driver and/or receiver pair contributes approximately 5 ns of propagation delay. This delay is insignificant
when using 12 MHz or slower clock speeds.
X-Ref Target - Figure 28
Figure 28:
TDO Sampling Example at 12 MHz (Analog Signals on Target System)
X-Ref Target - Figure 29
Figure 29:
Differential Clock Buffer Example
D
S
59
3
_2
8
_02140
8
Prop
a
g
a
tion del
a
y from A to B (26 n
s
) c
a
pt
u
red directly
a
t
the t
a
rget repre
s
ent
s
70% of the tot
a
l prop
a
g
a
tion del
a
y
s
een
b
y the c
ab
le (Fig
u
re 25).
TCK
TDO
TDO
S
amplin
g
Point
TDO
S
amplin
g
Point
S
N65LVD
S
105
Fo
u
r Differenti
a
l
Driver
s
S
N65LVD
S
2 (2)
TCK_CCLK_
S
CK
TCK_CCLK_
S
CK1
1
4
TCK_CCLK_
S
CK4
D
S
59
3
_29_02140
8
Loc
a
te driver p
a
ck
a
ge
a
dj
a
cent to 2-mm connector
Ro
u
te A & B tr
a
ce
s
for e
a
ch differenti
a
l
p
a
ir in p
a
r
a
llel with e
qua
l length
a
nd
con
s
i
s
tent
s
p
a
cing
Loc
a
te one receiver
a
d
a
cent
to e
a
ch t
a
rget device
Fo
u
r
B
u
ffered
Clock
s
S
erie
s
Termin
a
tion Re
s
i
s
tor
(20
Ω
3
0
Ω
)
Platform Cable USB II
DS593 (v1.5) June 23, 2015
www.xilinx.com
29
Each differential receiver can drive multiple target devices if there are no branches on the PCB trace and the total trace
length is less than four inches. A series termination resistor should be placed adjacent to the single-ended output of the
differential receiver.
Note:
If the target chain has, for example, a JTAG or slave-serial topology and a 24 MHz clock rate is desired, it is recommended that
matching buffers be used for both TCK_CCLK_SCK and TMS_PROG_SS. Matching buffers maintains a consistent phase relationship
between TCK_CCLK_SCK and TMS_PROG_SS. A buffer is not needed for TDI_DIN_MOSI, because it sees only one load.
USB Hub Types and Cable Performance
There are two important hub specifications affecting the performance of Platform Cable USB II: maximum port current and
total bandwidth.
Maximum Port Current
Platform Cable USB II is a bus-powered device, drawing less than 150 mA from the host USB port under all operating
conditions.
Note:
Some older USB root hubs or external bus-powered hubs might restrict peripherals to 100 mA. Platform Cable USB II cannot
enumerate on hubs with the 100 mA restriction.
Total Bandwidth
The maximum theoretical bandwidth is 480 Mb/s for a single USB 2.0 Hi-Speed device and 12 Mb/s for a single USB 1.1 full-
speed device. However, because hub bandwidth must be shared among all connected devices, actual bandwidth is in
practice lower than these theoretical values.
Platform Cable USB II performance is optimal when enumerated on a USB 2.0 Hi-Speed port. Hi-Speed USB operation is
guaranteed only if the cable is attached directly to a USB 2.0 root hub (
Figure 30E
), or to an external, self-powered USB 2.0
hub connected directly to a USB 2.0 root hub (
Figure 30D
).
If Platform Cable USB II is attached to a USB 1.1 root hub (
Figure 30A
) or to USB 2.0 external hub connected to a USB 1.1
root hub (
Figure 30B
), the cable enumerates as a full-speed device and cable performance is degraded. Communication
and protocol overhead limits any given USB device to approximately 30
%
of total bandwidth. For USB 1.1 hubs, the
maximum achievable throughput is approximately 3.6 Mb/s.
Certain self-powered, USB 2.0 hubs can continue to function as USB 1.1 hubs when disconnected from their external power
source (
Figure 30C
). When no external power source is present, these hubs draw their power from their upstream USB port.
If Platform Cable USB II is connected to such a hub while operating at USB 1.1 speeds, the cable enumerates as a full-
speed device. Furthermore, bus-powered hubs can only deliver a total of 500 mA to all connected devices. If individual ports
on bus-powered hubs are limited to less than 150 mA, Platform Cable USB II does not enumerate and is unavailable for use
by host software applications.
Platform Cable USB II
DS593 (v1.5) June 23, 2015
www.xilinx.com
30
Interface Pin Descriptions
X-Ref Target - Figure 30
Figure 30:
Platform Cable USB II Performance with Various Hub Types
Table
6:
JTAG/SPI/Slave Serial Port: 2 mm Connector Signals
Pin
Number
MODE
Direction
(2)
Description
JTAG
Configuration
SPI
Programming
(1)
Slave-Serial
Configuration
2V
REF
V
REF
V
REF
In
Target Reference Voltage
(3)
. This pin
should be connected to a voltage bus on the
target system that serves the JTAG, SPI, or
slave-serial interface. For example, when
programming a CoolRunner-II device using
JTAG, V
REF
should be connected to the
target V
AUX
bus.
4T
M
S
O
u
t
JTAG Test Mode Select
. This pin is the
JTAG mode signal establishing appropriate
TAP state transitions for target ISP devices
sharing the same data stream.
6T
C
K
O
u
t
JTAG Test Clock
. This pin is the clock
signal for JTAG operations and should be
connected to the TCK pin on all target ISP
devices sharing the same data stream.
8T
D
O
I
n
JTAG Test Data Out
. This pin is the serial
data stream received from the TDO pin on
the last device in a JTAG chain.
1.X Root H
ub
12 M
b
/
s
B
us
S
peed
1.X Root H
ub
2.0 Root H
ub
4
8
0 M
b
/
s
B
us
S
peed
2.0 Extern
a
l
B
us
-Powered
H
ub
12 M
b
/
s
B
us
S
peed
2.0 Extern
a
l
S
elf-Powered
H
ub
2.0 Root H
ub
4
8
0 M
b
/
s
B
us
S
peed
2.0 Extern
a
l
S
elf-Powered
H
ub
500
mA
500
mA
< 500
mA
500
mA
500
mA
< 500
mA
2.0 Root H
ub
500
mA
4
8
0 M
b
/
s
B
us
S
peed
500
mA
(A)
(B)
(C)
(D)
(E)
Power
D
S
59
3
_
3
0_02140
8
Power
U
S
B II
Pl
a
tform C
ab
le
U
S
B II
Pl
a
tform C
ab
le
U
S
B II
Pl
a
tform C
ab
le
U
S
B II
Pl
a
tform C
ab
le
U
S
B II
Pl
a
tform C
ab
le
En
u
mer
a
te
s
a
t
f
u
ll
s
peed
b
ec
aus
e
root h
ub
only
oper
a
te
s
a
t f
u
ll
s
peed — degr
a
ded
perform
a
nce d
u
e
to
s
low
bus
s
peed
En
u
mer
a
te
s
a
t
f
u
ll
s
peed
b
ec
aus
e
root h
ub
only
oper
a
te
s
a
t f
u
ll
s
peed — degr
a
ded
perform
a
nce d
u
e
to
s
low
bus
s
peed
En
u
mer
a
te
s
a
t f
u
ll
s
peed
b
ec
aus
e 2.0 extern
a
l
h
ub
oper
a
te
s
a
t f
u
ll
s
peed — degr
a
ded
perform
a
nce d
u
e to
s
low
bus
s
peed. C
ab
le m
a
y
not en
u
mer
a
te.
En
u
mer
a
te
s
a
t
Hi-
S
peed —
b
e
s
t
perform
a
nce d
u
e to
high
bus
s
peed.
En
u
mer
a
te
s
a
t
Hi-
S
peed —
b
e
s
t
perform
a
nce d
u
e to
high
bus
s
peed.
Platform Cable USB II
DS593 (v1.5) June 23, 2015
www.xilinx.com
31
10
TDI
Out
JTAG Test Data In
. This pin outputs the
serial data stream transmitted to the TDI pin
on the first device in a JTAG chain.
13
PGND
Out
JTAG Pseudo Ground.
Use of this pin is
optional. PGND is pulled Low during JTAG
operations; otherwise, it is high-Z. This pin is
connected to an open-drain driver and
requires a pull-up resistor on the target
system.
(4)
14
HALT
Out
JTAG Halt. Use of this pin is optional. Host
applications can customize the behavior of
this signal. See
HALT_INIT_WP Signal in
iMPACT, page 23
.
4–
S
S
O
u
t
SPI Select
. This pin is the active-Low SPI
chip select signal and should be connected
to the S
(1)
pin on the SPI flash device.
6–
S
C
K
O
u
t
SPI Clock
. This pin is the clock signal for
SPI operations and should be connected to
the C
(1)
pin on the SPI flash PROM.
8–
M
I
S
O
I
n
SPI Master-Input, Slave-Output
. This pin
is the target serial output data stream and
should be connected to the Q
(1)
pin on the
SPI flash device.
10
MOSI
Out
SPI Master-Output Slave-Input
. This pin
outputs the target serial input data stream
for SPI operations and should be connected
to the D
(1)
pin on the SPI flash device.
13
PGND
Out
SPI Pseudo Ground
. PGND is pulled Low
during SPI operations; otherwise, it is high-
Z. When connected to PROG_B on an
FPGA, the FPGA will high-Z its SPI signals
while the cable is programming the SPI
flash. This pin is connected to an open-drain
driver and requires a pull-up resistor on the
target system.
(4)
14
WP
SPI Write Protect
. This pin is reserved for
future use. Do not connect for SPI
programming.
4–
P
R
O
G
O
u
t
Slave Serial Configuration Reset
. This pin
is used to force a reconfiguration of the
target FPGA(s) and should be connected to
the PROG_B pin of the target FPGA for a
single-device system, or to the PROG_B pin
of all FPGAs in parallel in a daisy-chain
configuration.
6
CCLK
Out
Slave Serial Configuration Clock
. FPGAs
load one configuration bit per CCLK cycle in
slave-serial mode. CCLK should be
connected to the CCLK pin on the target
FPGA for single-device configuration, or to
the CCLK pin of all FPGAs in parallel in a
daisy-chain configuration.
Table
6:
JTAG/SPI/Slave Serial Port: 2 mm Connector Signals
(Cont 'd)
Pin
Number
MODE
Direction
(2)
Description
JTAG
Configuration
SPI
Programming
(1)
Slave-Serial
Configuration
Platform Cable USB II
DS593 (v1.5) June 23, 2015
www.xilinx.com
32
Platform Cable USB II Operating Characteristics
8–
D
o
n
e
I
n
Slave Serial Configuration Done
. This pin
indicates to Platform Cable USB II that
target FPGAs have received the entire
configuration bitstream and should be
connected to the Done pin on all FPGAs in
parallel for daisy-chained configurations.
Additional CCLK cycles are issued following
the positive transition of Done to insure that
the configuration process is complete.
10
DIN
Out
Slave Serial Configuration Data Input
.
This pin outputs the serial input data stream
for target FPGAs and should be connected
to the DIN pin of the target FPGA in a single-
device system, or to the DIN pin of the first
FPGA in a daisy-chain configuration.
13
PGND
Out
Slave Serial Pseudo Ground.
Use of this
pin is optional. PGND is pulled Low during
slave-serial operations; otherwise, it is high-
Z. This pin is connected to an open-drain
driver and requires a pull-up resistor on the
target system.
(4)
14
INIT
In
Slave Serial Configuration Initialization
.
This pin indicates that configuration memory
is being cleared and should be connected to
the INIT_B pin of the target FPGA for a
single-device system, or to the INIT_B pin
on all FPGAs in parallel in a daisy-chain
configuration.
3, 5, 7, 9,
11
––––
Digital Ground
. All ground pins should be
connected to digital ground on the target
system to minimize crosstalk.
1, 12
Not Connected.
Notes:
1.
The listed SPI pin names match those of SPI flash devices from ST Microelectronics. Pin names of compatible SPI devices from other
vendors can vary. Consult the vendor's SPI device data sheet for equivalent pin names.
2.
The signal pins (HALT_INIT_WP, TDI_DIN_MOSI, TDO_DONE_MISO, TCK_CCLK_SCK, TMS_PROG_SS) are bidirectional. Their
directions during cable operations are defined by the current configuration or programming mode (JTAG, SPI, or slave-serial).
3.
The target reference voltage must be regulated and not have a current-limiting resistor in series with the V
REF
pin.
4.
For more details, see
Target System Connections, page 16
and
Pseudo Ground Signal in iMPACT, page 23
.
Table
7:
Absolute Maximum Ratings
(1)
Symbol
Description
Conditions
Value
Units
V
BUS
USB Port Supply Voltage
5.25
V
V
REF
Target Reference Voltage
6.00
V
I
REF
Target Supply Current
V
REF
= 5.25V
100
mA
T
A
Ambient Operating Temperature
70
°
C
Table
6:
JTAG/SPI/Slave Serial Port: 2 mm Connector Signals
(Cont 'd)
Pin
Number
MODE
Direction
(2)
Description
JTAG
Configuration
SPI
Programming
(1)
Slave-Serial
Configuration
Platform Cable USB II
DS593 (v1.5) June 23, 2015
www.xilinx.com
33
I
OUT
DC Output Current (TCK_CCLK_SCK,
TMS_PROG_SS, TDI_DIN_MOSI, and
INIT)
±24
±mA
Notes:
1.
Exposure to absolute rating conditions for extended periods of time can affect product reliability. The values listed in this table are stress
ratings only. Functional operation of the product at these or any other conditions beyond those listed under
Table 8
: Recommended DC
Operating Conditions is not implied or recommended.
Table
8:
Recommended DC Operating Conditions
Symbol
Description
Conditions
Min
Max
Units
V
BUS
USB Port Supply Voltage
4.00
5.25
V
V
REF
Target Reference Voltage
1.5
5.00
V
T
A
Ambient Operating Temperature
0
70
o
C
T
STG
Storage Temperature
–40
+85
o
C
Table
9:
DC Electrical Characteristics
Symbol
Description
Conditions
Min
Max
Units
I
REF
Target Supply Current
V
REF
= 3.3V
15
mA
V
REF
= 2.5V
3
V
REF
= 1.8V
1
V
REF
= 1.5V
1
V
OH
High-Level Output Voltage
V
REF
= 3.3V; I
OH
= –8 mA
2.25
V
V
REF
= 2.5V; I
OH
= –8 mA
2.15
V
REF
= 1.8V; I
OH
= –8 mA
1.55
V
REF
= 1.5V; I
OH
= –8 mA
1.30
V
OL
Low-Level Output Voltage
V
REF
= 3.3V; I
OH
= 16 mA
0.40
V
V
REF
= 2.5V; I
OH
= 8 mA
0.30
V
REF
= 1.5V; I
OH
= 4 mA
0.24
V
IH
High-Level Input Voltage
V
REF
= 1.5V to 3.3V
1.35
V
V
IL
Low-Level Input Voltage
V
REF
= 1.5V to 3.3V
0.45
V
I
CC1
Dynamic Current
(1)
V
BUS
= 5.25V: TCK = 24 MHz
85
110
mA
I
CC2
Dynamic Current
(2)
V
BUS
= 5.25V; TCK = 6 MHz
85
100
mA
I
CCSU
Suspend Current
V
BUS
= 5.25V
250
350
μ
A
Notes:
1.
Operating at Hi-Speed on a USB 2.0 port.
2.
Operating at full-speed on a USB 1.1 port.
Table
10:
Switching Characteristics
Symbol
Description
Conditions
Min
Max
Units
T
CLK
Clock Period
TCK
750 kHz
1333
ns
24 MHz
41.66
ns
T
CPD
Cable Propagation Delay Time
(TDI or TMS relative to the negative
edge of TCK)
V
REF
= 1.5V to 3.3V
16
ns
Table
7:
Absolute Maximum Ratings
(1)
(Cont 'd)
Symbol
Description
Conditions
Value
Units
Platform Cable USB II
DS593 (v1.5) June 23, 2015
www.xilinx.com
34
USB-IF Compliance
Platform Cable USB II is certified by the USB Integrators Forum (USB-IF). Certification is achieved when a product passes
a battery of tests required by the USB-IF Compliance Program. These tests (performed at an independent test facility)
measure a product's conformity with Universal Serial Bus Specification Revision 2.0 and establish a reasonable level of
T
TSU
Target Setup Time
(TDI or TMS relative to the
positive edge of TCK)
V
REF
= 1.5V to 3.3V
4.8
ns
T
CSU
Cable Setup Time
(TDO relative to the
negative edge of TCK)
V
REF
= 1.5V to 3.3V
15.8
ns
T
TPD
Target Propagation Delay Time
(TDO relative to the
negative edge of TCK)
V
REF
= 1.5V to 3.3V
24.6
ns
X-Ref Target - Figure 31
Notes:
1.
All times are in nanoseconds and are relative to the target system interface connector.
2.
T
TSU
Min is the minimum setup time guaranteed by Platform Cable USB II relative to the positive edge of TCK_CCLK_SCK.
3.
T
CSU
Min is the minimum setup required by Platform Cable USB II to properly sample TDO_DONE_MISO.
4.
Propagation delays associated with buffers on the target system must be taken into account to satisfy the minimum setup times.
Figure 31:
Platform Cable USB II Timing Diagram
Table
10:
Switching Characteristics
(Cont 'd)
Symbol
Description
Conditions
Min
Max
Units
T
a
rget device
s
sa
mple
s
TM
S
_PROG_
SS
a
nd
TDI_DIN_MO
S
I on the ri
s
ing edge of TCK_CCLK_
S
CK
T
CLK
T
T
S
U
T
CPD
TCK_CCLK_
S
CK
TM
S
_PROG_
SS
/
TDI_DIN_MO
S
I
TDO_DONE_MI
S
O
Pl
a
tform C
ab
le U
S
B II
ass
ert
s
TM
S
_PROG_
SS
a
nd
TDI_DIN_MO
S
I on the f
a
lling
edge of TCK_CCLK_
S
CK
T
TPD
Pl
a
tform C
ab
le U
S
B II
sa
mple
s
TDO_DONE_MI
S
O
on the f
a
lling edge of TCK_CCLK_
S
CK
T
C
S
U
T
a
rget device
ass
ert
s
TDO_DONE_MI
S
O
on the f
a
lling edge of TCK_CCLK_
S
CK
D
S
59
3
_
3
1_02140
8
Platform Cable USB II
DS593 (v1.5) June 23, 2015
www.xilinx.com
35
acceptability. Products that pass this level of acceptability are added to the USB-IF Integrator's List and receive the rights of
usage for the USB logo.
FCC Notice
This equipment has been tested and found to comply with the limits for a Class A digital device, pursuant to Part 15 of the
FCC Rules. These limits are designed to provide reasonable protection against harmful interference when the equipment is
operated in a commercial environment. This equipment generates, uses, and can radiate radio frequency energy and, if not
installed and used in accordance with the data sheet, could cause harmful interference to radio communications. Operation
of this equipment in a residential area is likely to cause harmful interference, in which case, the user is required to correct the
interference at his own expense.
Industry Canada Information
This Class A digital apparatus complies with Canadian ICES-003.
Ordering Information
Platform Cable USB II ships with each of the items shown in
Table 11
plus a 1.8-meter, Hi-Speed USB, A-B cable.
Marking Information
Table
11:
Ordering Information
Item
Product Number
Platform Cable USB II
HW-USB-II-G
Ribbon Cable, 6-inch
HW-RIBBON14
Flying Wire Set
HW-USB-FLYLEADS-G
Table
12:
Marking Information
Model Name
Serial Prefix
Description
DLC10
XU
Platform Cable USB II
Platform Cable USB II
DS593 (v1.5) June 23, 2015
www.xilinx.com
36
Revision History
The following table shows the revision history for this document:
Notice of Disclaimer
The information disclosed to you hereunder (the “Materials”) is provided solely for the selection and use of Xilinx products. To the
maximum extent permitted by applicable law: (1) Materials are made available "AS IS" and with all faults, Xilinx hereby DISCLAIMS ALL
WARRANTIES AND CONDITIONS, EXPRESS, IMPLIED, OR STATUTORY, INCLUDING BUT NOT LIMITED TO WARRANTIES OF
MERCHANTABILITY, NON-INFRINGEMENT, OR FITNESS FOR ANY PARTICULAR PURPOSE; and (2) Xilinx shall not be liable
(whether in contract or tort, including negligence, or under any other theory of liability) for any loss or damage of any kind or nature related
to, arising under, or in connection with, the Materials (including your use of the Materials), including for any direct, indirect, special,
incidental, or consequential loss or damage (including loss of data, profits, goodwill, or any type of loss or damage suffered as a result of
any action brought by a third party) even if such damage or loss was reasonably foreseeable or Xilinx had been advised of the possibility
of the same. Xilinx assumes no obligation to correct any errors contained in the Materials or to notify you of updates to the Materials or to
product specifications. You may not reproduce, modify, distribute, or publicly display the Materials without prior written consent. Certain
products are subject to the terms and conditions of Xilinx's limited warranty, please refer to Xilinx's Terms of Sale which can be viewed at
www.xilinx.com/legal.htm#tos
; IP cores may be subject to warranty and support terms contained in a license issued to you by Xilinx. Xilinx
products are not designed or intended to be fail-safe or for use in any application requiring fail-safe performance; you assume sole risk and
liability for use of Xilinx products in such critical applications, please refer to Xilinx's Terms of Sale which can be viewed at
www.xilinx.com/legal.htm#tos
.
Date
Version
Description of Revisions
03/03/2008
1.0
Initial Xilinx release.
05/14/2008
1.1
• Updated trademark references.
• Added support for Platform Flash XL.
06/09/2008
1.2
Corrected the functional descriptions of pins
6
and
8
in
Table 6, page 30
.
03/17/2011
1.2.1
Converted document to latest template containing current Xilinx logos and colors.
06/25/2014
1.3
Updated support information for Xilinx tools and added references to the Vivado Design Suite
throughout the data sheet. Updated the devices listed in
Table 3
. Updated the
Notice of Disclaimer
.
01/16/2015
1.4
Updated note for 24 MHz in
Table 2
. Updated notes about PGND in
JTAG and Slave Serial
. Removed
obsolete XC4000, XC9500, XC9500XV, and Spartan devices from
Features
,
Table 3
, and
Signal
Integrity
.
06/23/2015
1.5
In
Figure 16
, removed note 6 about the Vivado tools not supporting the cable PGND signal. In
Pseudo
Ground Signal in iMPACT
, removed sentences stating that the Vivado tools do not support the PGND
function.