Piezoelectric Ceramics: Driving the Silent Interaction Revolution
Piezoelectric ceramics, a functional ceramic material capable of mutually converting mechanical energy and electrical energy, have the piezoelectric effect at their core.
Bestar Holdings' piezoelectric ceramic technology is built upon a dual effect: the direct piezoelectric effect, where the material generates an electric charge when subjected to mechanical stress, realizing the conversion of mechanical energy to electrical energy; and the inverse piezoelectric effect, where the material undergoes precise deformation when an electric field is applied, realizing the conversion of electrical energy to mechanical energy (Figure 1).
Figure 1: The piezoelectric effect converts mechanical energy to electric energy and vice versa. (Image source: BeStar Technologies, Inc.)
This bidirectional characteristic allows a single piezoelectric ceramic component to possess both sensing and actuation functions simultaneously. When a finger presses the surface, the piezoelectric ceramic layer converts the minute deformation into an electric charge signal to recognize the touch intent; upon receiving an instruction, it can then deform at microsecond speed, producing a vibration feedback that mimics a physical button. Bestar Holdings has achieved a balanced breakthrough in these parameters through material formulation and process optimization.
Precision, Reliability, and the Instantaneous Interaction Revolution
Compared to traditional moving coil and moving iron units, piezoelectric ceramics possess superior response speed. Piezoelectric units are directly driven, resulting in minimal energy loss, whereas moving coil and moving iron units must first convert the current into vibration under the action of a magnetic field, leading to greater energy loss. In smart automotive surface applications, Bestar Holdings' piezoelectric ceramic solution demonstrates multiple advantages:
- High Sensitivity and Accurate Sensing: Capable of recognizing subtle pressure changes and accurately capturing the touch intent
- All-Weather Stability: Remains reliable in extreme environments, unperturbed by fluctuations in cabin temperature and humidity
- Low Power Consumption: The direct drive mechanism consumes significantly less energy than traditional motor-based solutions
- Microsecond Response: The touch feedback delay is virtually imperceptible, achieving an intuitive "press-and-receive-feedback" experience
Diverse Integration from Smart Cockpits to Acoustic Systems
In the field of electric vehicle smart cockpits, Bestar Holdings' piezoelectric ceramic technology is redefining the human-vehicle interaction method. The smart cockpit interaction is a core application scenario. Used for window controls, steering wheel buttons, dome light adjustment, and other functions, a seamless surface conceals a precise piezoelectric layer that responds to a light touch, offering designers boundless creative space. Clear haptic feedback during blind operation in rain or snow is safer, resolving the issue of visual distraction caused by traditional touchscreens while driving.
Meanwhile, the acoustic system is another important application area. In the headphone sector, ceramic units have been a new star in recent years. Piezoelectric ceramic units are responsible for high-frequency compensation, while moving coil units handle low and mid-frequencies. This combination significantly enhances sound layering and detail reproduction, delivering a more transparent and clear treble, making it an excellent partner for moving coil units.
Figure 2: Piezoelectric ceramics are used in a wide variety of applications. (Image source: BeStar Technologies, Inc.)
The Exquisite Combination of Materials Science and Firing Technology
The manufacturing of piezoelectric ceramics is a precise process, encompassing multiple steps including compounding, mixing and milling, calcination (pre-sintering), secondary milling, granulation, forming, binder burnout, ceramic sintering, shaping and processing, electrode application, and high-voltage poling. The sintering process is the critical step that determines the performance of the piezoelectric ceramics.
Moreover, as environmental requirements increase, lead-free piezoelectric ceramics are becoming a major direction for development. Bestar Holdings is actively responding to this trend, promoting green development in the industry. These technological innovations and the manufacturing process of piezoelectric ceramics complement each other, collectively driving industry progress.
As smart cockpits evolve into a "third mobile space," Bestar Holdings' piezoelectric ceramic technology, with its ultimate reliability, design freedom that breaks physical constraints, and all-weather stable interaction performance, is accelerating the replacement of traditional buttons. In the future, with continuous breakthroughs in new materials and processes, especially the further improvement of lead-free and high-temperature stability, the application boundaries of piezoelectric ceramics will continue to expand.
Summary
From more precise medical diagnostic equipment to smarter home appliance interaction, from safer driving experiences to more immersive acoustic systems, this material—piezoelectric ceramics—will continue to profoundly change our way of life.
To obtain more technical and product details from BeStar Technologies, Inc.: https://www.digikey.com/en/products/result?s=N4IgTCBcDaIEIFMDKAXAhgJwAQBUEGMALAOwHsAbUgcwEsEBnQGH%2BsBJY-AOhAF0BfIA
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.
Visit TechForum