Nova Quickstart Guide Datasheet by Hologram, Inc.

View All Related Products | Download PDF Datasheet
(850/900/‘900/2‘00Mhz). Emma... nun. _| Hologram — a mu : K K L.. g . _ *3 D £2 =:: n I'_/
The modem is currently booting up
and may take approximately 20s
There is no power being supplied to
the modem. Make sure your modem
is plugged into a valid USB host
device
The modem is powered on and has
booted up
OFF
OR
ON
NETWORK LED
ANTENNA (UFL) PORT
POWER LED
POWER LED (RED)
No network detected. Make sure the
antenna is securely connected and
the SIM is fully inserted
It may take up to 200s for a network
to be detected
If no networks are detected, the
network status indicator LED will
remain o
Make sure your antenna is well
positioned to receive cell signal
2G network detected
3G network detected
Modem has an active data session
OFF
DOUBLE
BLINK
RAPID
BLINK
SOLID
NETWORK LED (BLUE) NOVA AND HOLOGRAM CLICLI QUICK REFERENCE
The following installation instructions are
geared toward use with Raspbian on the
Raspberry Pi. For information on working with
additional host devices, visit: hologram.io/nova
The Hologram Command Line Interface (CLI)
and Python SDK are downloadable via
curl from your Linux terminal:
curl -L hologram.io/python-install | bash
To update to the latest version:
curl -L hologram.io/python-update | bash
Once installed, you can immediately send data
to the Hologram cloud:
sudo hologram send “Hello World”
Messages can then be viewed and routed to
di erent destinations at:
dashboard.hologram.io
For a full list of commands
hologram --help
Receive inbound messages
(send from the Hologram Dashboard)
sudo hologram receive
Bring a connection up/down
sudo hologram modem connect
sudo hologram modem disconnect
Check signal strength
sudo hologram modem signal
Check network operator
sudo hologram modem operator
Send a message with a topic
sudo hologram send <message> -t <topic>
Get u-blox CellLocate location
sudo hologram modem location
For additional information on utilizing the
Hologram CLI and Python SDK, visit:
hologram.io/nova
NOVA QUICKSTART GUIDEINSERT ACTIVATED SIM ATTACH THE ANTENNAENCLOSURE (OPTIONAL)
For additional setup instructions
and information, visit:
hologram.io/nova
Before use, your Hologram SIM
needs to be activated.
To activate, visit:
hologram.io/start
NOTICE: Do not insert or remove
the SIM while the Nova is plugged
in - otherwise, the SIM may become
damaged or corrupt.
The two included antennas have
standard UFL connectors and work
globally over 2G/3G networks.
(850/900/1900/2100Mhz).
Inserting the Nova into the
transparent enclosure is optional
Before enclosing the Nova, insert a
SIM and connect the antenna.
1. ATTACH
ANTENNA
2. PLACE BOARD
IN BOTTOM TRAY FIRST
ANTENNA OUTSIDE CASE
FOR BEST RECEPTION
ANTENNA OPTIONALLY
FITS IN THE CASE
INS E R T SIM - B O T T OM VIEW
The larger black antenna provides
better reception, while the smaller
yellow antenna has the benefit of fitting
inside the case.

Products related to this Datasheet

RX TXRX MODULE CELL 3G AT&T
RX TXRX MODULE CELL 4G VERIZON