AN049 Getting Started Guide Datasheet by Kionix Inc.

View All Related Products | Download PDF Datasheet
‘ AN049 K I o n IX § I | __c. 1! IS 14 IO Vfld—Q— P I: TRIG C: — 2 12—0 ¥ 3 KX123 ‘1 III“ KX124 scmsu 4 w _ 6— 5 9 INT? 6 7 I __ ( g VI _ g . g 5 § 36 Tharnwood Dr. — Ithaca, NY 14850 USA © Kionix 2019 AN nghts Reserved Tel: 607-257-1080 — Fax: 607-257-1146 019 www.kianix.cam — infoQkioniXLam 1
AN049
Getting Started
36 Thornwood Dr. Ithaca, NY 14850 USA
Tel: 607-257-1080 Fax: 607-257-1146
www.kionix.com info@kionix.com
© Kionix 2019 All Rights Reserved
11 July 2019
Page 1 of 21
1. Introduction
This application note will help developers quickly implement proof-of-concept designs using the
KX112, KX122, KX123 and KX124 tri-axis accelerometers. Please refer to the corresponding
Product Specifications document for additional implementation guidelines. Kionix strives to ensure
that our accelerometers will meet design expectations by default, but it is not possible to provide
default setting to work in every environment. Depending on the intended application, it is very likely
that some customization will be required to optimize performance. The information provided here will
help the developer get the most out of these tri-axis accelerometers.
2. Circuit Schematic
This section shows recommended wiring for this family of accelerometers, based on proven
operation of the part. Specific applications may require modifications from these recommendations.
Please refer to the corresponding Product Specifications document for all pin descriptions.
Figure 1: KX123, KX124 Application Schematic
SDOIADDR<—-1;_\ 12="" 11="" 1o="" sdi/sda.—.2="" kx112="" 9="" io_voo:e3="" kx122="" 8="" trig="" c2="" 4="" 5="" 6="" 7="" l="" v="" '="" lnt1="" int2="" f‘="" ktanix'="" ©="" kionix="" 2019="" all="" rights="" reserved="" 019="" 1="">
AN049
© Kionix 2019 All Rights Reserved
11 July 2019
Page 2 of 21
Figure 2: KX112, KX122 Application Schematic
f‘ KTonix' Register Name Address Value ODCNTL 0X1 B 0X02 CNTL1 0X13 OXCO © Kionix 2019 All Right; Reserved 019 1
AN049
© Kionix 2019 All Rights Reserved
11 July 2019
Page 3 of 21
3. Quick Start Implementations
Here we present several basic ways to initialize the part. These can vary based on desired operation,
but generally the initial operations a developer wants to do are: 1) read back acceleration data
asynchronously, 2) read back acceleration data when next data is ready via interrupt (synchronous
data reading), 3) use of the sample buffer, 4) use the Wake-Up function, 5) activate the tilt position
function, 6) activate the tap/double-tap function, and 7) activate the free-fall function. These cursory
solutions are provided as a means for configuring the part to a known operational state. Note that
these conditions just provide a starting point, and the values may vary as developers refine their
application requirements.
4. Asynchronous Read Back Acceleration Data (Setting G-Range and ODR)
- Write 0x40 to Control Register 1 (CNTL1) to set the accelerometer in stand-by mode, to set
the performance mode to High Resolution (full power) and G-range to ±2g.
Register Name
Value
CNTL1
0x40
- Write 0x02 to Data Control Register (ODCNTL) to set the Output Data Rate (ODR) of the
accelerometer to 50 Hz. (Note: This is also the default value.)
Register Name
Value
ODCNTL
0x02
- Write 0xC0 to Control Register 1 (CNTL1) to set the accelerometer into operating mode (PC1
= 1)
Register Name
Value
CNTL1
0xC0
- Acceleration data can now be read from the XOUT_L, XOUT_H, YOUT_L, YOUT_H,
ZOUT_L, and ZOUT_H registers in 2’s complement format.
f‘ KTonix‘ Register Name Address Value |NC1 0X1C 0X38 |NC4 0X1 F 0X1 0 ODCNTL 0X1 B 0X02 Register Name Address Value CNTL1 0X18 OXEO © Klonix 2019 All Rights Reserved 019 1
AN049
© Kionix 2019 All Rights Reserved
11 July 2019
Page 4 of 21
5. Synchronous Hardware Interrupt Read Back Acceleration Data (Setting G-
Range and ODR)
- Write 0x60 to Control Register 1 (CNTL1) to set the accelerometer in stand-by mode, to set
the performance mode to High Resolution (full power), G-range to ±2g enable the availability
of new data as an interrupt.
Register Name
Value
CNTL1
0x60
- Write 0x38 to Interrupt Control Register (INC1) to enable physical interrupt pin INT1, to set
the polarity of the physical interrupt to active high and to transmit interrupt pulses with a
period of 0.03 to 0.05 msec.
Register Name
Value
INC1
0x38
- Write 0x10 to Interrupt Control Register 4 (INC4) to set the Data Ready interrupt to be
reported on physical interrupt pin INT1.
Register Name
Value
INC4
0x10
- Write 0x02 to Output Data Rate (ODR) Control Register (ODCNTL) to set the ODR of the
accelerometer to 50 Hz. (Note: This is also the default value.)
Register Name
Value
ODCNTL
0x02
- Write 0xE0 to Control Register 1 (CNTL1) to set the accelerometer into operating mode (PC1
= 1)
Register Name
Value
CNTL1
0xE0
- Acceleration data can now be read from the XOUT_L, XOUT_H, YOUT_L, YOUT_H,
ZOUT_L, and ZOUT_H registers in 2’s complement format. Also, the interrupt would be
reflected in Bit4 (INT) of STATUS_REG and Bit4 (DRDY) in INS2 register.
f‘ KTonix‘ Register Name Address Value |NC1 0X1C 0X38 |NC4 0X1 F 0X40 ODCNTL 0X1 B 0X02 BUFicNTLZ 0X38 OXAO CNTL1 0X18 0X80 © Klonix 2019 All Rights Reserved 019 1
AN049
© Kionix 2019 All Rights Reserved
11 July 2019
Page 5 of 21
6. Sample Buffer Operation
6.1. Sample Buffer-Full Interrupt via Physical Hardware Interrupt
- Write 0x00 to Control Register 1 (CNTL1) to set the accelerometer in stand-by mode, to
set the performance mode of the accelerometer to Low Power mode, and G-range to ±2g.
Register Name
Value
CNTL1
0x00
- Write 0x38 to Interrupt Control Register (INC1) to enable physical interrupt pin INT1, to set
the polarity of the physical interrupt to active high and to transmit interrupt pulses with a
period of 0.03 to 0.05 msec.
Register Name
Value
INC1
0x38
- Write 0x40 to Interrupt Control Register 4 (INC4) to set the Buffer Full interrupt to be
reported on physical interrupt pin INT1.
Register Name
Value
INC4
0x40
- Write 0x02 to Output Data Rate (ODR) Control Register (ODCNTL) to set the ODR of the
accelerometer to 50 Hz. (Note: This is also the default value.)
Register Name
Value
ODCNTL
0x02
- Write 0xA0 to Buffer Control Register 2 (BUF_CNTL2) to activate the sample buffer, to set
the resolution of the acceleration data samples collected to 8 bits, to enable report of the
interrupt status in INS2, and set the operating mode of the sample buffer to FIFO.
Register Name
Value
BUF_CNTL2
0xA0
- Write 0x80 to Control Register 1 (CNTL1) to set the accelerometer into operating mode
(PC1 = 1)
Register Name
Value
CNTL1
0x80
- Once Buffer-Full Interrupt is issued on INT1 pin, acceleration data can then be read from
the Buffer Read (BUF_READ) register at address 0x3F in 2’s complement format. Also,
the interrupt would be reflected in Bit4 (INT) of STATUS_REG register and Bit6 (BFI) of
INS2 register. Since the resolution of the samples data was set to 8-bit, only the most
significant 8 bits of each sample will be stored in the buffer, and recorded in the following
order: X_HIGH, Y_HIGH, Z_HIGH with the oldest data point read first as it is a FIFO
buffer. The full buffer contains 2043 X, Y, Z elements, which corresponds to 681 unique
acceleration data samples.
Register Name Address Value Register Name Address Value Register Name Address Value ODCNTL 0X1 B 0X02 int smp_th : 339; char smp_th_l : (smp_th 8. exFF); BUFicNTL1 0X3A 0X53 ‘ © Klonix 2019 All Rights Reserved e . g 019 KlOnIX 1
AN049
© Kionix 2019 All Rights Reserved
11 July 2019
Page 6 of 21
6.2. Trigger Mode Buffer Operation
- Ensure that the TRIG pin is can be controlled via hardware or software. The pin should be
held low (inactive state) and be driven high to activate the internal trigger event.
- Write 0x00 to Control Register 1 (CNTL1) to set the accelerometer in stand-by mode, to
set the performance mode of the accelerometer to Low Power mode, and G-range to ±2g.
Register Name
Value
CNTL1
0x00
- Write 0x38 to Interrupt Control Register (INC1) to enable physical interrupt pin INT1, to set
the polarity of the physical interrupt to active high and to transmit interrupt pulses with a
period of 0.03 to 0.05 msec.
Register Name
Value
INC1
0x38
- Write 0x40 to Interrupt Control Register 4 (INC4) to set the Buffer Full interrupt to be
reported on physical interrupt pin INT1.
Register Name
Value
INC4
0x40
- Write 0x02 to Data Control Register (ODCNTL) to set the Output Data Rate (ODR) of the
accelerometer to 50 Hz. (Note: This is also the default value).
Register Name
Value
ODCNTL
0x02
- Choose desired number of samples to collect before and after a trigger event. To begin,
we need to know the capacity of the buffer. The buffer has the capability of storing 2048
bytes of data. Design constraints limit the number of samples in the buffer to
rounddown(2048/dataset_in_bytes)-1. Consider 16-bit data being stored into the buffer
and a complete dataset_in_bytes=6 (3 axes * 2 bytes/axis). The resulting number of
samples that can be stored in the buffer is rounddown(2048/6)-1=340. For this example,
we will save time by only collecting a single sample after a trigger event. This means we
need to set a threshold of 339 samples (340-339=1 sample of data after a trigger event).
The sample threshold is stored in register space across 2 different registers BUF_CNTL1
(lower 8 bits) and BUF_CNTL2 (bits 9 and 10). The following is an illustration of what
values need to be written to the buffer threshold low and high bytes:
int smp_th = 339;
char smp_th_l = (smp_th & 0xFF); // 0x53
char smp_th_h = ((smp_th >> 8) & 0xFF); // 0x01
- Write 0x53 to Buffer Control Register 1 (BUF_CNTL1) as this is the value for
BUF_TH[7:0].
Register Name
Value
BUF_CNTL1
0x53
BUFicNTL2 0X38 buLcnflZ Register Name Address Value (WRITE) Register Name Address Value (READ) buficntlz |= BUFiCNTinBUFE l // Sample buffer active (1 < 7)="" buficntinbres="" l="" lérbit="" samples="" in="" buffer="" (1="">< 6="" buficntinbfie="" l="" buffer="" full="" int="" enable="" (1="">< register="" name="" address="" value="" (write)="" register="" name="" address="" value="" ©="" klonix="" 2019="" all="" rights="" reserved="" e="" .="" g="" 019="" klclan="" 1="">
AN049
© Kionix 2019 All Rights Reserved
11 July 2019
Page 7 of 21
- Read the contents of the Buffer Control Register 2
char buf_cntl2;
Register Name
Value (READ)
BUF_CNTL2
buf_cntl2
- Bit mask clear SMP_TH[9:8] from the value returned from the previous step.
BITMASK_CLEAR(buf_cntl2, (0x3 << 2)); // #define BITMASK_CLEAR(x,y) ((x) &= (~(y)))
- Logically OR and Bit Shift the new bit settings (smp_th_h) with the current value of
BUF_CNTL2.
buf_cntl2 |= (smp_th_h << 2);
- Write the new value of Buffer Control Register 2 (BUF_CNTL2). If starting with default values
the value of buf_cntl2 should be 0x04.
Register Name
Value (WRITE)
BUF_CNTL2
buf_cntl2
- Read the new contents of the Buffer Control Register 2
char buf_cntl2;
Register Name
Value (READ)
BUF_CNTL2
buf_cntl2
- Update and write the new bit settings in Buffer Control Register 2 (BUF_CTL2) to activate the
sample buffer, to set the resolution of the acceleration data samples collected to 16 bits, to
enable report of the buffer full interrupt status in INS2, and set the operating mode of the
sample buffer to Trigger Mode. If starting with default values the value of buf_cntl2 should be
0xE6.
buf_cntl2 |=
BUF_CNTL2_BUFE | // sample buffer active (1 << 7)
BUF_CNTL2_BRES | // 16-bit samples in buffer (1 << 6)
BUF_CNTL2_BFIE | // buffer full int enable (1 << 5)
BUF_CNTL2_BUF_M_BTRIGGER // trigger mode (2 << 0)
;
Register Name
Value (WRITE)
BUF_CNTL2
buf_cntl2
- Write 0x80 to Control Register 1 (CNTL1) to set the accelerometer into operating mode (PC1
= 1)
Register Name
Value
CNTL1
0x80
- Provide some time for the buffer to fill to the configured threshold. Assuming the default ODR
was used, it should take approximately 6.8 seconds. After this time, externally activate the
Master SAD + W RA Sr SAD + R ACK NACK Slave ACK ACK ACK DATA DATA Term Definition Sr Repeated Start Condition SAD Slave Address R Read Bit ACK Acknowledge RA Register Address Data Transmitted/Received Data © Kionix 2019 All Right; Reserved f‘ Kionix' 019 1
AN049
© Kionix 2019 All Rights Reserved
11 July 2019
Page 8 of 21
Trigger pin (Trig). Next, wait for the Buffer-Full Interrupt. Once Buffer-Full Interrupt is issued
on INT1 pin, acceleration data can then be read from the Buffer Read (BUF_READ) register
at address 0x3F in 2’s complement format. Also, the interrupt would be reflected in Bit4 (INT)
of STATUS_REG register and Bit6 (BFI) of INS2 register. Since the resolution of the samples
data was set to 16-bit, both high and low bytes of each sample were stored in the buffer, and
recorded in the following order: X_L, X_H, Y_L, Y_H, Z_L, Z_H with the oldest data point read
first as it is a FIFO buffer. The full buffer contains 2040 X, Y, Z elements, which corresponds
to 340 unique acceleration data samples. The data set will include all the data prior to the
trigger event, plus 1 sample after the trigger event.
Buffer reading tips:
a) The acceleration data can be read from a buffer using multiple-byte read as shown in the
Figure 3 below. The register auto-increment feature is disabled when data is read from the
Buffer Read register.
b) If data is read using single-byte read, it should be read in increments of 3 bytes in 8-bit
resolution mode and 6 bytes in 16-bit resolution mode.
c) It is very important to follow proper I2C Write-Read sequence as specified in the product
specifications. More specifically, the Master should avoid sending the Stop (P) bit at the
end of the I2C Write command, and should issue a Repeat Start bit (Sr) at the start of the
I2C Read command as show in the Figure 3. Failure of following this sequence may result
in reading the same value from the Read Buffer.
Term
Definition
S
Start Condition
Sr
Repeated Start Condition
SAD
Slave Address
W
Write Bit
R
Read Bit
ACK
Acknowledge
NACK
Not Acknowledge
RA
Register Address
Data
Transmitted/Received Data
P
Stop Condition
Figure 3: Proper I2C Sequence to Receive Data from the Slave
f‘ Kionix‘ Register Name Address Value Register Name Address Value Register Name Address Value ATH 0x30 0X08 Register Name Address Value © Klonix 2019 All Rights Reserved 019 1
AN049
© Kionix 2019 All Rights Reserved
11 July 2019
Page 9 of 21
7. Wake Up Function via latched physical hardware interrupt
- Write 0x42 to Control Register 1 (CNTL1) to set the accelerometer in stand-by mode, to set
the performance mode of the accelerometer to High Resolution (full power), G-range to ±2g
and enable the Wake Up (motion detect) function.
Register Name
Value
CNTL1
0x42
- Write 0x06 to Control Register 3 (CNTL3) to set the Output Data Rate of the Wake-Up
function (motion detection) as set but OWUF<2:0> bits to 50 Hz.
Register Name
Value
CNTL3
0x06
- Write 0x7F to Interrupt Control Register 2 (INC2) to define the direction of detected motion for
all positive and negative directions: x positive (x+), x negative (x-), y positive (y+), y negative
(y-), z positive (z+), z negative (z-) directions.
Register Name
Value
INC2
0x7F
- Write 0x05 to Interrupt Wake-Up Counter (WUFC) to set the time motion must be present
before a wake-up interrupt is set to 0.1 second. The following formula is used:
WUFC (counts) = Desired Delay Time (sec) x Wake-Up Function ODR (Hz)
WUFC (counts) = 0.1 sec x 50 Hz = 5 counts
Since the desired delay time is 0.1 second and the Wake-Up Function ODR was previously
set to 50 Hz, then the Wake-Up Timer is 5 counts.
Register Name
Value
WUFC
0x05
Write 0x08 to Interrupt Wake-Up Threshold (ATH) to set the level to 0.5g. The following
formula is used:
WAKEUP_THRESHOLD (counts) = Desired Threshold (g) x 16 (counts/g)
WAKEUP_THRESHOLD (counts) = 0.5 g x 16 counts/g = 8 counts
- Write 0x30 to Interrupt Control Register (INC1) to output the physical interrupt of the
previously defined Wake-Up detect function. This value will create an active high and
latched interrupt.
Register Name
Value
ATH
0x08
Register Name
Value
INC1
0x30
f‘ Kionix‘ Register Name Address Value Register Name Address Value Register Name Address Value INTiFiEL 0x17 n/a © Kionix 2019 All Right; Reserved 019 21
AN049
© Kionix 2019 All Rights Reserved
11 July 2019
Page 10 of 21
- Write 0x02 to Interrupt Control Register 4 (INC4) to set the wake-up function interrupt to be
reported on physical interrupt pin INT1.
Register Name
Value
INC4
0x02
- Write 0xC2 to Control Register 1 (CNTL1) to set the accelerometer in operating mode with
the previously defined settings.
Register Name
Value
CNTL1
0xC2
- Monitor the physical interrupt INT1 of the accelerometer, if the acceleration input profile
satisfies the criteria previously established for the 0.5g motion detect threshold level in both
positive and negative directions of the X, Y, Z axis for more than 0.1 second, then there
should be positive latched interrupt present. Also, the interrupt would be reflected in Bit4
(INT) of STATUS_REG register and Bit1 (WUFS) in the INS2 register.
- Read Interrupt Release (INT_REL) register to unlatch (clear) the output interrupt created by
the motion detection function.
Register Name
Value
INT_REL
n/a
- Monitor the physical interrupt INT1 of the accelerometer, the positive latched interrupt
should not be present. Repeat the last two steps of moving the accelerometer and clearing
the interrupt as needed to test this motion detect functionality based on the previous
settings.
f‘ KTonix‘ Register Name Address Value Register Name Address Value Register Name Address Value © Klonix 2019 All Rights Reserved 019 21
AN049
© Kionix 2019 All Rights Reserved
11 July 2019
Page 11 of 21
8. Activate Tilt Position Function with Face Detect
- Write 0x41 to Control Register 1 (CNTL1) to set the accelerometer in stand-by mode, to set
the performance mode of the accelerometer to High Resolution (full power), G-range to ±2g
and enable the Tilt Position function.
Register Name
Value
CNTL1
0x41
- Write 0x3F to Control 2 register (CNTL2) to enable Tilt detection from positive and negative
directions of all three axes (+x, -x, +y, -y, +z, -z). This step is optional as this is also a default
setting.
Register Name
Address
Value
CNTL2
0x19
0x3F
- Write 0x98 to Control 3 register (CNTL3) to set the output data rate for the Tilt Position
function to 12.5Hz. This step is optional as this is also a default setting.
Register Name
Address
Value
CNTL3
0x1A
0x98
- Write 0x01 to TILT_TIMER register. Here we assume an 80 msec timer will be sufficient. Note
that each count value written to this register is calculated as 1/(Tilt Position ODR) = 1/12.5Hz
= 80 msec.
Register Name
Address
Value
TILT_TIMER
0x22
0x01
- Write 0x0C to Tilt Angle Low Limit (TILT_ANGLE_LL) register to set the low threshold to 22º
from Horizontal. The value is calculated using the following equations: TILT_ANGLE_LL
(counts) = sin θ * (32 (counts/g)). This step is optional as this is also a default setting.
Register Name
Address
Value
TILT_ANGLE_LL
0x32
0x0C
- Write 0x2A to Tilt Angle High Limit (TILT_ANGLE_HL) register to set the High threshold. This
step is optional as this is also a default setting.
Register Name
Address
Value
TILT_ANGLE_HL
0x33
0x2A
- Write 0x14 to HYST_SET register to set the hysteresis that is placed between the screen
rotation states to ±15º. This step is optional as this is also a default setting.
Register Name
Address
Value
HYST_SET
0x34
0x14
(KTonix‘ Register Name Address Value Register Name Address Value © Kionix 2019 All Right; Reserved 019 21
AN049
© Kionix 2019 All Rights Reserved
11 July 2019
Page 12 of 21
- Write 0x30 to Interrupt Control Register (INC1) to output the physical interrupt of the
previously defined Tilt Position function. This value will create an active high and latched
interrupt.
Register Name
Address
Value
INC1
0x1C
0x30
- Write 0x01 to Interrupt Control Register 4 (INC4) to set the Tilt Position interrupt (TPI1) to be
reported on physical interrupt pin INT1.
Register Name
Address
Value
INC4
0x1F
0x01
- Write 0xC1 to Control Register 1 (CNTL1) to set the accelerometer in operating mode with the
previously defined settings.
Register Name
Address
Value
CNTL1
0x18
0xC1
- Monitor the physical interrupt INT1 of the accelerometer. If changes in the tilt position satisfies
the criteria previously established, then there should be a positive latched interrupt present.
Also, the interrupt would be reflected in Bit4 (INT) of STATUS_REG, Bit0 (TPS) of INS2
register, and Current Tilt Position register TSCP as well as Previous Tilt Position register
TSPP.
- Read Interrupt Release (INT_REL) register to unlatch (clear) the output interrupt created by
the Tilt Position function. The read value is dummy.
Register Name
Address
Value
INT_REL
0x17
N/A
8.1. Face Detect Position
- As was noted above, the current orientation of the sensor can be read from TSCP register at
any time. Assuming tilt detection was not changed from its default setting (detect positive and
negative directions of all three axes (+x, -x, +y, -y, +z, -z)), one of the bits in TSCP register
will be set to 1 to indicate the current orientation of the sensor.
f‘ KTonix‘ Register Name Address Value w Register Name Address Value Register Name Address Value © Klonix 2019 All Rights Reserved 019 21
AN049
© Kionix 2019 All Rights Reserved
11 July 2019
Page 13 of 21
9. Activate Tap/Double Tap Function
- Write 0x44 to Control Register 1 (CNTL1) to set the accelerometer in stand-by mode, to set
the performance mode of the accelerometer to High Resolution (full power), G-range to ±2g
and enable the Directional Tap function.
Register Name
Address
Value
CNTL1
0x18
0x44
- Write 0x3F to Interrupt Control 3 register (INC3) to enable tap/double tap from positive and
negative directions of all three axes (+x, -x, +y, -y, +z, -z). This step is optional as this is also
a default setting.
Register Name
Address
Value
INC3
0x1E
0x3F
- Write 0x98 to Control 3 register (CNTL3) to set the output data rate for the Directional Tap
function to 400Hz. This step is optional as this is also a default setting.
Register Name
Address
Value
CNTL3
0x1A
0x98
- Write 0x03 to Tap / Double-Tap Register Control register (TDTRC) to enable interrupt on
single tap and double tap. This step is optional as this is also a default setting. This setting
can be adjusted as needed.
Register Name
Address
Value
TDTRC
0x24
0x03
- Write 0x78 to Tap / Double-Tap Counter register (TDTC) to set the counter to 0.3 sec. The
TDTC counts starts at the beginning of the fist tap and it represents the minimum time
separation between the first tap and the second tap in a double tap event. More specifically,
the second tap event must end outside of the TDTC. This step is optional as this is also a
default setting. This setting can be adjusted as needed.
Register Name
Address
Value
TDTC
0x25
0x78
- Write 0xCB (203d) to Tap Threshold High register (TTH). The value is compared against the
upper 8 bits of the 4g output value (independent of the actual g-range setting of the device).
This register represents the 8-bit jerk high threshold to determine if a tap is detected. Though
this is an 8-bit register, the register value is internally multiplied by two to set the high
threshold. This multiplication results in a range of 0d to 510d with a resolution of two counts.
The Performance Index (PI) is the jerk signal that is expected to be less than this threshold,
but greater than the TTL threshold during single and double tap events. This step is optional
as this is also a default setting. This setting can be adjusted as needed.
Register Name
Address
Value
TTH
0x26
0xCB
f‘ KTonix‘ Register Name Address Value fl! double Register Name Address Value Register Name Address Value © Klonix 2019 All Rights Reserved 019 21
AN049
© Kionix 2019 All Rights Reserved
11 July 2019
Page 14 of 21
- Write 0x1A (26d) to Tap Threshold Low register (TTL). The value is compared against the
upper 8 bits of the 4g output value (independent of the actual g-range setting of the device).
This register represents the 8-bit (0d255d) jerk low threshold to determine if a tap is
detected. The Performance Index (PI) is the jerk signal that is expected to be greater than this
threshold and less than the TTH threshold during single and double tap events. This step is
optional as this is also a default setting. This setting can be adjusted as needed.
Register Name
Address
Value
TTL
0x27
0x1A
- Write 0xA2 (162d) to set the FTD counter register to 0.005 seconds. This register contains
counter information for the detection of any tap event. A tap event must be above the
performance index threshold for at least the low limit (FTDL0 FTDL2) and no more than the
high limit (FTDH0 FTDH4). This step is optional as this is also a default setting. This setting
can be adjusted as needed.
Register Name
Address
Value
FTD
0x28
0xA2
- Write 0x24 (36d) to set the STD counter register to 0.09 seconds. This register contains
counter information for the detection of a double tap event. This register sets the total amount
of time that the two taps in a double tap event can be above the PI threshold (TTL). This step
is optional as this is also a default setting. This setting can be adjusted as needed.
Register Name
Address
Value
STD
0x29
0x24
- Write 0x28 (40d) to set the TLT counter register to 0.1 seconds. This register contains counter
information for the detection of a tap event. This register sets the total amount of time that the
tap algorithm will count samples that are above the PI threshold (TTL) during a potential tap
event. It is used during both single and double tap events. However, reporting of single taps
on the physical interrupt pin INT1 or INT2 will occur at the end of the TWS. This step is
optional as this is also a default setting. This setting can be adjusted as needed.
Register Name
Address
Value
TLT
0x2A
0x28
- Write 0xA0 (160d) to set the TWS counter register to 0.4 seconds. This register contains
counter information for the detection of single and double taps. This counter defines the time
window for the entire tap event, single or double, to occur. Reporting of single taps on the
physical interrupt pin INT1 or INT2 will occur at the end of this tap window. This step is
optional as this is also a default setting. This setting can be adjusted as needed.
Register Name
Address
Value
TWS
0x2B
0xA0
- Write 0x30 to Interrupt Control Register (INC1) to output the physical interrupt of the
previously defined Tap/Double-Tap function. This value will create an active high and latched
interrupt.
(KTonix‘ Register Name Address Value Register Name Address Value © Kionix 2019 All Right; Reserved 019 21
AN049
© Kionix 2019 All Rights Reserved
11 July 2019
Page 15 of 21
Register Name
Address
Value
INC1
0x1C
0x30
- Write 0x04 to Interrupt Control Register 4 (INC4) to set the Tap/Double-Tap interrupt (TDTI)
to be reported on physical interrupt pin INT1.
Register Name
Address
Value
INC4
0x1F
0x04
- Write 0xC4 to Control Register 1 (CNTL1) to set the accelerometer in operating mode with the
previously defined settings.
Register Name
Address
Value
CNTL1
0x18
0xC4
- Monitor the physical interrupt INT1 of the accelerometer, if the acceleration input profile
satisfies the criteria previously established for Tap/Double-Tap, then there should be a
positive latched interrupt present. Also, the interrupt would be reflected in Bit4 (INT) of
STATUS_REG, and Bit3 and Bit2 (TDTS<1:0>) of INS2 registers. To distinguish between a
single and double-tap events, monitor INS2 register bits <TDTS1:TDTS0>. TDTS1 bit3 would
be set for Double-tap event, and TDTS0 bit2 for Single-tap event. Also, INS1 register can be
monitored to identify the direction the tap came from.
- Read Interrupt Release (INT_REL) register to unlatch (clear) the output interrupt created by
the Tap/Double-Tap detection function. The read value is dummy.
Register Name
Address
Value
INT_REL
0x17
N/A
f‘ KTonix‘ Register Name Address Value Register Name Address Value Register Name Address Value © Klonix 2019 All Rights Reserved 019 21
AN049
© Kionix 2019 All Rights Reserved
11 July 2019
Page 16 of 21
10. Activate Free-fall Function
- Write 0x40 to Control Register 1 (CNTL1) to set the accelerometer in stand-by mode, to set
the performance mode of the accelerometer to 16-bit resolution, and G-range to ±2g.
Register Name
Address
Value
CNTL1
0x18
0x40
- Write 0x80 to Free-Fall Control Register (FFCNTL) to enable Free fall engine, to set Free-fall
interrupt latch control, count up/down debounce methodology, and the Output Data Rate
(ODR) to 12.5Hz (Default).
Register Name
Address
Value
FFCNTL
0x2E
0x80
- Write 0x08 to Free-Fall Threshold Register (FFTH) to set the Free-fall threshold to 0.5g based
on the following equation:
FFTH (counts) = Free fall Threshold (g) x 16 (counts/g)
FFTH [counts] =0.5 g x 16 counts/g = 8 counts
Register Name
Address
Value
FFTH
0x2C
0x08
- Write 0x04 to Free-Fall Counter Register (FFC) to set the Free-fall delay detection to 0.320
sec. Note that the period of the free-fall counter is a function of Free-fall ODR set by
<OFFI2:OFF0> bits in FFCTNL register. The following equation can be used:
FFC (counts) = Free fall delay (sec) x Free fall ODR (Hz)
FFC [counts] = 0.320 sec x 12.5Hz = 4 counts
Register Name
Address
Value
FFC
0x2D
0x04
- Write 0x30 to Interrupt Control Register (INC1) to output the physical interrupt of the
previously defined Free-fall detect function. This value will create an active high and latched
interrupt.
Register Name
Address
Value
INC1
0x1C
0x30
- Write 0x80 to Interrupt Control Register 4 (INC4) to set the Free-fall interrupt (FFI) to be
reported on physical interrupt pin INT1.
Register Name
Address
Value
INC4
0x1F
0x80
(KTonix' Register Name Address Value © Kionix 1019 All Rights Reserved 019 21
AN049
© Kionix 2019 All Rights Reserved
11 July 2019
Page 17 of 21
- Write 0xC0 to Control Register 1 (CNTL1) to set the accelerometer in operating mode with the
previously defined settings.
Register Name
Address
Value
CNTL1
0x18
0xC0
- Monitor the physical interrupt INT1 of the accelerometer, if the acceleration input profile
satisfies the criteria previously established for the 0.5g free-fall detect threshold level in both
positive and negative directions of the X, Y, Z axis for more than 0.320 second, then there
should be a positive latched interrupt present. Also, Free-fall events will now be reflected in
Bit4 (INT) of STATUS_REG register, and Bit7 (FFS) of INS2 register.
- Read Interrupt Release (INT_REL) register to unlatch (clear) the output interrupt created by
the free-fall detection function. The read value is dummy.
Register Name
Address
Value
INT_REL
0x17
N/A
Procedure IZC Clock SPI Clock Enable to Valid Outputs Start-Up Time Power-Up Time (Time from VDD and I0 VDD valid to device boot completion) Software Reset Delav Standby to Operation Delay TN004 Power On ‘ © Kionix 2019 All Rights Reserved a . _ 019 Kiunix 21
AN049
© Kionix 2019 All Rights Reserved
11 July 2019
Page 18 of 21
11. Timing Requirements
There are several timing requirements that developers should keep in mind when working with
the KX112/KX122/KX123/KX124 accelerometer. Please refer to Technical Note TN004 Power On
Procedure for more information.
I²C Clock - The I²C Clock can support Fast Mode up to 400 KHz and High-Speed mode up to 3.4
MHz.
SPI Clock - The SPI Clock can support up to 10 MHz.
Enable to Valid Outputs (Start-Up Time) - After the part is enabled (PC1 bit in Control Register 1
is asserted), it takes from 2 ms to 1300 ms depending on the ODR and Power Mode setting
before the acceleration outputs are valid. (See the relevant Product Specification for details)
Power-Up Time (Time from VDD and IO_VDD valid to device boot completion) - After a Power-
up, the part takes between 20 ms to 50 ms before it is ready for communication.
Software Reset Delay - After a Software Reset, the part takes 2 ms before it is ready for
communication.
Standby to Operation Delay - Please allow 1.5/ODR delay time when transitioning from stand-by
PC1 = 0 to operating mode PC1 = 1 to allow new settings to load.
Latched/Pulsed (IEL — bit 3 — 0x081 Polarit IEA — bit 4 — 0X10 Enable/Disable IEN — bit 5 — 0X20 Read the Interrugt Release Register to Clear Microcontroller/GPIO lnterrugt Handling Interrugt Polling f‘ KTonix' © Kionix 2019 All Rights Reserved 019 21
AN049
© Kionix 2019 All Rights Reserved
11 July 2019
Page 19 of 21
12. Interrupt Configuration
The physical interrupt has 6 possible configurations, based on two states for each of the three
customizable variables located in Interrupt Control Register 1:
Latched/Pulsed (IEL bit 3 0x08)
0 Latched mode When an interrupt is triggered, it will remain active on the pin until
cleared.
1 Pulse mode When an interrupt is triggered, it will cause a short (~50µs) pulse on the
pin and clear itself.
Polarity (IEA bit 4 0x10)
0 Active Low The interrupt pin will normally be HIGH, but will transition to LOW when
an interrupt is triggered.
1 Active High The interrupt pin will normally be LOW, but will transition to HIGH when
an interrupt is triggered.
Enable/Disable (IEN bit 5 0x20)
0 Disabled Interrupt conditions will not be reflected on the physical interrupt pin.
1 Enabled Interrupt conditions will be reflected on the physical interrupt pin.
12.1. A Few Interrupt Tips
Read the Interrupt Release Register to Clear
In latched mode, the INT_REL register must be read in order to clear the physical interrupt
pin. This will also clear the Interrupt Source Registers and the INT bit (0x10) in
STATUS_REG.
Microcontroller/GPIO Interrupt Handling
GPIO configuration is based solely on the connected hardware. The accelerometers in
this family can be configured to issue interrupts depending on how the GPIO is
programmed to catch them (if this is not the case, please contact your Kionix Sales
Representative). Generally, when an interrupt is triggered, the developer should take the
following steps:
1. Disable GPIO interrupt
2. Clear GPIO interrupt and generate desired functionality
3. Enable GPIO interrupt
These steps should be taken without calling any digital communication transactions if
done in an interrupt context, because the operating system or kernel will not allow busy-
waiting on an I/O operation during an interrupt service routine.
Interrupt Polling - If physical interrupts are not used, a polling mechanism can be devised, which
checks the INT bit in STATUS_REG. This mechanism should then look at INS2 to determine
which engine caused the interrupt and what steps should be taken before clearing the interrupt
source information by reading the INT_REL register.
All Interrugt Issues Tilt Interrugt Not Working WUF {Wake Ug Function Interrugt Not Working TDT Ta /DoubIe-Ta Interru tNotWorkin Free fall Detect Interrugt Not Working ‘ © Kionix 1019 All Rights Reserved e . _ 019 KlCian 21
AN049
© Kionix 2019 All Rights Reserved
11 July 2019
Page 20 of 21
13. Troubleshooting
All Interrupt Issues
- Make sure the accelerometer is configured to issue interrupt signals in the way that your
GPIO is programmed to handle them.
- An oscilloscope on the physical interrupt pin can be a valuable tool to confirm physical
interrupt operation.
- Double check the Tilt Position State Mask bits in CNTL2 (Tilt Position Function), the axis
mask bits in CNTL2 (Wake-up Function), and/or the Tap/Double-Tap Mask bits in CNTL3
(Tap/Double-Tap Function), and Free Fall Threshold value in FFTH (Free Fall Detect
Function)
- The Tilt Timer, WUF Timer, and TDT Timer(s) are based on their respective Output Data
Rates, so make sure the correct cycle time is used when calculating the expected timer
length (please refer to the specific product specification).
Tilt Interrupt Not Working
- Make sure that the Tilt Position engine is enabled (TPE bit in CNTL1).
- Try shortening the timer requirements and make sure the next state transition does not
occur until after the expiration of the Tilt Timer.
- Try increasing the Tilt Angle to ensure that the engine can see the transition between the
X and Y axes and the Z axis (this should not be necessary if using the default value for Tilt
Angle, but it’s worth considering if problems continue).
WUF (Wake Up Function) Interrupt Not Working
- Make sure that the WUF engine is enabled (WUFE bit in CNTL1).
- Try altering the threshold requirements to achieve desired operation. If the part is waking
up too easily, try increasing the threshold. If the interrupt is not firing at all, the threshold
may be set too high.
- Try shortening the timer requirements, and make sure the acceleration on an unmasked
axis is above the threshold until the expiration of the WUF Timer.
TDT (Tap/Double-Tap) Interrupt Not Working
- Make sure that the TDT engine is enabled (TDTE bit in CNTL1).
- Try altering the threshold requirements to achieve desired operation. If the part is
generating interrupts too often, perhaps due to a large noise floor created by excessive
environmental vibrations, try increasing the performance index low threshold (TTL) and/or
reducing the performance index high threshold (TTH). If the interrupt is not firing at all,
perhaps the low threshold may be set too high, or the high threshold may be set too low.
- There are many timers in this engine which must work together closely, so for standard
operation if one timer is changed the other timers may need to be changed proportionally.
Free fall Detect Interrupt Not Working
- Make sure the Free fall engine is enabled (FFIE bit in FFCNTL)
- Try adjusting the threshold requirements to achieve desired operation by adjusting the
threshold value in the FFTH register. If the part is generating interrupts two often, try
increasing the delay/debounce time in the FFC register. If the interrupt is not firing at all,
perhaps the threshold is set too high.
Placement Orientation httgflwww. onix.com/garametric/Accelerometers © Kionix 1019 All Rights Reserved ¥ . _ 019 KlOnIX 21
AN049
© Kionix 2019 All Rights Reserved
11 July 2019
Page 21 of 21
14. Accelerometer Placement and Orientation
Placement It is important to note that the placement of the accelerometer within the target device can
have a significant effect on tap/double-tap direction resolution. If tap detection is desired, the part should
be placed as far away from the edges of the device housing as possible, with the ideal location being at
the target device’s center of mass.
Orientation While it is recommended to align the accelerometer’s axes with those of the target device,
it will sometimes be desirable or necessary to alter the part’s orientation with respect to the device
housing. Rotating about the Z axis at intervals of 90 degrees or about the X or Y axes at intervals of 180
degrees should not impact functionality. However, it is highly recommended that the device is not rotated
90 or 270 degrees about the X or Y axes. Due to the asymmetrical nature of the tilt position function,
altering the orientation of the Z axis in this manner can cause incorrect screen rotation direction
resolution.
15. The Kionix Advantage
Kionix technology provides for X, Y, and Z-axis sensing on a single, silicon chip. One accelerometer can
be used to enable a variety of simultaneous features including, but not limited to:
Hard Disk Drive protection
Vibration analysis
Tilt screen navigation
Sports modeling
Theft, man-down, accident alarm
Image stability, screen orientation & scrolling
Computer pointer
Navigation, mapping
Game playing
Automatic sleep mode
16. Theory of Operation
Kionix MEMS linear tri-axis accelerometers function on the principle of differential capacitance.
Acceleration causes displacement of a silicon structure resulting in a change in capacitance. A signal-
conditioning CMOS technology ASIC detects and transforms changes in capacitance into an analog
output voltage, which is proportional to acceleration. These outputs can then be sent to a micro-controller
for integration into various applications.
For product summaries, specifications, and schematics, please refer to the Kionix MEMS accelerometer
product catalog at http://www.kionix.com/parametric/Accelerometers

Products related to this Datasheet

ACCELEROMETER 2-8G I2C/SPI 12LGA
ACCELEROMETER 2-8G I2C/SPI 16LGA
ACCELEROMETER 2-8G I2C/SPI 16LGA
ACCELEROMETER 2-8G I2C/SPI 12LGA
KX112-1042 EVAL BOARD
KX124-1051 EVAL BOARD
KX122-1037 EVAL BOARD
ACCELEROMETER 2-8G I2C/SPI 16LGA
ACCELEROMETER 2-8G I2C/SPI 16LGA
ACCELEROMETER 2-8G I2C/SPI 12LGA
ACCELEROMETER 2-8G I2C/SPI 16LGA
EVAL BOARD FOR IC KX122-1037
ACCELEROMETER 2-8G I2C/SPI 16LGA
ACCELEROMETER 2-8G I2C/SPI 12LGA