Pressure Conversion Calculator

Convert pressure measurements including psi to bar, kg/cm2 to psi, bar to kg/cm2, and other pressure conversions including pa, bar, kg/cm2, psi, mm H2O, and inches H2O by using DigiKey's pressure conversion calculator.

A pascal (Pa N/m2) is a unit of pressure equivalent to one newton per square meter.

A Bar is equal to 100000 Pa and is slightly less than the average atmospheric pressure on Earth at sea level.

Kilogram per square centimeter (kg/cm2) is a pressure measure equal to one kilogram-force per square centimeter, another name for this unit is technical atmosphere.

Pound per square inch (psi) is the result from a force of one pound-force applied to an area of one square inch.

Millimeters of water column at 4 degrees Celsius (mm H2O @ 4°C) is defined as the pressure exerted by a column of water 1 mm high, at 4°C, at the standard acceleration of gravity.

Inches of water column at 4 degrees Celsius (inches H2O @ 4°C) is defined as the pressure exerted by a column of water 1 inch in height, at 4°C, at the standard acceleration of gravity.

 

Convert from:

Calculate Reset
Pa (N/m2) Bar kg/cm2 psi mm H2O @ 4°C
inches H2O @ 4°C

Related Products:

Pressure Sensors, Transducers
Pressure Sensors,
Transducers